This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.Now I am working on the SPI communication between 28335 and EtherCAT -- LAN9252. The error reported on TwinCAT is as follows: the board of LAN9252 was welded by myself. Also, does the PORT0 of EtherCAT slave station have to be the input port? I connected PORT1 to my computer, my ESI file was burned successfully, and TwinCAT was able to scan the slave station information.What's the problem?Thanks.
Hi dear,
Is there question specifically about the F2833x and its SPI port?
Thanks.
您好,上图是我的SPI配置和SPI的读写函数,我自己检查了几遍,可能是由于我是初学者,没有查出什么问题,请问我的这个SPI配置的是否有问题?
此外,我的堆栈在CCS中的运行陷入了图片上的do_while的循环,程序运行时SPI的数据发送接受寄存器有改变且有值,但似乎不能向LAN9252的对应地址寄存器写值和读值,9252相关的程序是倍福SSC自动生成的,并无大的改动,请问您了解这个状况的原因吗?另外非常感谢您帮我反馈问题。
您好,
PDIReadLAN9252DirectReg ()返回的值是多少? 是正确的值吗?还是说代码就卡在那里?