This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,TI的技术专家
我使用的MCU是TMS320F28075PZP(100PIN),测试MCD不通过,使用的是C2000Ware库,版本C2000Ware_4_02_00_00,问题详细描述在英文技术论坛已发,请参考
目前的问题是,设置了OSCOFF(SysCtl_disconnectMCDClockSource();就是这条语句),MCDCR寄存器的bit0,即MCDSTS flag没有变1,也就是说没有检查到时钟丢失。用的是库里面的示例程序。
//############################################################################# // // FILE: sta_main.c // // TITLE: Self Test Application Main source // //############################################################################# // $TI Release: F2807x Diagnostic Library v1.00.02.00 $ // $Release Date: Mon Dec 18 17:00:32 CST 2017 $ // $Copyright: // Copyright (C) 2016-2017 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included files for device configuration // #include <stdbool.h> #include <stdint.h> #include <string.h> #include "driverlib.h" #include "device.h" #include "F2807x_device.h" #include "F021_F2837xD_C28x.h" // // Included files for test-infrastructure. // #include "sta_timer.h" #include "sta_tests.h" #include "sta_comm.h" // // Globals // int16_t enableErrorInject; int16_t enableReset; volatile bool nmiISRFlag = false; uint16_t nmiStatus = 0U; bool mcdDetect = false; uint32_t result = 1; uint32_t fail = 0U; // // Prototypes // void STA_Main_configXCLKOut(void); Fapi_StatusType STA_Main_initFlashAPI(void); #ifdef _FLASH // These are defined by the linker (see device linker command file) extern uint16_t RamfuncsLoadStart; extern uint16_t RamfuncsLoadSize; extern uint16_t RamfuncsRunStart; extern uint16_t HwbistLoadStart; extern uint16_t HwbistLoadSize; extern uint16_t HwbistRunStart; #endif // // Function Prototypes // __interrupt void nmi_isr(void); // // Main // void main(void) { #ifdef _FLASH memcpy(&HwbistRunStart, &HwbistLoadStart, (size_t)&HwbistLoadSize); #endif unsigned char *msg; uint16_t testIndex = 0; Fapi_StatusType statusFlashAPI = Fapi_Status_Success; enableErrorInject = 0; uint16_t nmiWatchdogPeriod = 0x1000; // // Configure PLL, disable WD, enable peripheral clocks. // Device_init(); // // Disable pin locks and enable internal pull-ups. // Device_initGPIO(); //*********************************** //added by yang for debug GPIO_setPinConfig(GPIO_43_GPIO43); GPIO_setDirectionMode(43,GPIO_DIR_MODE_OUT); GPIO_setPadConfig(43,GPIO_PIN_TYPE_STD); GPIO_writePin(43,1); //************************************ // // Put watchdog in interrupt mode. // SysCtl_setWatchdogMode(SYSCTL_WD_MODE_INTERRUPT); // statusFlashAPI = STA_Main_initFlashAPI(); // if(statusFlashAPI != Fapi_Status_Success) // { // ESTOP0; // } // // Disable global interrupts. // DINT; // // Initialize interrupt controller and vector table. // Interrupt_initModule(); Interrupt_initVectorTable(); SysCtl_clearAllNMIFlags(); Interrupt_register(INT_NMI, &nmi_isr); SysCtl_setNMIWatchdogPeriod(nmiWatchdogPeriod); // // Enabling the NMI global interrupt (typically already enabled by boot ROM // or GEL file). // EALLOW; HWREGH(NMI_BASE + NMI_O_CFG) |= NMI_CFG_NMIE; EDIS; Interrupt_enable(INT_NMI); EINT; ERTM; if(SysCtl_getClock(DEVICE_OSCSRC_FREQ) != DEVICE_SYSCLK_FREQ) { fail++; } SysCtl_enableMCD(); SysCtl_disconnectMCDClockSource(); fail=3; while(nmiISRFlag != true) { fail++; } fail=5; // A missing clock was detected. // if(mcdDetect != true) { fail++; } // Check if the NMI triggered was due to a clock failure. // if((nmiStatus & SYSCTL_NMI_CLOCKFAIL) != SYSCTL_NMI_CLOCKFAIL) { fail++; } // Check the PLL System clock after the Missing clock detection // is simulated. It should be equal to INTOSC1(10Mhz). // if(SysCtl_getClock(DEVICE_OSCSRC_FREQ) != SYSCTL_DEFAULT_OSC_FREQ) { fail++; } // To lock the PLL after missing clock detection, we first explicitly // switch the clock source to INTOSC1, reset the missing clock detect // circuit, and then re-lock the PLL. // // Configure oscillator source to INTOSC1. // SysCtl_selectOscSource(SYSCTL_OSCSRC_OSC1); SysCtl_connectMCDClockSource(); // Reset the missing clock detection logic after clock failure. // SysCtl_resetMCD(); // Set up PLL control and clock dividers using the original clock source. // SysCtl_setClock(DEVICE_SETCLOCK_CFG); // Check the system clock after the missing clock detection is cleared // and handled using INTOSC1 as clock source. // if(SysCtl_getClock(DEVICE_OSCSRC_FREQ) != DEVICE_SYSCLK_FREQ) { fail++; } // Status of a successful handling of missing clock detection. // if(fail != 0U) { result = 1; //fail // GPIO_writePin(43,0); } else { result = 0; //pass // GPIO_writePin(43,0); } while(1); // // Debug // // STA_Main_configXCLKOut(); // // Configure SCI A as the main communication port // // STA_Comm_configSCIA(); // // Configure Timer 0 as the main time-out timer // // STA_Timer_config(4000U); //#if STA_UTIL_PROFILE // STA_Util_configProfiler(CPUTIMER1_BASE); //#endif // // Enable Global Interrupt (INTM) and real time interrupt (DBGM) // // EINT; // ERTM; // // Send starting message. // // msg = "\r\n\n\nBegin Test\0"; // STA_Comm_transmitData(msg); /* for(;;) { if(STA_Timer_isTimedOut()) { if(enableErrorInject) { STA_Tests_injectErrorEnable(); } else { STA_Tests_injectErrorDisable(); } if(enableReset) { STA_Tests_enableReset(); } else { STA_Tests_disableReset(); } STA_Comm_transmitData( STA_Tests_testDevice(STA_Tests_testArray[testIndex++])); if(testIndex >= STA_TESTS_NUMBERS) { testIndex = 0U; } STA_Timer_restart(); } } */ } // // STA_Main_configXCLKOut(void) // void STA_Main_configXCLKOut(void) { // Configure GPIO 73 as SYSCLK out GPIO_setPadConfig(73,GPIO_PIN_TYPE_STD); GPIO_setPinConfig(GPIO_73_XCLKOUT); // Clock source is SYSCLK SysCtl_selectClockOutSource(SYSCTL_CLOCKOUT_SYSCLK); EALLOW; // XCLOCK out = clock source /8 HWREG(CLKCFG_BASE + SYSCTL_O_XCLKOUTDIVSEL) = 3U; EDIS; } // // STA_Main_initFlashAPI(void) // #pragma CODE_SECTION(STA_Main_initFlashAPI, ".TI.ramfunc"); Fapi_StatusType STA_Main_initFlashAPI(void) { Fapi_StatusType returnStatus; // // Disable ECC when initializing the Flash API // Flash_disableECC(FLASH0ECC_BASE); EALLOW; // // This function is required to initialize the Flash API based on System // frequency before any other Flash API operation can be performed // returnStatus = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, DEVICE_SYSCLK_FREQ / 1000000U); EDIS; return(returnStatus); } // // nmiISR - The interrupt service routine called when the NMI // is generated on clock failure detection. // __interrupt void nmi_isr(void) { nmiISRFlag = true; mcdDetect = SysCtl_isMCDClockFailureDetected(); nmiStatus = SysCtl_getNMIFlagStatus(); SysCtl_clearAllNMIFlags(); GPIO_writePin(43,0); } // // End of File //