This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374S: ADC不同触发源触发ADC采样异常

Part Number: TMS320F28374S


 各位大侠:
         当前在设置采样时,发现如果同一路采样例如ADCA,在配置SOC过程中,采用了时钟不同步,频率不相同的不同EPWM触发源,会非常大概率存在采样异常情况,想请问一下,当这种情况下,需要注意些什么,采用外部电路都是运放输入的,
       具体配置附件,附件影响ADC采样的就是触发源0x0F,EPWM6,因为他的同步时钟已经和其他EPWM不一样( EPwm6Regs.TBCTL.bit.PHSEN= TB_DISABLE;),频率为31K,与其他几路EPWM不同步,EPWM3/EPWM4=30K,和EPWM1/2同步,ADC异常采样见附件。
/**********************************ADC配置*********************************************/
	
    /*ADC Clock Prescaler, Sys CLock = 200M, ADC Clock = 200/4 = 50M*/
    /*TODO:>set 6 ADCCLK divider to /4, 50M*/
    /*TODO:>set 2 ADCCLK divider to /2, 100M*/
	AdcaRegs.ADCCTL2.bit.PRESCALE      = 2;
	AdcbRegs.ADCCTL2.bit.PRESCALE      = 2;
	AdccRegs.ADCCTL2.bit.PRESCALE      = 2;
	AdcdRegs.ADCCTL2.bit.PRESCALE      = 2;

    /*SOC Signaling Mode*/
	AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
	AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
	AdcSetMode(ADC_ADCC, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
	AdcSetMode(ADC_ADCD, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);

    /*Set pulse positions to late*/
	AdcaRegs.ADCCTL1.bit.INTPULSEPOS   = 1;
	AdcbRegs.ADCCTL1.bit.INTPULSEPOS   = 1;
	AdccRegs.ADCCTL1.bit.INTPULSEPOS   = 1;
	AdcdRegs.ADCCTL1.bit.INTPULSEPOS   = 1;
	
    /*power up the ADC*/
    /*0-All analog circuitry inside the core is powered down*/
    /*1-All analog circuitry inside the core is powered up*/
	AdcaRegs.ADCCTL1.bit.ADCPWDNZ      = 1;
	AdcbRegs.ADCCTL1.bit.ADCPWDNZ      = 1;
	AdccRegs.ADCCTL1.bit.ADCPWDNZ      = 1;
	AdcdRegs.ADCCTL1.bit.ADCPWDNZ      = 1;

	/*ADC interruput 1 enable*/
    /*0-ADCINTFLG register is cleared, ADCINT2 pulses are generated*/
    /*1-ADCINT2 pulses are generated whenever an EOC pulse is generated*/
	AdcaRegs.ADCINTSEL1N2.bit.INT1CONT = 1;   //连续模式
	AdcaRegs.ADCINTSEL1N2.bit.INT1E    = 1;   //Int Enable
	AdcaRegs.ADCINTSEL1N2.bit.INT1SEL  = 0x05;//EOC5 is trigger for ADCINT1

    /*ADC interruput 2 enable*/
    AdcbRegs.ADCINTSEL1N2.bit.INT1CONT = 1;   //连续模式
    AdcbRegs.ADCINTSEL1N2.bit.INT1E    = 1;   //Int Enable
    AdcbRegs.ADCINTSEL1N2.bit.INT1SEL  = 0x01;//EOC1 is trigger for ADCINT1
    //delay for 1ms to allow ADC time to power up
    DELAY_US(1000);

    /*TODO:>采样窗口最小14,5ns*20 = 100ns*/
	/* Sample ADCINA1 PV1_I, triggered by eMPW6 ADCSOCA, 12 system clock smaple window */
	AdcaRegs.ADCSOC0CTL.bit.CHSEL    = 1;
	AdcaRegs.ADCSOC0CTL.bit.TRIGSEL  = 0x0F;
	AdcaRegs.ADCSOC0CTL.bit.ACQPS    = 19;
	/* Sample ADCINA3 PV2_I, triggered by eMPW7 ADCSOCA, 12 system clock smaple window */
	AdcaRegs.ADCSOC1CTL.bit.CHSEL    = 3;
	AdcaRegs.ADCSOC1CTL.bit.TRIGSEL  = 0x11;
	AdcaRegs.ADCSOC1CTL.bit.ACQPS    = 19;
	/* Sample ADCINA5 BAT1_I, triggered by eMPW3 ADCSOCA, 12 system clock smaple window */
	AdcaRegs.ADCSOC2CTL.bit.CHSEL    = 5;
	AdcaRegs.ADCSOC2CTL.bit.TRIGSEL  = 0x09;
	AdcaRegs.ADCSOC2CTL.bit.ACQPS    = 19;
	/* Sample ADCINA0 PV1_VOLT Voltage, triggered by eMPW1 ADCSOCA, 12 system clock smaple window */
	AdcaRegs.ADCSOC3CTL.bit.CHSEL    = 0;
	AdcaRegs.ADCSOC3CTL.bit.TRIGSEL  = 0x05;
	AdcaRegs.ADCSOC3CTL.bit.ACQPS    = 19;
	/* Sample ADCINA2 PV2_VOLT Voltage, triggered by eMPW1 ADCSOCA, 12 system clock smaple window */
	AdcaRegs.ADCSOC4CTL.bit.CHSEL    = 2;
	AdcaRegs.ADCSOC4CTL.bit.TRIGSEL  = 0x05;
	AdcaRegs.ADCSOC4CTL.bit.ACQPS    = 19;
	/* Sample ADCINA4 BAT_VOLT, triggered by eMPW1 ADCSOCA, 12 system clock smaple window */
	AdcaRegs.ADCSOC5CTL.bit.CHSEL    = 4;
	AdcaRegs.ADCSOC5CTL.bit.TRIGSEL  = 0x05;
	AdcaRegs.ADCSOC5CTL.bit.ACQPS    = 19;



/**********************************EPWM配置*****************************************************************************************/
{
	EALLOW;
	InputXbarRegs.INPUT1SELECT = 29;//DC_OCP  - GPIO29 - TZ1
	InputXbarRegs.INPUT2SELECT = 31;//INV_OCP - GPIO31 - TZ2
	InputXbarRegs.INPUT3SELECT = 99;//BUS_OVP - GPIO99 - TZ3
	EDIS;

	EALLOW;
	CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;      // Stop all the TB clocks
	ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV = 1;// EPWMCLK必须2分频SYSCLK
	EDIS;

    //RLDCSF - AQSFRC寄存器中的值从阴影寄存器中的载入方式,零点载入,周期值载入还是立即载入
    //EPwm1Regs.AQSFRC.bit.RLDCSF = 0x03;  // load immediately
    //EPwm2Regs.AQSFRC.bit.RLDCSF = 0x03;  // load immediately

    // force all PWM to low
    // AQCSFRC - CSFB + CSFA
    // CSFB + CSFA
    // 00 00 - disable
    // 01 01 - B low & A low
    // 10 10 - B high & A high
    // 11 11 - disable
    // EPwm1Regs.AQCSFRC.all = 0x05;       // 0101, A low & B low
    // EPwm2Regs.AQCSFRC.all = 0x05;       // 0101, A low & B low

	//时钟输入均默认PWM1的时钟
	//EPWM1->EPWM2->EPWM3
	//EPWM1->EPWM4->EPWM5-EPWM6
	//EPWM1->EPWM7->EPWM8-EPWM9
	//EPWM1->EPWM10->EPWM11-EPWM12

	/* inverter ePWM generator */
	//================================================================================
	//PWM1A-G1和G4在正半周期发出相同的PWM波
	//PWM1B-G6在正半周期发出互补的PWM波
	//PWM2A-G2和G3在负半周期发出相同的PWM波
	//PWM2B-G5在负半周期发出互补的PWM波
    EPwm1Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm1Regs.TBPRD                     = INV_PWM_PERD;    //set the PWM period
    EPwm1Regs.TBPHS.bit.TBPHS           = 2;
    EPwm1Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm1Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm1Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)
    EPwm1Regs.TBCTL.bit.SYNCOSEL        = TB_CTR_ZERO;     //Master, Sent sync signal while count to zero

    EPwm1Regs.TBCTL.bit.PHSEN           = TB_DISABLE;      //Master, no need phase load
    EPwm1Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm1Regs.TBCTR                     = 0;
	EPwm1Regs.CMPA.bit.CMPA             = 0;               //Duty = 0% at the beginning
	EPwm1Regs.CMPB.bit.CMPB             = 0;
	EPwm1Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
	EPwm1Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
	EPwm1Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_ZERO_PRD; //Load compare A register when counter = zero or period
	EPwm1Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_ZERO_PRD; //Load compare B register when counter = zero or period

	//比较点的动作
	EPwm1Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
	EPwm1Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
	EPwm1Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
	EPwm1Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

	//死区设置
	EPwm1Regs.DBCTL.bit.IN_MODE         = DBA_ALL;
	EPwm1Regs.DBCTL.bit.POLSEL          = DB_ACTV_HIC;
	EPwm1Regs.DBCTL.bit.OUT_MODE        = DB_FULL_ENABLE;  //enable inverter PWM deadband control
	EPwm1Regs.DBRED.bit.DBRED           = DB_1US;
	EPwm1Regs.DBFED.bit.DBFED           = DB_1US;

	EPwm1Regs.ETSEL.bit.SOCAEN          = 1;               //Enable PWM1SOCA
	EPwm1Regs.CMPB.bit.CMPB             = 250;
	EPwm1Regs.ETSEL.bit.SOCASEL         = ET_CTRU_CMPB;    //Enable event time-base counter count up and = comapre B
	EPwm1Regs.ETPS.bit.SOCAPRD          = ET_1ST;          //Generate the EPWMxSOCA pulse on the first event

	EALLOW;
	//触发TZ时的设置-TODO-放到死区的前面
	EPwm1Regs.TZSEL.bit.OSHT1           = TZ_ENABLE;       //PV过流
	EPwm1Regs.TZSEL.bit.OSHT2           = TZ_ENABLE;       //逆变过流
	EPwm1Regs.TZSEL.bit.OSHT3           = TZ_ENABLE;       //电池过流
	EPwm1Regs.TZCTL.bit.TZA             = TZ_FORCE_LO;     //触发TZ时输出低电平
	EPwm1Regs.TZCTL.bit.TZB             = TZ_FORCE_LO;
	EPwm1Regs.TZFRC.bit.OST             = 1;               //Disable PWM at first
	EDIS;

	//PWM1触发中断设置
	EPwm1Regs.ETSEL.bit.INTSEL          = ET_CTR_ZERO;     //Interrupt when counter = zero
	EPwm1Regs.ETPS.bit.INTPRD           = ET_1ST;          //Interrupt generate on the first time
	EPwm1Regs.ETSEL.bit.INTEN           = ET_DISABLE;      //disable PWM interrupt

	/* inverter ePWM generator */
    EPwm2Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm2Regs.TBPRD                     = INV_PWM_PERD;    //set the PWM period
    EPwm2Regs.TBPHS.bit.TBPHS           = 2;
    EPwm2Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm2Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm2Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)
    EPwm2Regs.TBCTL.bit.SYNCOSEL        = TB_CTR_ZERO;     //Sent sync signal while count to zero

    EPwm2Regs.TBCTL.bit.PHSEN           = TB_ENABLE;       //
    EPwm2Regs.TBCTL.bit.PHSDIR          = 1;
    EPwm2Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm2Regs.TBCTR                     = 0;
	EPwm2Regs.CMPA.bit.CMPA             = 0;               //Duty = 0% at the beginning
	EPwm2Regs.CMPB.bit.CMPB             = 0;
	EPwm2Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
	EPwm2Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
	EPwm2Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_ZERO_PRD; //Load compare A register when counter = zero or period
	EPwm2Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_ZERO_PRD; //Load compare B register when counter = zero or period

	//比较点的动作
	EPwm2Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
	EPwm2Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
	EPwm2Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
	EPwm2Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

	//死区设置
	EPwm2Regs.DBCTL.bit.IN_MODE         = DBA_ALL;
	EPwm2Regs.DBCTL.bit.POLSEL          = DB_ACTV_HIC;
	EPwm2Regs.DBCTL.bit.OUT_MODE        = DB_FULL_ENABLE;  //enable inverter PWM deadband control
	EPwm2Regs.DBRED.bit.DBRED           = DB_1US;
	EPwm2Regs.DBFED.bit.DBFED           = DB_1US;

	EPwm2Regs.ETSEL.bit.SOCAEN          = 1;               //Disable PWM2SOCA
    EPwm2Regs.CMPB.bit.CMPB             = 250;
    EPwm2Regs.ETSEL.bit.SOCASEL         = ET_CTRU_CMPB;    //Enable event time-base counter count up and = comapre B
	EPwm2Regs.ETPS.bit.SOCAPRD          = ET_1ST;          //Generate the EPWMxSOCA pulse on the first event

	EALLOW;
	EPwm2Regs.TZSEL.bit.OSHT1           = TZ_ENABLE;
	EPwm2Regs.TZSEL.bit.OSHT2           = TZ_ENABLE;
	EPwm2Regs.TZSEL.bit.OSHT3           = TZ_ENABLE;
	EPwm2Regs.TZCTL.bit.TZA             = TZ_FORCE_LO;
	EPwm2Regs.TZCTL.bit.TZB             = TZ_FORCE_LO;
	EPwm2Regs.TZFRC.bit.OST             = 1;               //Disable PWM at first
	EDIS;

	//PWM2触发中断的设置
	EPwm2Regs.ETSEL.bit.INTSEL          = ET_CTR_PRDZERO;  //Interrupt when counter = zero or period
	EPwm2Regs.ETPS.bit.INTPRD           = ET_1ST;          //Interrupt generate on the first time
	EPwm2Regs.ETSEL.bit.INTEN           = ET_DISABLE;      //disable PWM interrupt


    //--------------------------------------------------------------------------------
	/*Charger ePWM generator, Buck-Boost*/
    EPwm3Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm3Regs.TBPRD                     = BAT_PWM_PERD;    //set the PWM period
    EPwm3Regs.TBPHS.bit.TBPHS           = 2;
    EPwm3Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm3Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm3Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)
    EPwm3Regs.TBCTL.bit.SYNCOSEL        = TB_SYNC_IN;
    EPwm3Regs.TBCTL.bit.PHSEN           = TB_ENABLE;
    EPwm3Regs.TBCTL.bit.PHSDIR          = 1;
    EPwm3Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm3Regs.TBCTR                     = 0;
	EPwm3Regs.CMPA.bit.CMPA             = 0;               //Duty = 0% at the beginning
	EPwm3Regs.CMPB.bit.CMPB             = 0;
	EPwm3Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
	EPwm3Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
	EPwm3Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_ZERO_PRD; //Load compare A register when counter = zero or period
	EPwm3Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_ZERO_PRD; //Load compare B register when counter = zero or period

	EPwm3Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
	EPwm3Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
	EPwm3Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
	EPwm3Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

	EPwm3Regs.DBCTL.bit.IN_MODE         = DBA_ALL;
	EPwm3Regs.DBCTL.bit.POLSEL          = DB_ACTV_HIC;
	EPwm3Regs.DBCTL.bit.OUT_MODE        = DB_FULL_ENABLE;  // enable inverter PWM deadband control
	EPwm3Regs.DBRED.bit.DBRED           = DB_1US;
	EPwm3Regs.DBFED.bit.DBFED           = DB_1US;

	EPwm3Regs.ETSEL.bit.SOCAEN          = 1;               //Disable PWM1SOCA
    EPwm3Regs.CMPB.bit.CMPB             = 300;
    EPwm3Regs.ETSEL.bit.SOCASEL         = ET_CTRU_CMPB;    //Enable event time-base counter count up and = compare B
	EPwm3Regs.ETPS.bit.SOCAPRD          = ET_1ST;          //Generate the EPWMxSOCA pulse on the first event

	EALLOW;
	EPwm3Regs.TZSEL.bit.OSHT1           = TZ_ENABLE;
	EPwm3Regs.TZSEL.bit.OSHT2           = TZ_ENABLE;
	EPwm3Regs.TZSEL.bit.OSHT3           = TZ_ENABLE;
	EPwm3Regs.TZCTL.bit.TZA             = TZ_FORCE_LO;
	EPwm3Regs.TZCTL.bit.TZB             = TZ_FORCE_LO;
	EPwm3Regs.TZFRC.bit.OST             = 1;               //Disable PWM at first
	EDIS;

	EPwm3Regs.ETSEL.bit.INTEN           = ET_DISABLE;      //disable PWM interrupt

    /*Charger ePWM generator, Buck-Boost*/
    EPwm4Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm4Regs.TBPRD                     = BAT_PWM_PERD;    //set the PWM period
    EPwm4Regs.TBPHS.bit.TBPHS           = BAT_PWM_PERD;
    EPwm4Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm4Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm4Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)
    EPwm4Regs.TBCTL.bit.SYNCOSEL        = TB_SYNC_IN;
    EPwm4Regs.TBCTL.bit.PHSEN           = TB_ENABLE;
    EPwm4Regs.TBCTL.bit.PHSDIR          = 1;
    EPwm4Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm4Regs.TBCTR                     = 0;
    EPwm4Regs.CMPA.bit.CMPA             = 0;               //Duty = 0% at the beginning
    EPwm4Regs.CMPB.bit.CMPB             = 0;
    EPwm4Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
    EPwm4Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
    EPwm4Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_ZERO_PRD; //Load compare A register when counter = zero or period
    EPwm4Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_ZERO_PRD; //Load compare B register when counter = zero or period

    EPwm4Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
    EPwm4Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
    EPwm4Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
    EPwm4Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

    EPwm4Regs.DBCTL.bit.IN_MODE         = DBA_ALL;
    EPwm4Regs.DBCTL.bit.POLSEL          = DB_ACTV_HIC;
    EPwm4Regs.DBCTL.bit.OUT_MODE        = DB_FULL_ENABLE;  // enable inverter PWM deadband control
    EPwm4Regs.DBRED.bit.DBRED           = DB_1US;
    EPwm4Regs.DBFED.bit.DBFED           = DB_1US;

    EPwm4Regs.ETSEL.bit.SOCAEN          = 1;               //Disable PWM1SOCA
    EPwm4Regs.CMPB.bit.CMPB             = 300;
    EPwm4Regs.ETSEL.bit.SOCASEL         = ET_CTRU_CMPB;    //Enable event time-base counter count up and = compare B
    EPwm4Regs.ETPS.bit.SOCAPRD          = ET_1ST;          //Generate the EPWMxSOCA pulse on the first event

    EALLOW;
    EPwm4Regs.TZSEL.bit.OSHT1           = TZ_ENABLE;
    EPwm4Regs.TZSEL.bit.OSHT2           = TZ_ENABLE;
    EPwm4Regs.TZSEL.bit.OSHT3           = TZ_ENABLE;
    EPwm4Regs.TZCTL.bit.TZA             = TZ_FORCE_LO;
    EPwm4Regs.TZCTL.bit.TZB             = TZ_FORCE_LO;
    EPwm4Regs.TZFRC.bit.OST             = 1;               //Disable PWM at first
    EDIS;

    EPwm4Regs.ETSEL.bit.INTEN           = ET_DISABLE;      //disable PWM interrupt

    /*PWM5-NoUsed*/
	EPwm5Regs.TBCTL.bit.PHSEN           = TB_ENABLE;
	EPwm5Regs.TBCTL.bit.SYNCOSEL        = TB_SYNC_IN;

    //--------------------------------------------------------------------------------
	/*Boost1 ePWM generator*/
    EPwm6Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm6Regs.TBPRD                     = BOOST_PWM_PERD;  // set the PWM period
    EPwm6Regs.TBPHS.bit.TBPHS           = 2;
    EPwm6Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm6Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm6Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)
    EPwm6Regs.TBCTL.bit.SYNCOSEL        = TB_SYNC_IN;

    EPwm6Regs.TBCTL.bit.PHSEN           = TB_DISABLE;
    EPwm6Regs.TBCTL.bit.PHSDIR          = 1;
    EPwm6Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm6Regs.TBCTR                     = 0;
	EPwm6Regs.CMPA.bit.CMPA             = 0;               //Duty = 0% at the beginning
	EPwm6Regs.CMPB.bit.CMPB             = 0;
	EPwm6Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
	EPwm6Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
	EPwm6Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_PRD;      //Load compare A register when counter = zero or period
	EPwm6Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_PRD;      //Load compare B register when counter = zero or period

	EPwm6Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
	EPwm6Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
	EPwm6Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
	EPwm6Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

	EPwm6Regs.ETSEL.bit.SOCAEN          = 1;               //enable PWM7SOCA
    EPwm6Regs.CMPB.bit.CMPB             = 50;
    EPwm6Regs.ETSEL.bit.SOCASEL         = ET_CTRU_CMPB;    //Enable event time-base counter count up and = compare B
	EPwm6Regs.ETPS.bit.SOCAPRD          = ET_1ST;          //Generate the EPWMxSOCA pulse on the first event

	EALLOW;
	EPwm6Regs.TZSEL.bit.OSHT1           = TZ_ENABLE;
	EPwm6Regs.TZSEL.bit.OSHT2           = TZ_ENABLE;
	EPwm6Regs.TZSEL.bit.OSHT3           = TZ_ENABLE;
	EPwm6Regs.TZCTL.bit.TZA             = TZ_FORCE_LO;
	EPwm6Regs.TZCTL.bit.TZB             = TZ_FORCE_LO;
	EPwm6Regs.TZFRC.bit.OST             = 1;               //Disable PWM at first
	EDIS;

	EPwm6Regs.ETSEL.bit.INTSEL          = ET_CTR_PRDZERO;  //Interrupt when counter = zero or period
	EPwm6Regs.ETPS.bit.INTPRD           = ET_1ST;          //Interrupt generate on the first time
	EPwm6Regs.ETSEL.bit.INTEN           = ET_DISABLE;      //disable PWM interrupt

    /* Boost2 ePWM generator */
    EPwm7Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm7Regs.TBPRD                     = BOOST_PWM_PERD;  //set the PWM period
    EPwm7Regs.TBPHS.bit.TBPHS           = BOOST_PWM_PERD;
    EPwm7Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm7Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm7Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)
    EPwm7Regs.TBCTL.bit.SYNCOSEL        = TB_SYNC_IN;

    EPwm7Regs.TBCTL.bit.PHSEN           = TB_ENABLE;
    EPwm7Regs.TBCTL.bit.PHSDIR          = 1;
    EPwm7Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm7Regs.TBCTR                     = 0;
    EPwm7Regs.CMPA.bit.CMPA             = 0;               //Duty = 0% at the beginning
    EPwm7Regs.CMPB.bit.CMPB             = 0;
    EPwm7Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
    EPwm7Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
    EPwm7Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_PRD;      //Load compare A register when counter = zero or period
    EPwm7Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_PRD;      //Load compare B register when counter = zero or period

    EPwm7Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
    EPwm7Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
    EPwm7Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
    EPwm7Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

    EPwm7Regs.ETSEL.bit.SOCAEN          = 1;               //enable PWMxSOCA
    EPwm7Regs.CMPB.bit.CMPB             = 50;
    EPwm7Regs.ETSEL.bit.SOCASEL         = ET_CTRU_CMPB;    //Enable event time-base counter count up and = compare B
    EPwm7Regs.ETPS.bit.SOCAPRD          = ET_1ST;          //Generate the EPWMxSOCA pulse on the first event

    EALLOW;
    EPwm7Regs.TZSEL.bit.OSHT1           = TZ_ENABLE;
    EPwm7Regs.TZSEL.bit.OSHT2           = TZ_ENABLE;
    EPwm7Regs.TZSEL.bit.OSHT3           = TZ_ENABLE;
    EPwm7Regs.TZCTL.bit.TZA             = TZ_FORCE_LO;
    EPwm7Regs.TZCTL.bit.TZB             = TZ_FORCE_LO;
    EPwm7Regs.TZFRC.bit.OST             = 1;               //Disable PWM at first
    EDIS;

    EPwm7Regs.ETSEL.bit.INTSEL          = ET_CTR_PRDZERO;  //Interrupt when counter = zero or period
    EPwm7Regs.ETPS.bit.INTPRD           = ET_1ST;          //Interrupt generate on the first time
    EPwm7Regs.ETSEL.bit.INTEN           = ET_DISABLE;      //disable PWM interrupt

    //--------------------------------------------------------------------------------
    /*********************32K倍频---EPWM配置作为ADC触发使用->逆变器电压电流*********************/
    EALLOW;
    SyncSocRegs.SYNCSELECT.bit.EPWM10SYNCIN = 0;            //时钟同步到EPWM1->INV
    EDIS;

    EPwm10Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm10Regs.TBPRD                     = INV_PWM_PERD>>1; //set the PWM period
    EPwm10Regs.TBPHS.bit.TBPHS           = 0;
    EPwm10Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm10Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm10Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)

    EPwm10Regs.TBCTL.bit.PHSEN           = TB_ENABLE;       //Master, no need phase load
    EPwm10Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm10Regs.TBCTR                     = 0;
    EPwm10Regs.CMPA.bit.CMPA             = INV_PWM_PERD>>2; //Duty = 0% at the beginning
    EPwm10Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
    EPwm10Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
    EPwm10Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_ZERO;     //Load compare A register when counter = zero or period
    EPwm10Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_ZERO;     //Load compare B register when counter = zero or period

    //比较点的动作
    EPwm10Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
    EPwm10Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
    EPwm10Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
    EPwm10Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

    //TEST-EPWM10A开波,保证EPWM10触发和逆变器发波时钟一致:
    //死区设置
    EPwm10Regs.DBCTL.bit.IN_MODE         = DBA_ALL;
    EPwm10Regs.DBCTL.bit.POLSEL          = DB_ACTV_HIC;
    EPwm10Regs.DBCTL.bit.OUT_MODE        = DB_FULL_ENABLE;  //enable inverter PWM deadband control
    EPwm10Regs.DBRED.bit.DBRED           = DB_1US;
    EPwm10Regs.DBFED.bit.DBFED           = DB_1US;

    EPwm10Regs.ETSEL.bit.SOCAEN          = 1;               //Enable PWM10SOCA
    EPwm10Regs.CMPB.bit.CMPB             = 250;
    EPwm10Regs.ETSEL.bit.SOCASEL         = ET_CTRU_CMPB;    //Enable event time-base counter count up and = comapre B
    EPwm10Regs.ETPS.bit.SOCAPRD          = ET_1ST;          //Generate the EPWMxSOCA pulse on the first event

    EPwm10Regs.ETSEL.bit.INTSEL          = ET_CTR_ZERO;     //Interrupt when counter = zero
    EPwm10Regs.ETPS.bit.INTPRD           = ET_1ST;          //Interrupt generate on the first time
    EPwm10Regs.ETSEL.bit.INTEN           = ET_DISABLE;      //disable PWM interrupt

    //--------------------------------------------------------------------------------
    /*驱动电源的PWM-Driver power ePWM generator*/
    EPwm11Regs.TBCTL.bit.PRDLD           = TB_IMMEDIATE;
    EPwm11Regs.TBPRD                     = DRV_PWM_PERD;    //set the PWM period
    EPwm11Regs.TBPHS.bit.TBPHS           = 2;
    EPwm11Regs.TBCTL.bit.FREE_SOFT       = 2;               //Free run
    EPwm11Regs.TBCTL.bit.CLKDIV          = TB_DIV1;
    EPwm11Regs.TBCTL.bit.HSPCLKDIV       = TB_DIV1;         //TBCLK = SYS_CLK/(CLKDIV * HSPCLKDIV)
    EPwm11Regs.TBCTL.bit.SYNCOSEL        = TB_SYNC_IN;

    EPwm11Regs.TBCTL.bit.PHSEN           = TB_DISABLE;      //独立主机不载入相位
    EPwm11Regs.TBCTL.bit.PHSDIR          = 1;
    EPwm11Regs.TBCTL.bit.CTRMODE         = TB_COUNT_UPDOWN; //Count up down mode
    EPwm11Regs.TBCTR                     = 0;
    EPwm11Regs.CMPA.bit.CMPA             = EPwm11Regs.TBPRD>>1;
    EPwm11Regs.CMPB.bit.CMPB             = 0;
    EPwm11Regs.CMPCTL.bit.SHDWAMODE      = CC_SHADOW;       //Using shadow
    EPwm11Regs.CMPCTL.bit.SHDWBMODE      = CC_SHADOW;       //Using shadow
    EPwm11Regs.CMPCTL.bit.LOADAMODE      = CC_CTR_PRD;      //Load compare A register when counter = zero or period
    EPwm11Regs.CMPCTL.bit.LOADBMODE      = CC_CTR_PRD;      //Load compare B register when counter = zero or period

    EPwm11Regs.AQCTLA.bit.CAU            = AQ_CLEAR;        //Force 0 when counter count up and = compare A
    EPwm11Regs.AQCTLA.bit.CAD            = AQ_SET;          //Force 1 when counter count down and = compare A
    EPwm11Regs.AQCTLA.bit.ZRO            = AQ_NO_ACTION;    //Do nothing at equal to zero
    EPwm11Regs.AQCTLA.bit.PRD            = AQ_NO_ACTION;    //Do nothing at period

    EPwm11Regs.DBCTL.bit.IN_MODE         = DBA_ALL;
    EPwm11Regs.DBCTL.bit.POLSEL          = DB_ACTV_HIC;
    EPwm11Regs.DBCTL.bit.OUT_MODE        = DB_FULL_ENABLE;  // enable inverter PWM deadband control
    EPwm11Regs.DBRED.bit.DBRED           = 0;
    EPwm11Regs.DBFED.bit.DBFED           = 0;

    EPwm11Regs.TZCLR.bit.OST             = 1;               //enable PWM at first

    //--------------------------------------------------------------------------------
	EALLOW;
	CpuSysRegs.PCLKCR0.bit.TBCLKSYNC     = 1;               //Start all the timers synced
	EDIS;
}