This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: 芯片的应用问题

Part Number: TMS320F280025

汽车空调热泵项目当前是400V、800V系统,后面可能升级到1500V的应用

当前280025的应用,后期可能需要升级资源,比如主频当前80M可能要升级到100  120M  存储资源增加  还最好有OTA功能,需要推荐一个性价比高的?

当前280025是否可以同时支持CAN和LIN接口,具体怎么使用?

PIN32、PIN27 GPIO口配置下拉后,晶振不能起振,配置悬空就可以起振,所以PIN 3、4、7、10、25等目前配置都是下拉,是否会影响芯片其它功能?

PIN 10是否可以用来做AD口,规格书上说是做模拟输入?