This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有關SPI的問題



我想問一下,如果我現在,有多個模塊需要使用SPI,但是GPIO口所定義的給SPI的口只有GPIO16——19,我想問一下如何才能解決這個問題,球大神指教!小弟感激不盡,謝謝了!!!

  • 還想問一個問題,我看USER's GUIDE 上面的介紹,比如說,GPIO18上有SPICLKA、SCITXDA、XCLKOUT和普通功能,這四種,如果我使用了SPI設定了一個,又需要使用SCI那應該如何使用和定義,我使用的F28027。謝謝了!

  • 第一:F28027只有一个SPI模块,所以如果需要很多个SPI模块,就只能通过I/O口进行模拟

    第二:F28027有一个SCI,一个SPI模块,SCI的RX,TX引脚可以配置映射为GPOI 18, 19也可以配置映射为GPIO7 GPIO12,而SPI只能配置映射为GPIO16-19,所以SCI和SPI可以同时使用。详细可见F28027 datasheet 第11页