我想問一下,如果我現在,有多個模塊需要使用SPI,但是GPIO口所定義的給SPI的口只有GPIO16——19,我想問一下如何才能解決這個問題,球大神指教!小弟感激不盡,謝謝了!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想問一下,如果我現在,有多個模塊需要使用SPI,但是GPIO口所定義的給SPI的口只有GPIO16——19,我想問一下如何才能解決這個問題,球大神指教!小弟感激不盡,謝謝了!!!
第一:F28027只有一个SPI模块,所以如果需要很多个SPI模块,就只能通过I/O口进行模拟
第二:F28027有一个SCI,一个SPI模块,SCI的RX,TX引脚可以配置映射为GPOI 18, 19也可以配置映射为GPIO7 GPIO12,而SPI只能配置映射为GPIO16-19,所以SCI和SPI可以同时使用。详细可见F28027 datasheet 第11页