This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
利用两个epwm模块 epwm1A和 epwm2A。epwm1A设置为同步信号输出,epwm2A接收epwm1A的同步信号。当epwm1A的PRD改变时,CMA变为0.1*PRD。epwm2A的PRD跟随epwm1A变化,CMA也是0.1*PRD。而此过程,epwm1A与epwm2A的相对相移需要一直保持恒定。
正常情况如下,这是我需要的波形。注意绿色为1A,黄色为2A,后面的波形都是以此情况。
但是在运行过程中,它会周期性出现以下两种波形,这是为什么?
只有当我的PRD由小变大的时候才出现,而PRD由大变小一切正常。如下图。
代码配置如下
初始化PWM
改变PRD,CMA,PHS代码如下
你好,非常感谢你的回复,我明确配置了EPWM1的装载方式,问题仍然存在。根据手册,利用寄存器LINK,问题也没有解决。代码如下。
// // Included Files // #include "driverlib.h" #include "device.h" __interrupt void cpuTimer0ISR(void); void initCPUTimers(void); void configCPUTimer(uint32_t cpuTimer, float freq, float period); void pin_init(void); void init_PWM(void); #define myEPWM1_BASE EPWM1_BASE #define myEPWM2_BASE EPWM2_BASE uint32_t epwm_period1 = 1000; uint32_t epwm_compare1 = 100; uint32_t epwm_shift = 500; // // Main // void main(void) { // // Initializes device clock and peripherals // Device_init(); // // Initializes PIE and clears PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initializes the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC); pin_init(); init_PWM(); initCPUTimers(); // // Configure CPU-Timer 0, // configCPUTimer(CPUTIMER0_BASE, DEVICE_SYSCLK_FREQ, 100); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC); // // ISRs for each CPU Timer interrupt // Interrupt_register(INT_TIMER0, &cpuTimer0ISR); // // Enables CPU int1 which are connected to CPU-Timer 0. // Enable TINT0 in the PIE: Group 1 interrupt 7 // Interrupt_enable(INT_TIMER0); // // Starts CPU-Timer 0. // CPUTimer_startTimer(CPUTIMER0_BASE); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; while(1) { } } __interrupt void cpuTimer0ISR(void) { if(epwm_period1 == 1000) { epwm_period1 = 100; epwm_compare1 = 10; epwm_shift = 50; //updata epwm1 and epwm2 CMA HWREG(0X0000406B)=epwm_compare1; HWREG(0X0000416B)=epwm_compare1; //updata epwm1 and epwm2 PRD HWREG(0X00004063)=epwm_period1; HWREG(0X00004163)=epwm_period1; //updata epwm2 PHS HWREG(0X00004161)=epwm_shift; } else if(epwm_period1 == 100) { epwm_period1 = 1000; epwm_compare1 = 100; epwm_shift = 500; //updata epwm1 and epwm2 PRD HWREG(0X00004063)=epwm_period1; HWREG(0X00004163)=epwm_period1; //updata epwm1 and epwm2 CMA HWREG(0X0000406B)=epwm_compare1; HWREG(0X0000416B)=epwm_compare1; //updata epwm2 PHS HWREG(0X00004161)=epwm_shift; } // // Acknowledge this interrupt to receive more interrupts from group 1 // Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1); } void initCPUTimers(void) { // // Initialize timer period to maximum // CPUTimer_setPeriod(CPUTIMER0_BASE, 0xFFFFFFFF); // // Initialize pre-scale counter to divide by 1 (SYSCLKOUT) // CPUTimer_setPreScaler(CPUTIMER0_BASE, 0); // // Make sure timer is stopped // CPUTimer_stopTimer(CPUTIMER0_BASE); // // Reload all counter register with period value // CPUTimer_reloadTimerCounter(CPUTIMER0_BASE); } void configCPUTimer(uint32_t cpuTimer, float freq, float period) { uint32_t temp; // // Initialize timer period: // temp = (uint32_t)((freq / 1000000) * period); CPUTimer_setPeriod(cpuTimer, temp); // // Set pre-scale counter to divide by 1 (SYSCLKOUT): // CPUTimer_setPreScaler(cpuTimer, 0); // // Initializes timer control register. The timer is stopped, reloaded, // free run disabled, and interrupt enabled. // Additionally, the free and soft bits are set // CPUTimer_stopTimer(cpuTimer); CPUTimer_reloadTimerCounter(cpuTimer); CPUTimer_setEmulationMode(cpuTimer, CPUTIMER_EMULATIONMODE_STOPAFTERNEXTDECREMENT); CPUTimer_enableInterrupt(cpuTimer); } void init_PWM(void) { EPWM_setClockPrescaler(myEPWM1_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); EPWM_setTimeBasePeriod(myEPWM1_BASE, 1000); EPWM_setPeriodLoadMode(myEPWM1_BASE, EPWM_PERIOD_SHADOW_LOAD); EPWM_selectPeriodLoadEvent(myEPWM1_BASE, EPWM_SHADOW_LOAD_MODE_COUNTER_ZERO); EPWM_setTimeBaseCounter(myEPWM1_BASE, 0); EPWM_setTimeBaseCounterMode(myEPWM1_BASE, EPWM_COUNTER_MODE_UP); EPWM_disablePhaseShiftLoad(myEPWM1_BASE); EPWM_setPhaseShift(myEPWM1_BASE, 0); EPWM_enableSyncOutPulseSource(myEPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_CNTR_ZERO); EPWM_setCounterCompareValue(myEPWM1_BASE, EPWM_COUNTER_COMPARE_A, 500); EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareValue(myEPWM1_BASE, EPWM_COUNTER_COMPARE_B, 500); EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setClockPrescaler(myEPWM2_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); EPWM_setTimeBasePeriod(myEPWM2_BASE, 1000); EPWM_setPeriodLoadMode(myEPWM2_BASE, EPWM_PERIOD_SHADOW_LOAD); EPWM_selectPeriodLoadEvent(myEPWM2_BASE, EPWM_SHADOW_LOAD_MODE_COUNTER_SYNC); EPWM_setTimeBaseCounter(myEPWM2_BASE, 0); EPWM_setTimeBaseCounterMode(myEPWM2_BASE, EPWM_COUNTER_MODE_UP); EPWM_enablePhaseShiftLoad(myEPWM2_BASE); EPWM_setPhaseShift(myEPWM2_BASE, 500); EPWM_setSyncInPulseSource(myEPWM2_BASE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1); EPWM_setCounterCompareValue(myEPWM2_BASE, EPWM_COUNTER_COMPARE_A, 500); EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareValue(myEPWM2_BASE, EPWM_COUNTER_COMPARE_B, 500); EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); } void pin_init(void) { GPIO_setPinConfig(GPIO_0_EPWM1_A); GPIO_setPinConfig(GPIO_1_EPWM1_B); GPIO_setPinConfig(GPIO_2_EPWM2_A); GPIO_setPinConfig(GPIO_3_EPWM2_B); } // // End of File //