This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28069内部参考电压

你好,我想请问下,关于28069内部参考电压的问题,由于稳压电路的原因,输入到28069的3.3V实际可能低于3.3V,大概在3.294V左右,想请问下,如果还是采用内部参考电压,具体得到的参考值为多少。我用AD采样的和外部示波器等测量的有一定的误差,采样的值偏高了,是不是内部的参考电压不是3.3V了。谢谢。