This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35 对shared Ram的理解



您好!我想请教下关于F28m35中shared RAM的理解。

1、如果C28向S0 RAM中写程序,M3从该位置读程序,那么就涉及到两个核对RAM的访问。那么这个读写是不是同时发生的?如果不能同时发生,那么在不同的project中如何协调这个读写的过程的呢?

2、另外我想问下,下面程序中语句中&g_sIpcController1是干嘛的?

    IPCMtoCDataWrite(&g_sIpcController1, pulMsgRam[0],(unsigned long)usWWord16,

                     IPC_LENGTH_16_BITS, ENABLE_BLOCKING,

                     NO_FLAG);

3、当我的数据涉及正负,是不是要把例子中unsigned 改成signed?

  • timberrain,

    1,如果两个核同时对shared ram的同一个单元访问,芯片有仲裁的机制,详情可以查看reference guide 5.1.1.4.

    1. M3 CPU Access (RD/WR)

    2. M3 uDMA Access (RD/WR)

    3. C28 CPU Data Read

    4. C28 CPU Write (Data/Progra

    5. C28 CPU Program Fetch/Re

    6. C28 DMA Access (RD/WR)

    2. 这个是在哪个例程中的?双击该变量就可以查看变量的定义。

    3. 是,要将变量编程有符号位。

    -Eric