This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320F28035

Other Parts Discussed in Thread: TMS320F28035

专家你好。

   我做的TMS320F28035的电源项目将要做PCB了,要尽可能地达到合理。因为是第一次和这款芯片打交道所以才有以下初级问题。请谅解。

1、初始状态问题。

手册中说The pullups on the PWM pins are not enabled at reset. The pullups on other GPIO pins are enabled upon reset.。我用的引脚功能是PWM,但它又是GPIO的复用功能,如PNT的69脚,它既是EPWM1A,又是GPIO0,那么在复位时,它到底会怎么样呢?是不是复用功能时,以PWM功能为准;没有PWM功能的GPIO引脚将执行上拉使能?  -----由于用在电源上,初始状态对其很重要。

2、BootROM

SPRS584F中的Table 3-6,提到了与串行口相关的,只有SCI,而在Table 3-7. 中说了Peripheral Bootload Pins有五种,除SCI可以在表六中找到其进入这种模式的方法外,其它如CAN等怎么进入呢?

3、ADC问题。

ADC的两个通道可以同时采样、保持。假如信号S1、S2,在T0时刻同时采样,在T1时刻对S1作ADC转换,结束后,在T2时刻对S2转换。现在的问题是:对于S2,它可以保持这么久而电压不变(或相当小)吗?

谢谢专家