This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335ePWM占空比0%和100%点需要特殊设置,应该怎么实现?

Other Parts Discussed in Thread: TMS320F28335

TMS320F28335在实现PWM波占空比0%~100%变化时了解到占空比不能直接设置为0%或者100%,比如直接设100%的时候会出现向下闪动的信号,应该如何对这两个点进行特殊设置?谢谢!

  • 请参考文献:

    Using the ePWM Module for 0% - 100%Duty Cycle Control【spraai1】

  • 计数器计数方向是上升下降计数还是上升计数还是下降计数。输出高低电平方面怎么进行set 和reset 的.

  • 这是我用的子程序,用的是上升计数的

    PWMA_below,  pwma分母

    PWMA_above, pwma分子

    PWMB_below, pwmb分母

    PWMB_above,pwmb分子

    函数是这样定义的:比如说PWMA_below=2,PWMA_above=1,那么设置的占空比是1/2

            void HRPWM1_Config(period,PWMA_below,PWMA_above,PWMB_below,PWMB_above)

    {

             EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;        // set Immediate load  1

    EPwm1Regs.TBPRD = period;                    // PWM frequency = 1 / period  PWM 周期=1/频率

    EPwm1Regs.CMPA.half.CMPA = period / PWMA_below * (PWMA_below - PWMA_above);                  

                        EPwm1Regs.CMPA.half.CMPAHR = (1 << 8);              // initialize HRPWM extension

    EPwm1Regs.CMPB = period / PWMB_below * PWMB_above;                     EPwm1Regs.TBPHS.all = 0;

    EPwm1Regs.TBCTR = 0;

    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;         //计数增模式 用于非对称

    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;          // EPWM1 is the Master

    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;

    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4;           //定时器选择,决定频率的范围

    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV4;

    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;

    EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;

    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;

    EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR;               // PWM toggle low/high

    EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;

    EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;

    EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR;

    EALLOW;

    EPwm1Regs.HRCNFG.all = 0x0;

    EPwm1Regs.HRCNFG.bit.EDGMODE = HR_REP; //MEP control on Rising edge

    EPwm1Regs.HRCNFG.bit.CTLMODE = HR_CMP;

    EPwm1Regs.HRCNFG.bit.HRLOAD  = HR_CTR_ZERO;

    EDIS;

    }

  • 非常谢谢你这么快速的回复,我下载了文档了,很有参考价值,3Q

  • ePwm1.A 和ePwm1.B互补输出  配置成互补形式

    EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR;               // PWM toggle low/high

    EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;

    EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET;

    EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR;

    改成

    EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET;               // PWM toggle low/high

    EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;  

    EPwm1Regs.AQCTLB.bit.ZRO = AQ_CLEAR;  

    EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;

    需要输出满占空比时,比较值应该写入一个period大的值,如:period+1,这一操作可以通过软件来进行设计

    这样更改之后 比较值也需要做相应改变。