This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812DSPBIOS 烧写报错 求助 急!



目前使用的CCS版本是3.3.81.6  其中BIOS已经升级到5.33.06版本  使用的DSP是2812。 程序编译没有错误,cmd文件根据TI例程以及spra958h文件改写,在烧写结束时报了一个warning导致烧写失败,此时带仿真器可以运行但是断电后无法运行,warning如下:

warning: this program contains initialized RAM data.It may run successfully under code composer studio, but not as a standalone system because of this.if you flashprogram requires initialized data in RAM. you will need to write flash code to initialize RAM memory.

程序使用BIOS 因此包含了三个cmd文件,如下:希望专家以及同僚帮我看看是否有问题

(1)DSP281x_Headers_BIOS.cmd

MEMORY

{

PAGE 0:    /* Program Memory */

PAGE 1:    /* Data Memory */

  DEV_EMU     : origin = 0x000880, length = 0x000180     /* device emulation registers */

  FLASH_REGS  : origin = 0x000A80, length = 0x000060     /* FLASH registers */

  CSM         : origin = 0x000AE0, length = 0x000010     /* code security module registers */

  XINTF       : origin = 0x000B20, length = 0x000020     /* external interface registers */

  CPU_TIMER0  : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */

  CPU_TIMER1  : origin = 0x000C08, length = 0x000008     /* CPU Timer1 registers */

  CPU_TIMER2  : origin = 0x000C10, length = 0x000008     /* CPU Timer2 registers (CPU Timer2 reserved for BIOS)*/

  PIE_CTRL    : origin = 0x000CE0, length = 0x000020     /* PIE control registers */

  ECANA       : origin = 0x006000, length = 0x000040     /* eCAN control and status registers */

  ECANA_LAM   : origin = 0x006040, length = 0x000040     /* eCAN local acceptance masks */

  ECANA_MOTS  : origin = 0x006080, length = 0x000040     /* eCAN message object time stamps */

  ECANA_MOTO  : origin = 0x0060C0, length = 0x000040     /* eCAN object time-out registers */

  ECANA_MBOX  : origin = 0x006100, length = 0x000100     /* eCAN mailboxes */

  SYSTEM      : origin = 0x007010, length = 0x000020     /* System control registers */

  SPIA        : origin = 0x007040, length = 0x000010     /* SPI registers */

  SCIA        : origin = 0x007050, length = 0x000010     /* SCI-A registers */

  XINTRUPT    : origin = 0x007070, length = 0x000010     /* external interrupt registers */

  GPIOMUX     : origin = 0x0070C0, length = 0x000020     /* GPIO mux registers */

  GPIODAT     : origin = 0x0070E0, length = 0x000020     /* GPIO data registers */

  ADC         : origin = 0x007100, length = 0x000020     /* ADC registers */

  EVA         : origin = 0x007400, length = 0x000040     /* Event Manager A registers */

  EVB         : origin = 0x007500, length = 0x000040     /* Event Manager B registers */

  SCIB        : origin = 0x007750, length = 0x000010     /* SCI-B registers */

  MCBSPA      : origin = 0x007800, length = 0x000040     /* McBSP registers */

  CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations. */

}

SECTIONS

{

/*** The PIE Vector table is called PIEVECT by DSP/BIOS ***/

  PieVectTableFile  : > PIEVECT,     PAGE = 1,  TYPE = DSECT

/*** Peripheral Frame 0 Register Structures ***/

  DevEmuRegsFile    : > DEV_EMU,     PAGE = 1

  FlashRegsFile     : > FLASH_REGS,  PAGE = 1

  CsmRegsFile       : > CSM,         PAGE = 1

  XintfRegsFile     : > XINTF,       PAGE = 1

  CpuTimer0RegsFile : > CPU_TIMER0,  PAGE = 1  

  CpuTimer1RegsFile : > CPU_TIMER1,  PAGE = 1  

  CpuTimer2RegsFile : > CPU_TIMER2,  PAGE = 1  

  PieCtrlRegsFile   : > PIE_CTRL,    PAGE = 1

/*** Peripheral Frame 1 Register Structures ***/

  ECanaRegsFile     : > ECANA,       PAGE = 1

  ECanaLAMRegsFile  : > ECANA_LAM    PAGE = 1  

  ECanaMboxesFile   : > ECANA_MBOX   PAGE = 1

  ECanaMOTSRegsFile : > ECANA_MOTS   PAGE = 1

  ECanaMOTORegsFile : > ECANA_MOTO   PAGE = 1

/*** Peripheral Frame 2 Register Structures ***/

  SysCtrlRegsFile   : > SYSTEM,      PAGE = 1

  SpiaRegsFile      : > SPIA,        PAGE = 1

  SciaRegsFile      : > SCIA,        PAGE = 1

  XIntruptRegsFile  : > XINTRUPT,    PAGE = 1

  GpioMuxRegsFile   : > GPIOMUX,     PAGE = 1

  GpioDataRegsFile  : > GPIODAT      PAGE = 1

  AdcRegsFile       : > ADC,         PAGE = 1

  EvaRegsFile       : > EVA,         PAGE = 1

  EvbRegsFile       : > EVB,         PAGE = 1

  ScibRegsFile      : > SCIB,        PAGE = 1

  McbspaRegsFile    : > MCBSPA,      PAGE = 1

/*** Code Security Module Register Structures ***/

  CsmPwlFile        : > CSM_PWL,     PAGE = 1

}

(2)F2812_BIOS_1.cmd  用户定义的cmd

SECTIONS

{

/*** User Defined Sections ***/

  codestart         : > BEGIN_FLASH,               PAGE = 0                /* Used by file CodeStartBranch.asm */

  internalMemFuncs  : > FLASH_ABCDEFGHIJ,          PAGE = 0                /* Used by file Xintf.c.  Link to internal memory */

  csm_rsvd          : > CSM_RSVD,                  PAGE = 0         /* Used by file Passwords.asm */

  passwords         : > PASSWORDS,                 PAGE = 0         /* Used by file Passwords.asm */

  DSP1SRFile        : > DSP1REG,                   PAGE = 1

  secureRamFuncs    :   LOAD = FLASH_ABCDEFGHIJ,   PAGE = 0         /* Used by file Flash.c */

                        RUN = L0SARAM,             PAGE = 0         /* Load to flash, run from CSM secure RAM */

                        LOAD_START(_secureRamFuncs_loadstart),

                        LOAD_SIZE(_secureRamFuncs_loadsize),

                        RUN_START(_secureRamFuncs_runstart)

  IQmathTables      : > IQTABLES                   PAGE = 0, TYPE = NOLOAD

  IQmath            : > FLASH_ABCDEFGHIJ           PAGE = 0

}

(3)BIOS自动生成的cmd:

-u _FXN_F_nop

GBL_USERLIMPMODEABORTFXN = _FXN_F_nop;

-u _UserInit

GBL_USERINITFXN = _UserInit;

-u L1SARAM

MEM_SEGZERO = L1SARAM;

-u L1SARAM

MEM_MALLOCSEG = L1SARAM;

-u CLK_F_getshtime

CLK_TIMEFXN = CLK_F_getshtime;

-u CLK_F_run

CLK_HOOKFXN = CLK_F_run;

-u KNL_tick_stub

PRD_THOOKFXN = KNL_tick_stub;

-u L1SARAM

RTDX_DATAMEMSEG = L1SARAM;

-u L1SARAM

HST_DSMBUFSEG = L1SARAM;

-u GBL_NULL

SWI_EHOOKFXN = GBL_NULL;

-u GBL_NULL

SWI_IHOOKFXN = GBL_NULL;

-u SWI_F_exec

SWI_EXECFXN = SWI_F_exec;

-u SWI_F_run

SWI_RUNFXN = SWI_F_run;

-u L1SARAM

TSK_STACKSEG = L1SARAM;

-u _FXN_F_nop

TSK_VCREATEFXN = _FXN_F_nop;

-u _FXN_F_nop

TSK_VDELETEFXN = _FXN_F_nop;

-u _FXN_F_nop

TSK_VEXITFXN = _FXN_F_nop;

-u IDL_F_stub

IDL_CALIBRFXN = IDL_F_stub;

-u _UTL_doAbort

SYS_ABORTFXN = _UTL_doAbort;

-u _UTL_doError

SYS_ERRORFXN = _UTL_doError;

-u _UTL_halt

SYS_EXITFXN = _UTL_halt;

-u _UTL_doPutc

SYS_PUTCFXN = _UTL_doPutc;

-u _FXN_F_nop

GIO_CREATEFXN = _FXN_F_nop;

-u _FXN_F_nop

GIO_DELETEFXN = _FXN_F_nop;

-u _FXN_F_nop

GIO_PENDFXN = _FXN_F_nop;

-u _FXN_F_nop

GIO_POSTFXN = _FXN_F_nop;

/* OBJECT ALIASES */

_PIEVECT = PIEVECT;

_OTP = OTP;

_H0SARAM = H0SARAM;

_L1SARAM = L1SARAM;

_L0SARAM = L0SARAM;

_M1SARAM = M1SARAM;

_M0SARAM = M0SARAM;

_ZONE6 = ZONE6;

_PASSWORDS = PASSWORDS;

_BEGIN_H0 = BEGIN_H0;

_BEGIN_FLASH = BEGIN_FLASH;

_FLASH_ABCDEFGHIJ = FLASH_ABCDEFGHIJ;

_CSM_RSVD = CSM_RSVD;

_IQTABLES = IQTABLES;

_DSP1REG = DSP1REG;

_ZONE1 = ZONE1;

_PRD_clock = PRD_clock;

_PRD0 = PRD0;

_RTA_fromHost = RTA_fromHost;

_RTA_toHost = RTA_toHost;

_HWI_RESET = HWI_RESET;

_HWI_INT1 = HWI_INT1;

_HWI_INT2 = HWI_INT2;

_HWI_INT3 = HWI_INT3;

_HWI_INT4 = HWI_INT4;

_HWI_INT5 = HWI_INT5;

_HWI_INT6 = HWI_INT6;

_HWI_INT7 = HWI_INT7;

_HWI_INT8 = HWI_INT8;

_HWI_INT9 = HWI_INT9;

_HWI_INT10 = HWI_INT10;

_HWI_INT11 = HWI_INT11;

_HWI_INT12 = HWI_INT12;

_HWI_INT13 = HWI_INT13;

_HWI_TINT = HWI_TINT;

_HWI_DLOG = HWI_DLOG;

_HWI_RTOS = HWI_RTOS;

_HWI_RESERVED = HWI_RESERVED;

_HWI_NMI = HWI_NMI;

_HWI_ILLEGAL = HWI_ILLEGAL;

_HWI_USER1 = HWI_USER1;

_HWI_USER2 = HWI_USER2;

_HWI_USER3 = HWI_USER3;

_HWI_USER4 = HWI_USER4;

_HWI_USER5 = HWI_USER5;

_HWI_USER6 = HWI_USER6;

_HWI_USER7 = HWI_USER7;

_HWI_USER8 = HWI_USER8;

_HWI_USER9 = HWI_USER9;

_HWI_USER10 = HWI_USER10;

_HWI_USER11 = HWI_USER11;

_HWI_USER12 = HWI_USER12;

_PIE_INT1_1 = PIE_INT1_1;

_PIE_INT1_2 = PIE_INT1_2;

_PIE_INT1_3 = PIE_INT1_3;

_PIE_INT1_4 = PIE_INT1_4;

_PIE_INT1_5 = PIE_INT1_5;

_PIE_INT1_6 = PIE_INT1_6;

_PIE_INT1_7 = PIE_INT1_7;

_PIE_INT1_8 = PIE_INT1_8;

_PIE_INT2_1 = PIE_INT2_1;

_PIE_INT2_2 = PIE_INT2_2;

_PIE_INT2_3 = PIE_INT2_3;

_PIE_INT2_4 = PIE_INT2_4;

_PIE_INT2_5 = PIE_INT2_5;

_PIE_INT2_6 = PIE_INT2_6;

_PIE_INT2_7 = PIE_INT2_7;

_PIE_INT2_8 = PIE_INT2_8;

_PIE_INT3_1 = PIE_INT3_1;

_PIE_INT3_2 = PIE_INT3_2;

_PIE_INT3_3 = PIE_INT3_3;

_PIE_INT3_4 = PIE_INT3_4;

_PIE_INT3_5 = PIE_INT3_5;

_PIE_INT3_6 = PIE_INT3_6;

_PIE_INT3_7 = PIE_INT3_7;

_PIE_INT3_8 = PIE_INT3_8;

_PIE_INT4_1 = PIE_INT4_1;

_PIE_INT4_2 = PIE_INT4_2;

_PIE_INT4_3 = PIE_INT4_3;

_PIE_INT4_4 = PIE_INT4_4;

_PIE_INT4_5 = PIE_INT4_5;

_PIE_INT4_6 = PIE_INT4_6;

_PIE_INT4_7 = PIE_INT4_7;

_PIE_INT4_8 = PIE_INT4_8;

_PIE_INT5_1 = PIE_INT5_1;

_PIE_INT5_2 = PIE_INT5_2;

_PIE_INT5_3 = PIE_INT5_3;

_PIE_INT5_4 = PIE_INT5_4;

_PIE_INT5_5 = PIE_INT5_5;

_PIE_INT5_6 = PIE_INT5_6;

_PIE_INT5_7 = PIE_INT5_7;

_PIE_INT5_8 = PIE_INT5_8;

_PIE_INT6_1 = PIE_INT6_1;

_PIE_INT6_2 = PIE_INT6_2;

_PIE_INT6_3 = PIE_INT6_3;

_PIE_INT6_4 = PIE_INT6_4;

_PIE_INT6_5 = PIE_INT6_5;

_PIE_INT6_6 = PIE_INT6_6;

_PIE_INT6_7 = PIE_INT6_7;

_PIE_INT6_8 = PIE_INT6_8;

_PIE_INT7_1 = PIE_INT7_1;

_PIE_INT7_2 = PIE_INT7_2;

_PIE_INT7_3 = PIE_INT7_3;

_PIE_INT7_4 = PIE_INT7_4;

_PIE_INT7_5 = PIE_INT7_5;

_PIE_INT7_6 = PIE_INT7_6;

_PIE_INT7_7 = PIE_INT7_7;

_PIE_INT7_8 = PIE_INT7_8;

_PIE_INT8_1 = PIE_INT8_1;

_PIE_INT8_2 = PIE_INT8_2;

_PIE_INT8_3 = PIE_INT8_3;

_PIE_INT8_4 = PIE_INT8_4;

_PIE_INT8_5 = PIE_INT8_5;

_PIE_INT8_6 = PIE_INT8_6;

_PIE_INT8_7 = PIE_INT8_7;

_PIE_INT8_8 = PIE_INT8_8;

_PIE_INT9_1 = PIE_INT9_1;

_PIE_INT9_2 = PIE_INT9_2;

_PIE_INT9_3 = PIE_INT9_3;

_PIE_INT9_4 = PIE_INT9_4;

_PIE_INT9_5 = PIE_INT9_5;

_PIE_INT9_6 = PIE_INT9_6;

_PIE_INT9_7 = PIE_INT9_7;

_PIE_INT9_8 = PIE_INT9_8;

_PIE_INT10_1 = PIE_INT10_1;

_PIE_INT10_2 = PIE_INT10_2;

_PIE_INT10_3 = PIE_INT10_3;

_PIE_INT10_4 = PIE_INT10_4;

_PIE_INT10_5 = PIE_INT10_5;

_PIE_INT10_6 = PIE_INT10_6;

_PIE_INT10_7 = PIE_INT10_7;

_PIE_INT10_8 = PIE_INT10_8;

_PIE_INT11_1 = PIE_INT11_1;

_PIE_INT11_2 = PIE_INT11_2;

_PIE_INT11_3 = PIE_INT11_3;

_PIE_INT11_4 = PIE_INT11_4;

_PIE_INT11_5 = PIE_INT11_5;

_PIE_INT11_6 = PIE_INT11_6;

_PIE_INT11_7 = PIE_INT11_7;

_PIE_INT11_8 = PIE_INT11_8;

_PIE_INT12_1 = PIE_INT12_1;

_PIE_INT12_2 = PIE_INT12_2;

_PIE_INT12_3 = PIE_INT12_3;

_PIE_INT12_4 = PIE_INT12_4;

_PIE_INT12_5 = PIE_INT12_5;

_PIE_INT12_6 = PIE_INT12_6;

_PIE_INT12_7 = PIE_INT12_7;

_PIE_INT12_8 = PIE_INT12_8;

_PRD_swi = PRD_swi;

_KNL_swi = KNL_swi;

_TSK_idle = TSK_idle;

_IDL_cpuLoad = IDL_cpuLoad;

_LNK_dataPump = LNK_dataPump;

_RTA_dispatcher = RTA_dispatcher;

_IDL0 = IDL0;

_IDL1 = IDL1;

_IDL2 = IDL2;

_LOG_system = LOG_system;

_trace = trace;

_IDL_busyObj = IDL_busyObj;

/* MODULE GBL */

SECTIONS {

  .vers (COPY): {} /* version information */

}

-priority

-llnkrtdx.a28L

-ldrivers.a28L         /* device drivers support */

-lsioboth.a28L         /* supports both SIO models */

-lbios.a28L            /* DSP/BIOS support */

-lrtdxx.lib            /* RTDX support */

-lrts2800_ml.lib       /* C and C++ run-time library support */

/* MODULE MEM */

-stack 0x200

MEMORY {

  PAGE 1:   PIEVECT:    origin = 0xd00,         len = 0x100

  PAGE 0:   OTP:        origin = 0x3d7800,      len = 0x400

  PAGE 1:   H0SARAM:    origin = 0x3f8002,      len = 0x1ffe

  PAGE 1:   L1SARAM:    origin = 0x9000,        len = 0x1000

  PAGE 0:   L0SARAM:    origin = 0x8000,        len = 0x1000

  PAGE 1:   M1SARAM:    origin = 0x400,         len = 0x400

  PAGE 1:   M0SARAM:    origin = 0x0,           len = 0x400

  PAGE 1:   ZONE6:      origin = 0x100000,      len = 0x10000

  PAGE 0:   PASSWORDS:  origin = 0x3f7ff8,      len = 0x8

  PAGE 0:   BEGIN_H0:   origin = 0x3f8000,      len = 0x2

  PAGE 0:   BEGIN_FLASH: origin = 0x3f7ff6,     len = 0x2

  PAGE 0:   FLASH_ABCDEFGHIJ: origin = 0x3d8000, len = 0x1ff80

  PAGE 0:   CSM_RSVD:   origin = 0x3f7f80,      len = 0x76

  PAGE 0:   IQTABLES:   origin = 0x3ff000,      len = 0xb50

  PAGE 1:   DSP1REG:    origin = 0x5000,        len = 0x2d

  PAGE 1:   ZONE1:      origin = 0x502d,        len = 0x97

}

/* MODULE CLK */

SECTIONS {

  .clk: {

       CLK_F_gethtime = CLK_F_getshtime;

       *(.clk)

  } > L1SARAM  PAGE 1, RUN_START(CLK_A_TABBEG)

}

_CLK_PRD = CLK_PRD;

_CLK_COUNTSPMS = CLK_COUNTSPMS;

_CLK_REGS = CLK_REGS;

_CLK_USETIMER = CLK_USETIMER;

_CLK_TIMERNUM = CLK_TIMERNUM;

_CLK_TCR = CLK_TCR;

_CLK_TDDR = CLK_TDDR;

/* MODULE PRD */

SECTIONS {

  .prd: RUN_START(PRD_A_TABBEG), RUN_END(PRD_A_TABEND) {

  } > L1SARAM PAGE 1

}

PRD_A_TABLEN = 1;

/* MODULE RTDX */

_RTDX_interrupt_mask = 0x0;

/* MODULE SWI */

SECTIONS {

  .swi: RUN_START(SWI_A_TABBEG), RUN_END(SWI_A_TABEND) {

  } > L1SARAM PAGE 1

}

SWI_A_TABLEN = 2;

/* MODULE TSK */

SECTIONS {

  .tsk: {

       *(.tsk)

  } > L1SARAM PAGE 1

}

/* MODULE IDL */

SECTIONS {

  .idl: {

       *(.idl)

  } > L1SARAM PAGE 1, RUN_START(IDL_A_TABBEG)

  .idlcal: {

       *(.idlcal)

  } > L1SARAM PAGE 1, RUN_START(IDL_A_CALBEG)

}

LOG_A_TABLEN = 2; _LOG_A_TABLEN = 2;

PIP_A_TABLEN = 2;

SECTIONS {

       frt:    {} > FLASH_ABCDEFGHIJ PAGE 0

       .bios:    {} > FLASH_ABCDEFGHIJ PAGE 0

       .data:    {} > FLASH_ABCDEFGHIJ PAGE 0

       .pinit:   {} > FLASH_ABCDEFGHIJ PAGE 0

       .text:    {} > FLASH_ABCDEFGHIJ PAGE 0

       .cinit:    {} > FLASH_ABCDEFGHIJ PAGE 0

       .const:    {} > FLASH_ABCDEFGHIJ PAGE 0

       .switch:   {} > FLASH_ABCDEFGHIJ PAGE 0

       .gblinit:   {} > FLASH_ABCDEFGHIJ PAGE 0

       .sysinit:   {} > FLASH_ABCDEFGHIJ PAGE 0

       .rtdx_text: {}  > FLASH_ABCDEFGHIJ PAGE 0

       .hwi: {

      /* no HWI stubs are necessary */

      }  > FLASH_ABCDEFGHIJ PAGE 0

       GROUP {

        .econst: {}

        .printf (COPY): {}

       } > FLASH_ABCDEFGHIJ PAGE 0

       .bss:     {} > H0SARAM PAGE 1

       .ebss:     {} > H0SARAM PAGE 1

       .hwi_disp_sec:     {} > H0SARAM PAGE 1

       .sysdata: {} > L1SARAM PAGE 1

       .dsm: {} > L1SARAM PAGE 1

       .mem:  {} > L1SARAM PAGE 1

       .cio:     {} > L1SARAM PAGE 1

       .gio:     {} > L1SARAM PAGE 1

       .sys:     {} > L1SARAM PAGE 1

       .sysregs: {} > L1SARAM PAGE 1

       .rtdx_data: {}  > L1SARAM PAGE 1

       .TSK_idle$stk: {

           *(.TSK_idle$stk)

       } > L1SARAM PAGE 1

       /* LOG_system buffer */

       .LOG_system$buf: align = 0x80 {} > L1SARAM PAGE 1

       /* trace buffer */

       .trace$buf: align = 0x40 {} > L1SARAM PAGE 1

       .args: fill=0 {

           *(.args)

           . += 0x4;

       } > L1SARAM PAGE 1

      /* RTA_fromHost buffer */

      .hst1: align = 0x4 {} > L1SARAM PAGE 1

      /* RTA_toHost buffer */

      .hst0: align = 0x4 {} > L1SARAM PAGE 1

       .trace: fill = 0x0 {

          _SYS_PUTCBEG = .;

          . += 0x200;

          _SYS_PUTCEND = . - 1;

       } > L1SARAM PAGE 1

       .hst: RUN_START(HST_A_TABBEG), RUN_START(_HST_A_TABBEG), RUN_END(HST_A_TABEND), RUN_END(_HST_A_TABEND) {

       } > L1SARAM PAGE 1

       .log: RUN_START(LOG_A_TABBEG), RUN_START(_LOG_A_TABBEG), RUN_END(LOG_A_TABEND), RUN_END(_LOG_A_TABEND) {

       } > L1SARAM PAGE 1

       .pip: RUN_START(PIP_A_TABBEG), RUN_START(_PIP_A_TABBEG), RUN_END(PIP_A_TABEND), RUN_END(_PIP_A_TABEND) {

       } > L1SARAM PAGE 1

       .sts: RUN_START(STS_A_TABBEG), RUN_START(_STS_A_TABBEG), RUN_END(STS_A_TABEND), RUN_END(_STS_A_TABEND) {

       } > L1SARAM PAGE 1

       .trcdata: START(_trcdata_loadstart), END(_trcdata_loadend), SIZE(_trcdata_loadsize), RUN_START(_trcdata_runstart) {

       } load > FLASH_ABCDEFGHIJ PAGE 0, run > L1SARAM PAGE 1

       .L1SARAM$heap: {

           . += 0x200;

       } RUN_START(L1SARAM$B), RUN_START(_L1SARAM_base), RUN_SIZE(L1SARAM$L), RUN_SIZE(_L1SARAM_length) > L1SARAM PAGE 1

       .stack: {

           GBL_stackbeg = .;

           *(.stack)

           GBL_stackend = GBL_stackbeg + 0x200 - 1;

       _HWI_STKBOTTOM = GBL_stackbeg;

           _HWI_STKTOP = (GBL_stackend + 1);

       } > M1SARAM PAGE 1

       .hwi_vec: START(_hwi_vec_loadstart), END(_hwi_vec_loadend), SIZE(_hwi_vec_loadsize), RUN_START(_hwi_vec_runstart) {

      /* no HWI stubs are necessary */

      } load > FLASH_ABCDEFGHIJ PAGE 0, run > PIEVECT PAGE 1

}

这样的错误在网上也有很多,但是针对BIOS的很少,我不知道是CCS设置的问题还是cmd文件的问题希望

在这方面有研究的朋友给予我帮助,谢谢了。