目前使用的CCS版本是3.3.81.6 其中BIOS已经升级到5.33.06版本 使用的DSP是2812。 程序编译没有错误,cmd文件根据TI例程以及spra958h文件改写,在烧写结束时报了一个warning导致烧写失败,此时带仿真器可以运行但是断电后无法运行,warning如下:
warning: this program contains initialized RAM data.It may run successfully under code composer studio, but not as a standalone system because of this.if you flashprogram requires initialized data in RAM. you will need to write flash code to initialize RAM memory.
程序使用BIOS 因此包含了三个cmd文件,如下:希望专家以及同僚帮我看看是否有问题
(1)DSP281x_Headers_BIOS.cmd
MEMORY
{
PAGE 0: /* Program Memory */
PAGE 1: /* Data Memory */
DEV_EMU : origin = 0x000880, length = 0x000180 /* device emulation registers */
FLASH_REGS : origin = 0x000A80, length = 0x000060 /* FLASH registers */
CSM : origin = 0x000AE0, length = 0x000010 /* code security module registers */
XINTF : origin = 0x000B20, length = 0x000020 /* external interface registers */
CPU_TIMER0 : origin = 0x000C00, length = 0x000008 /* CPU Timer0 registers */
CPU_TIMER1 : origin = 0x000C08, length = 0x000008 /* CPU Timer1 registers */
CPU_TIMER2 : origin = 0x000C10, length = 0x000008 /* CPU Timer2 registers (CPU Timer2 reserved for BIOS)*/
PIE_CTRL : origin = 0x000CE0, length = 0x000020 /* PIE control registers */
ECANA : origin = 0x006000, length = 0x000040 /* eCAN control and status registers */
ECANA_LAM : origin = 0x006040, length = 0x000040 /* eCAN local acceptance masks */
ECANA_MOTS : origin = 0x006080, length = 0x000040 /* eCAN message object time stamps */
ECANA_MOTO : origin = 0x0060C0, length = 0x000040 /* eCAN object time-out registers */
ECANA_MBOX : origin = 0x006100, length = 0x000100 /* eCAN mailboxes */
SYSTEM : origin = 0x007010, length = 0x000020 /* System control registers */
SPIA : origin = 0x007040, length = 0x000010 /* SPI registers */
SCIA : origin = 0x007050, length = 0x000010 /* SCI-A registers */
XINTRUPT : origin = 0x007070, length = 0x000010 /* external interrupt registers */
GPIOMUX : origin = 0x0070C0, length = 0x000020 /* GPIO mux registers */
GPIODAT : origin = 0x0070E0, length = 0x000020 /* GPIO data registers */
ADC : origin = 0x007100, length = 0x000020 /* ADC registers */
EVA : origin = 0x007400, length = 0x000040 /* Event Manager A registers */
EVB : origin = 0x007500, length = 0x000040 /* Event Manager B registers */
SCIB : origin = 0x007750, length = 0x000010 /* SCI-B registers */
MCBSPA : origin = 0x007800, length = 0x000040 /* McBSP registers */
CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations. */
}
SECTIONS
{
/*** The PIE Vector table is called PIEVECT by DSP/BIOS ***/
PieVectTableFile : > PIEVECT, PAGE = 1, TYPE = DSECT
/*** Peripheral Frame 0 Register Structures ***/
DevEmuRegsFile : > DEV_EMU, PAGE = 1
FlashRegsFile : > FLASH_REGS, PAGE = 1
CsmRegsFile : > CSM, PAGE = 1
XintfRegsFile : > XINTF, PAGE = 1
CpuTimer0RegsFile : > CPU_TIMER0, PAGE = 1
CpuTimer1RegsFile : > CPU_TIMER1, PAGE = 1
CpuTimer2RegsFile : > CPU_TIMER2, PAGE = 1
PieCtrlRegsFile : > PIE_CTRL, PAGE = 1
/*** Peripheral Frame 1 Register Structures ***/
ECanaRegsFile : > ECANA, PAGE = 1
ECanaLAMRegsFile : > ECANA_LAM PAGE = 1
ECanaMboxesFile : > ECANA_MBOX PAGE = 1
ECanaMOTSRegsFile : > ECANA_MOTS PAGE = 1
ECanaMOTORegsFile : > ECANA_MOTO PAGE = 1
/*** Peripheral Frame 2 Register Structures ***/
SysCtrlRegsFile : > SYSTEM, PAGE = 1
SpiaRegsFile : > SPIA, PAGE = 1
SciaRegsFile : > SCIA, PAGE = 1
XIntruptRegsFile : > XINTRUPT, PAGE = 1
GpioMuxRegsFile : > GPIOMUX, PAGE = 1
GpioDataRegsFile : > GPIODAT PAGE = 1
AdcRegsFile : > ADC, PAGE = 1
EvaRegsFile : > EVA, PAGE = 1
EvbRegsFile : > EVB, PAGE = 1
ScibRegsFile : > SCIB, PAGE = 1
McbspaRegsFile : > MCBSPA, PAGE = 1
/*** Code Security Module Register Structures ***/
CsmPwlFile : > CSM_PWL, PAGE = 1
}
(2)F2812_BIOS_1.cmd 用户定义的cmd
SECTIONS
{
/*** User Defined Sections ***/
codestart : > BEGIN_FLASH, PAGE = 0 /* Used by file CodeStartBranch.asm */
internalMemFuncs : > FLASH_ABCDEFGHIJ, PAGE = 0 /* Used by file Xintf.c. Link to internal memory */
csm_rsvd : > CSM_RSVD, PAGE = 0 /* Used by file Passwords.asm */
passwords : > PASSWORDS, PAGE = 0 /* Used by file Passwords.asm */
DSP1SRFile : > DSP1REG, PAGE = 1
secureRamFuncs : LOAD = FLASH_ABCDEFGHIJ, PAGE = 0 /* Used by file Flash.c */
RUN = L0SARAM, PAGE = 0 /* Load to flash, run from CSM secure RAM */
LOAD_START(_secureRamFuncs_loadstart),
LOAD_SIZE(_secureRamFuncs_loadsize),
RUN_START(_secureRamFuncs_runstart)
IQmathTables : > IQTABLES PAGE = 0, TYPE = NOLOAD
IQmath : > FLASH_ABCDEFGHIJ PAGE = 0
}
(3)BIOS自动生成的cmd:
-u _FXN_F_nop
GBL_USERLIMPMODEABORTFXN = _FXN_F_nop;
-u _UserInit
GBL_USERINITFXN = _UserInit;
-u L1SARAM
MEM_SEGZERO = L1SARAM;
-u L1SARAM
MEM_MALLOCSEG = L1SARAM;
-u CLK_F_getshtime
CLK_TIMEFXN = CLK_F_getshtime;
-u CLK_F_run
CLK_HOOKFXN = CLK_F_run;
-u KNL_tick_stub
PRD_THOOKFXN = KNL_tick_stub;
-u L1SARAM
RTDX_DATAMEMSEG = L1SARAM;
-u L1SARAM
HST_DSMBUFSEG = L1SARAM;
-u GBL_NULL
SWI_EHOOKFXN = GBL_NULL;
-u GBL_NULL
SWI_IHOOKFXN = GBL_NULL;
-u SWI_F_exec
SWI_EXECFXN = SWI_F_exec;
-u SWI_F_run
SWI_RUNFXN = SWI_F_run;
-u L1SARAM
TSK_STACKSEG = L1SARAM;
-u _FXN_F_nop
TSK_VCREATEFXN = _FXN_F_nop;
-u _FXN_F_nop
TSK_VDELETEFXN = _FXN_F_nop;
-u _FXN_F_nop
TSK_VEXITFXN = _FXN_F_nop;
-u IDL_F_stub
IDL_CALIBRFXN = IDL_F_stub;
-u _UTL_doAbort
SYS_ABORTFXN = _UTL_doAbort;
-u _UTL_doError
SYS_ERRORFXN = _UTL_doError;
-u _UTL_halt
SYS_EXITFXN = _UTL_halt;
-u _UTL_doPutc
SYS_PUTCFXN = _UTL_doPutc;
-u _FXN_F_nop
GIO_CREATEFXN = _FXN_F_nop;
-u _FXN_F_nop
GIO_DELETEFXN = _FXN_F_nop;
-u _FXN_F_nop
GIO_PENDFXN = _FXN_F_nop;
-u _FXN_F_nop
GIO_POSTFXN = _FXN_F_nop;
/* OBJECT ALIASES */
_PIEVECT = PIEVECT;
_OTP = OTP;
_H0SARAM = H0SARAM;
_L1SARAM = L1SARAM;
_L0SARAM = L0SARAM;
_M1SARAM = M1SARAM;
_M0SARAM = M0SARAM;
_ZONE6 = ZONE6;
_PASSWORDS = PASSWORDS;
_BEGIN_H0 = BEGIN_H0;
_BEGIN_FLASH = BEGIN_FLASH;
_FLASH_ABCDEFGHIJ = FLASH_ABCDEFGHIJ;
_CSM_RSVD = CSM_RSVD;
_IQTABLES = IQTABLES;
_DSP1REG = DSP1REG;
_ZONE1 = ZONE1;
_PRD_clock = PRD_clock;
_PRD0 = PRD0;
_RTA_fromHost = RTA_fromHost;
_RTA_toHost = RTA_toHost;
_HWI_RESET = HWI_RESET;
_HWI_INT1 = HWI_INT1;
_HWI_INT2 = HWI_INT2;
_HWI_INT3 = HWI_INT3;
_HWI_INT4 = HWI_INT4;
_HWI_INT5 = HWI_INT5;
_HWI_INT6 = HWI_INT6;
_HWI_INT7 = HWI_INT7;
_HWI_INT8 = HWI_INT8;
_HWI_INT9 = HWI_INT9;
_HWI_INT10 = HWI_INT10;
_HWI_INT11 = HWI_INT11;
_HWI_INT12 = HWI_INT12;
_HWI_INT13 = HWI_INT13;
_HWI_TINT = HWI_TINT;
_HWI_DLOG = HWI_DLOG;
_HWI_RTOS = HWI_RTOS;
_HWI_RESERVED = HWI_RESERVED;
_HWI_NMI = HWI_NMI;
_HWI_ILLEGAL = HWI_ILLEGAL;
_HWI_USER1 = HWI_USER1;
_HWI_USER2 = HWI_USER2;
_HWI_USER3 = HWI_USER3;
_HWI_USER4 = HWI_USER4;
_HWI_USER5 = HWI_USER5;
_HWI_USER6 = HWI_USER6;
_HWI_USER7 = HWI_USER7;
_HWI_USER8 = HWI_USER8;
_HWI_USER9 = HWI_USER9;
_HWI_USER10 = HWI_USER10;
_HWI_USER11 = HWI_USER11;
_HWI_USER12 = HWI_USER12;
_PIE_INT1_1 = PIE_INT1_1;
_PIE_INT1_2 = PIE_INT1_2;
_PIE_INT1_3 = PIE_INT1_3;
_PIE_INT1_4 = PIE_INT1_4;
_PIE_INT1_5 = PIE_INT1_5;
_PIE_INT1_6 = PIE_INT1_6;
_PIE_INT1_7 = PIE_INT1_7;
_PIE_INT1_8 = PIE_INT1_8;
_PIE_INT2_1 = PIE_INT2_1;
_PIE_INT2_2 = PIE_INT2_2;
_PIE_INT2_3 = PIE_INT2_3;
_PIE_INT2_4 = PIE_INT2_4;
_PIE_INT2_5 = PIE_INT2_5;
_PIE_INT2_6 = PIE_INT2_6;
_PIE_INT2_7 = PIE_INT2_7;
_PIE_INT2_8 = PIE_INT2_8;
_PIE_INT3_1 = PIE_INT3_1;
_PIE_INT3_2 = PIE_INT3_2;
_PIE_INT3_3 = PIE_INT3_3;
_PIE_INT3_4 = PIE_INT3_4;
_PIE_INT3_5 = PIE_INT3_5;
_PIE_INT3_6 = PIE_INT3_6;
_PIE_INT3_7 = PIE_INT3_7;
_PIE_INT3_8 = PIE_INT3_8;
_PIE_INT4_1 = PIE_INT4_1;
_PIE_INT4_2 = PIE_INT4_2;
_PIE_INT4_3 = PIE_INT4_3;
_PIE_INT4_4 = PIE_INT4_4;
_PIE_INT4_5 = PIE_INT4_5;
_PIE_INT4_6 = PIE_INT4_6;
_PIE_INT4_7 = PIE_INT4_7;
_PIE_INT4_8 = PIE_INT4_8;
_PIE_INT5_1 = PIE_INT5_1;
_PIE_INT5_2 = PIE_INT5_2;
_PIE_INT5_3 = PIE_INT5_3;
_PIE_INT5_4 = PIE_INT5_4;
_PIE_INT5_5 = PIE_INT5_5;
_PIE_INT5_6 = PIE_INT5_6;
_PIE_INT5_7 = PIE_INT5_7;
_PIE_INT5_8 = PIE_INT5_8;
_PIE_INT6_1 = PIE_INT6_1;
_PIE_INT6_2 = PIE_INT6_2;
_PIE_INT6_3 = PIE_INT6_3;
_PIE_INT6_4 = PIE_INT6_4;
_PIE_INT6_5 = PIE_INT6_5;
_PIE_INT6_6 = PIE_INT6_6;
_PIE_INT6_7 = PIE_INT6_7;
_PIE_INT6_8 = PIE_INT6_8;
_PIE_INT7_1 = PIE_INT7_1;
_PIE_INT7_2 = PIE_INT7_2;
_PIE_INT7_3 = PIE_INT7_3;
_PIE_INT7_4 = PIE_INT7_4;
_PIE_INT7_5 = PIE_INT7_5;
_PIE_INT7_6 = PIE_INT7_6;
_PIE_INT7_7 = PIE_INT7_7;
_PIE_INT7_8 = PIE_INT7_8;
_PIE_INT8_1 = PIE_INT8_1;
_PIE_INT8_2 = PIE_INT8_2;
_PIE_INT8_3 = PIE_INT8_3;
_PIE_INT8_4 = PIE_INT8_4;
_PIE_INT8_5 = PIE_INT8_5;
_PIE_INT8_6 = PIE_INT8_6;
_PIE_INT8_7 = PIE_INT8_7;
_PIE_INT8_8 = PIE_INT8_8;
_PIE_INT9_1 = PIE_INT9_1;
_PIE_INT9_2 = PIE_INT9_2;
_PIE_INT9_3 = PIE_INT9_3;
_PIE_INT9_4 = PIE_INT9_4;
_PIE_INT9_5 = PIE_INT9_5;
_PIE_INT9_6 = PIE_INT9_6;
_PIE_INT9_7 = PIE_INT9_7;
_PIE_INT9_8 = PIE_INT9_8;
_PIE_INT10_1 = PIE_INT10_1;
_PIE_INT10_2 = PIE_INT10_2;
_PIE_INT10_3 = PIE_INT10_3;
_PIE_INT10_4 = PIE_INT10_4;
_PIE_INT10_5 = PIE_INT10_5;
_PIE_INT10_6 = PIE_INT10_6;
_PIE_INT10_7 = PIE_INT10_7;
_PIE_INT10_8 = PIE_INT10_8;
_PIE_INT11_1 = PIE_INT11_1;
_PIE_INT11_2 = PIE_INT11_2;
_PIE_INT11_3 = PIE_INT11_3;
_PIE_INT11_4 = PIE_INT11_4;
_PIE_INT11_5 = PIE_INT11_5;
_PIE_INT11_6 = PIE_INT11_6;
_PIE_INT11_7 = PIE_INT11_7;
_PIE_INT11_8 = PIE_INT11_8;
_PIE_INT12_1 = PIE_INT12_1;
_PIE_INT12_2 = PIE_INT12_2;
_PIE_INT12_3 = PIE_INT12_3;
_PIE_INT12_4 = PIE_INT12_4;
_PIE_INT12_5 = PIE_INT12_5;
_PIE_INT12_6 = PIE_INT12_6;
_PIE_INT12_7 = PIE_INT12_7;
_PIE_INT12_8 = PIE_INT12_8;
_PRD_swi = PRD_swi;
_KNL_swi = KNL_swi;
_TSK_idle = TSK_idle;
_IDL_cpuLoad = IDL_cpuLoad;
_LNK_dataPump = LNK_dataPump;
_RTA_dispatcher = RTA_dispatcher;
_IDL0 = IDL0;
_IDL1 = IDL1;
_IDL2 = IDL2;
_LOG_system = LOG_system;
_trace = trace;
_IDL_busyObj = IDL_busyObj;
/* MODULE GBL */
SECTIONS {
.vers (COPY): {} /* version information */
}
-priority
-llnkrtdx.a28L
-ldrivers.a28L /* device drivers support */
-lsioboth.a28L /* supports both SIO models */
-lbios.a28L /* DSP/BIOS support */
-lrtdxx.lib /* RTDX support */
-lrts2800_ml.lib /* C and C++ run-time library support */
/* MODULE MEM */
-stack 0x200
MEMORY {
PAGE 1: PIEVECT: origin = 0xd00, len = 0x100
PAGE 0: OTP: origin = 0x3d7800, len = 0x400
PAGE 1: H0SARAM: origin = 0x3f8002, len = 0x1ffe
PAGE 1: L1SARAM: origin = 0x9000, len = 0x1000
PAGE 0: L0SARAM: origin = 0x8000, len = 0x1000
PAGE 1: M1SARAM: origin = 0x400, len = 0x400
PAGE 1: M0SARAM: origin = 0x0, len = 0x400
PAGE 1: ZONE6: origin = 0x100000, len = 0x10000
PAGE 0: PASSWORDS: origin = 0x3f7ff8, len = 0x8
PAGE 0: BEGIN_H0: origin = 0x3f8000, len = 0x2
PAGE 0: BEGIN_FLASH: origin = 0x3f7ff6, len = 0x2
PAGE 0: FLASH_ABCDEFGHIJ: origin = 0x3d8000, len = 0x1ff80
PAGE 0: CSM_RSVD: origin = 0x3f7f80, len = 0x76
PAGE 0: IQTABLES: origin = 0x3ff000, len = 0xb50
PAGE 1: DSP1REG: origin = 0x5000, len = 0x2d
PAGE 1: ZONE1: origin = 0x502d, len = 0x97
}
/* MODULE CLK */
SECTIONS {
.clk: {
CLK_F_gethtime = CLK_F_getshtime;
*(.clk)
} > L1SARAM PAGE 1, RUN_START(CLK_A_TABBEG)
}
_CLK_PRD = CLK_PRD;
_CLK_COUNTSPMS = CLK_COUNTSPMS;
_CLK_REGS = CLK_REGS;
_CLK_USETIMER = CLK_USETIMER;
_CLK_TIMERNUM = CLK_TIMERNUM;
_CLK_TCR = CLK_TCR;
_CLK_TDDR = CLK_TDDR;
/* MODULE PRD */
SECTIONS {
.prd: RUN_START(PRD_A_TABBEG), RUN_END(PRD_A_TABEND) {
} > L1SARAM PAGE 1
}
PRD_A_TABLEN = 1;
/* MODULE RTDX */
_RTDX_interrupt_mask = 0x0;
/* MODULE SWI */
SECTIONS {
.swi: RUN_START(SWI_A_TABBEG), RUN_END(SWI_A_TABEND) {
} > L1SARAM PAGE 1
}
SWI_A_TABLEN = 2;
/* MODULE TSK */
SECTIONS {
.tsk: {
*(.tsk)
} > L1SARAM PAGE 1
}
/* MODULE IDL */
SECTIONS {
.idl: {
*(.idl)
} > L1SARAM PAGE 1, RUN_START(IDL_A_TABBEG)
.idlcal: {
*(.idlcal)
} > L1SARAM PAGE 1, RUN_START(IDL_A_CALBEG)
}
LOG_A_TABLEN = 2; _LOG_A_TABLEN = 2;
PIP_A_TABLEN = 2;
SECTIONS {
frt: {} > FLASH_ABCDEFGHIJ PAGE 0
.bios: {} > FLASH_ABCDEFGHIJ PAGE 0
.data: {} > FLASH_ABCDEFGHIJ PAGE 0
.pinit: {} > FLASH_ABCDEFGHIJ PAGE 0
.text: {} > FLASH_ABCDEFGHIJ PAGE 0
.cinit: {} > FLASH_ABCDEFGHIJ PAGE 0
.const: {} > FLASH_ABCDEFGHIJ PAGE 0
.switch: {} > FLASH_ABCDEFGHIJ PAGE 0
.gblinit: {} > FLASH_ABCDEFGHIJ PAGE 0
.sysinit: {} > FLASH_ABCDEFGHIJ PAGE 0
.rtdx_text: {} > FLASH_ABCDEFGHIJ PAGE 0
.hwi: {
/* no HWI stubs are necessary */
} > FLASH_ABCDEFGHIJ PAGE 0
GROUP {
.econst: {}
.printf (COPY): {}
} > FLASH_ABCDEFGHIJ PAGE 0
.bss: {} > H0SARAM PAGE 1
.ebss: {} > H0SARAM PAGE 1
.hwi_disp_sec: {} > H0SARAM PAGE 1
.sysdata: {} > L1SARAM PAGE 1
.dsm: {} > L1SARAM PAGE 1
.mem: {} > L1SARAM PAGE 1
.cio: {} > L1SARAM PAGE 1
.gio: {} > L1SARAM PAGE 1
.sys: {} > L1SARAM PAGE 1
.sysregs: {} > L1SARAM PAGE 1
.rtdx_data: {} > L1SARAM PAGE 1
.TSK_idle$stk: {
*(.TSK_idle$stk)
} > L1SARAM PAGE 1
/* LOG_system buffer */
.LOG_system$buf: align = 0x80 {} > L1SARAM PAGE 1
/* trace buffer */
.trace$buf: align = 0x40 {} > L1SARAM PAGE 1
.args: fill=0 {
*(.args)
. += 0x4;
} > L1SARAM PAGE 1
/* RTA_fromHost buffer */
.hst1: align = 0x4 {} > L1SARAM PAGE 1
/* RTA_toHost buffer */
.hst0: align = 0x4 {} > L1SARAM PAGE 1
.trace: fill = 0x0 {
_SYS_PUTCBEG = .;
. += 0x200;
_SYS_PUTCEND = . - 1;
} > L1SARAM PAGE 1
.hst: RUN_START(HST_A_TABBEG), RUN_START(_HST_A_TABBEG), RUN_END(HST_A_TABEND), RUN_END(_HST_A_TABEND) {
} > L1SARAM PAGE 1
.log: RUN_START(LOG_A_TABBEG), RUN_START(_LOG_A_TABBEG), RUN_END(LOG_A_TABEND), RUN_END(_LOG_A_TABEND) {
} > L1SARAM PAGE 1
.pip: RUN_START(PIP_A_TABBEG), RUN_START(_PIP_A_TABBEG), RUN_END(PIP_A_TABEND), RUN_END(_PIP_A_TABEND) {
} > L1SARAM PAGE 1
.sts: RUN_START(STS_A_TABBEG), RUN_START(_STS_A_TABBEG), RUN_END(STS_A_TABEND), RUN_END(_STS_A_TABEND) {
} > L1SARAM PAGE 1
.trcdata: START(_trcdata_loadstart), END(_trcdata_loadend), SIZE(_trcdata_loadsize), RUN_START(_trcdata_runstart) {
} load > FLASH_ABCDEFGHIJ PAGE 0, run > L1SARAM PAGE 1
.L1SARAM$heap: {
. += 0x200;
} RUN_START(L1SARAM$B), RUN_START(_L1SARAM_base), RUN_SIZE(L1SARAM$L), RUN_SIZE(_L1SARAM_length) > L1SARAM PAGE 1
.stack: {
GBL_stackbeg = .;
*(.stack)
GBL_stackend = GBL_stackbeg + 0x200 - 1;
_HWI_STKBOTTOM = GBL_stackbeg;
_HWI_STKTOP = (GBL_stackend + 1);
} > M1SARAM PAGE 1
.hwi_vec: START(_hwi_vec_loadstart), END(_hwi_vec_loadend), SIZE(_hwi_vec_loadsize), RUN_START(_hwi_vec_runstart) {
/* no HWI stubs are necessary */
} load > FLASH_ABCDEFGHIJ PAGE 0, run > PIEVECT PAGE 1
}
这样的错误在网上也有很多,但是针对BIOS的很少,我不知道是CCS设置的问题还是cmd文件的问题希望
在这方面有研究的朋友给予我帮助,谢谢了。