This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教,CCS5中如何只烧写OUT文件,而没有或看不到原文件?,谢谢!
如果只有.out文件而没有源工程文件,可以按照以下方法进行烧写:
1)点击view->Target Configurations;
2)在Target Configurations中选中所选择的仿真器配置(如果没有则新建一个),右击后选择"Launch Selected Configuration";
3)在Debug窗口选中需要连接的仿真器之后,点击run->Connect Target;
4)之后就是和有工程文件的烧写方式一样了,点击load,找到.out目录,完成load。
Seven,
工程中包含C28和CLA的源代码,烧写的时候连接C28,load即可。
在调试的时候,如果只调试C28,只需要connect C28即可,CLA不用管。
如果也要调试CLA,则load c28后, connect CLA, run 》 load sysboml
Eric
在Debug界面下的View中选择Debug窗口,其中有仿真器出现吗,如果有,可以通过邮寄仿真器进行Connect,如果没有,那说明没有正确Launch Selected Configuration