This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35 TI-RTOS系统移植 工程文件的建立



您好:

    我现在需要在F28m35中移植个TI-RTOS的系统。我打算在已有的TI-RTOS  demo上做相应的修改。我有几个问题请教。

1、因为是双核,我需要建立两个project。我准备在M3中移植TI-RTOS系统,C28中不移植。那么是否是M3的project,是在TI-RTOS  demo中的project上修改,而C28的project在F28m35普通的project中修改就可以了?

2、像我1中说的,一个核跑系统,另一个不跑系统,这样可以吗?

3、这两个project烧写到DSP的顺序是怎么样的?能否介绍下这个双核project烧写的细节步骤什么的?

  • 1. 在实际CCS代码编写中,两个内核的代码实际上是分成两个不停的项目分开编写,而两个内核的外设使用在初始化的时候已经由M3分配完毕。所以在两个内核全速运行时,他们之间的只会通过IPC总线或者共享内存区交换数据,并不产生其他交差的任务,所以两个内核分别跑什么样的代码不会对另外一个有影响。

    2. 烧写的顺序是先烧入M3的.out文件,再烧入C28的.ou文件