最近打算做一块28335的板子玩玩。看了下淘宝上大多用的是RTL8019的方案。不过很多ARM板的网络接口用的是DM9000的方案。不知大家有没有什么好的方案推荐~谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近打算做一块28335的板子玩玩。看了下淘宝上大多用的是RTL8019的方案。不过很多ARM板的网络接口用的是DM9000的方案。不知大家有没有什么好的方案推荐~谢谢~
TI没有基于F28335的网络应用的参考设计。
但我们有最新的双核芯片F28M35x,内部集成了Cortex M3,有10M/100M 网口。
好主意~可以考虑外挂个M3,不过是不是太拉风了,然后貌似没有比较快的数据接口啊。。F28M35x啥时可以申请样片啊?
其实不用外挂,直接用F28M35x就看可以了,因为这个F28M35x内部就已经包含了CM3。 并且价位是单个C2000的价位。 说白了就是买一颗C2000,送一颗CM3.
另,F28M35x 已经可以购买开发板,在下面这个网页上的estore上购买,或者联系当地的代理商购买。
建议您先买一个开发板,而不是直接买样片,因为这颗芯片和以前的C2000的最大区别是内部有个CM3,所以还是建议先用开发板,再买芯片。
www.ti.com/c2000tools
谢谢!