This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在选择CLA情况下--run---load symbol---browse project 操作后,CCS提示no entry available 提示。
但是在连接C28XX的CPU时,代码是能烧写的;
这是什么原因,谢谢
用的是TI的28035的例程,CCS5.3
我主要是看视频教程上点击browse project选项的,
但是如果点击browse--选择相应的.out文件,
点击Resum(F8)按钮--代码停在__mdebugstop();处,但是再次按F5(step into)按钮,
CCS会提示如下故障:
CLA_0: Can't Single Step Target Program: (Error -2060 @ 0x0) Requested operation cannot be done while device is running. Halt the device, and retry the operation. (Emulation package 5.0.872.0)
和视频教程上的操作结果不一样,变量的值也是毫无变化!!
头痛啊
我编译时,
1、搞锤子进行编译,编译完后,看它的提示:
'Finished building target: XXXX.out'
' '
**** Build Finished ****
此时算真正通过了,有汇编语言的项目,有时候有错误时在problems窗口没有提示错误,但编译不会产生OUT文件。
2、搞虫子,进行调试。些时不用执行菜单即可将OUT加载
你可以单步调试,或者在这个task的开头和结尾都添加一个__mdebugstop();,然后再resume。也可以把__mdebugstop();去掉,但去掉后CLA task会直接运行过去,不能调试CLA程序。
刚刚找出了原因了。
我又看了一遍视频教程,发现是先成功连接CLA后,再点击C28XX_CPU核,再点击RESUME,等待几秒后,就可以看到CLA里面变量的值发生变化了。
谢谢各位,
您好:
我想看下代码运行的时间,准备用clock功能查看
步骤如下:
Enable--Show,
在CCS5的左下角有个时钟的图表,还有数值0
但是当我在CLA里用_mdebugstop();设置断点,发现时钟的数值并没有跟着更新,难道在CLA里面不能用时钟功能来看代码运行的时间吗?