This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在选择CLA情况下--run---load symbol---browse project 操作后,CCS提示no entry available 提示。
但是在连接C28XX的CPU时,代码是能烧写的;
这是什么原因,谢谢
用的是TI的28035的例程,CCS5.3
我主要是看视频教程上点击browse project选项的,
但是如果点击browse--选择相应的.out文件,
点击Resum(F8)按钮--代码停在__mdebugstop();处,但是再次按F5(step into)按钮,
CCS会提示如下故障:
CLA_0: Can't Single Step Target Program: (Error -2060 @ 0x0) Requested operation cannot be done while device is running. Halt the device, and retry the operation. (Emulation package 5.0.872.0)
和视频教程上的操作结果不一样,变量的值也是毫无变化!!
头痛啊