This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大虾新年好。现在出F28M35的原理图,准备用内部的稳压器,1.2和1.8两路电压由内部产生。问题如下:
芯片的各个VDD12引脚,在内部是不是相连的?VDD18是不是也已经内部相连了?看官网开发板的原理图和瑞泰创新的都是启用的内部VREG,但是VDD12和VDD18又在外部分别全部连接起来了。我总觉得没必要,内部的的1.2V和1.8V电源轨应该在片子内部就将各相关电源引脚连接了。请大虾帮忙确认到底是怎么样的?2、F28M35H52C芯片的第91脚到底是NC还是VDD12,这个开发板原理和DATAsheet(2556KB大小的那个,第90和110页)上明显不一样,大乌龙。请确认,谢谢。
急切恭候回复中。如果内部的1.2及1.8两组电源轨分别将相关引脚在芯片内部做了链接,那么PCB设计的时候,在芯片外部就没必要再做同组互联了,事实上给PCB设计省去了很多麻烦。如果内部没有连接的话,那么内部的VREG我感觉意义就不太大了,首先PCB设计没有简化,另外现在的电源技术单片集成3路以上电源难度不大,可以直接选择外供,同时功耗还低。
我本人比较重视电源和PCB设计,请TI专家指教。谢谢!
谢谢您的解答。关于第1个问题意思是只要我在外面加上陶瓷电容,就没必要在PCB上将所有VDD12连接在一起了吧(同理VDD18)?
第2个问题请参见附件的第2页,这是官方原理图,第91引脚明确为VDD12。另外值得一提的是,在内部VREF使能的情况下(pin113、101用0ohm电阻接地),VDD12和VDD18依然在PCB上做了同组内互联。
具体还请指教,多谢。