各位大虾新年好。现在出F28M35的原理图,准备用内部的稳压器,1.2和1.8两路电压由内部产生。问题如下:
芯片的各个VDD12引脚,在内部是不是相连的?VDD18是不是也已经内部相连了?看官网开发板的原理图和瑞泰创新的都是启用的内部VREG,但是VDD12和VDD18又在外部分别全部连接起来了。我总觉得没必要,内部的的1.2V和1.8V电源轨应该在片子内部就将各相关电源引脚连接了。请大虾帮忙确认到底是怎么样的?2、F28M35H52C芯片的第91脚到底是NC还是VDD12,这个开发板原理和DATAsheet(2556KB大小的那个,第90和110页)上明显不一样,大乌龙。请确认,谢谢。