Other Parts Discussed in Thread: C2000WARE
我的板子型号是280049,我在用HRPWM实现高精度移相,并可以调整高精度周期,但是出来的波形没有实现,是不是我的寄存器配置有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的板子型号是280049,我在用HRPWM实现高精度移相,并可以调整高精度周期,但是出来的波形没有实现,是不是我的寄存器配置有问题?
#include "driverlib.h" #include "device.h" #include "board.h" #include "SFO_V8.h" #include <math.h> // // Defines // #define EPWM_TIMER_TBPRD 4545UL//5000UL #define LAST_EPWM_INDEX_FOR_EXAMPLE 5 #define MIN_HRPWM_PRD_PERCENT (20.0003f) #define myEPWM1_BASE EPWM1_BASE #define myEPWM2_BASE EPWM2_BASE #define myEPWM3_BASE EPWM3_BASE // // Globals // static float64_t periodFine = MIN_HRPWM_PRD_PERCENT; uint16_t status; //int MEP_ScaleFactor; // Global variable used by the SFO library // Result can be used for all HRPWM channels // This variable is also copied to HRMSTEP // register by SFO() function. //volatile uint32_t ePWM[] = // {myEPWM1_BASE,myEPWM2_BASE, myEPWM3_BASE}; // // Function Prototypes // void initHRPWM(uint32_t period); void error(void); void PinMuxEPWM1_init(); void PinMuxEPWM2_init(); void PinMuxEPWM3_init(); void EPWM1_init(); void EPWM2_init(); void EPWM3_init(); void initGPIO(); // // Main // void changeHZ(double zTemp,double iAngle) { uint32_t compCount = 0UL; double iTemp = 0.0f; uint32_t aTemp = 100000UL; uint32_t xTemp = 0UL; double yTemp = 0.0f; uint32_t iPhase=0; iTemp = aTemp / zTemp; xTemp = floor(iTemp); //取整数部分 yTemp = iTemp - xTemp; //减,以取小数部分 compCount= ((xTemp-1) << 8UL)+ (float32_t)(yTemp*256); HRPWM_setTimeBasePeriod(myEPWM1_BASE, compCount); HRPWM_setTimeBasePeriod(myEPWM3_BASE, compCount); HRPWM_setTimeBasePeriod(myEPWM2_BASE, compCount); // // set duty 50% initially // HRPWM_setCounterCompareValue(myEPWM1_BASE, HRPWM_COUNTER_COMPARE_A, (xTemp/2 << 8)); //HRPWM_setCounterCompareValue(myEPWM1_BASE, HRPWM_COUNTER_COMPARE_B, (xTemp/2 << 8)); HRPWM_setCounterCompareValue(myEPWM3_BASE, HRPWM_COUNTER_COMPARE_A, (xTemp/2 << 8)); //HRPWM_setCounterCompareValue(myEPWM3_BASE, HRPWM_COUNTER_COMPARE_B, (xTemp/2 << 8)); HRPWM_setCounterCompareValue(myEPWM2_BASE, HRPWM_COUNTER_COMPARE_A, (xTemp/2 << 8)); //HRPWM_setCounterCompareValue(myEPWM2_BASE, HRPWM_COUNTER_COMPARE_B, (xTemp/2 << 8)); //iPhase/xTemp*360=iAngle; // iTemp=((iAngle*xTemp)/360.0f); compCount=(uint32_t)iTemp; iPhase=xTemp-compCount; EPWM_setPhaseShift(myEPWM3_BASE, iPhase); EPWM_setPhaseShift(myEPWM2_BASE, iPhase); } void main(void) { uint16_t abit = 0; float32_t angle = 1.0; // //compCount= ((xTemp-1) << 8UL)+ (float32_t)(yTemp*256); //HRPWM_setTimeBasePeriod(myEPWM1_BASE, compCount); //HRPWM_setTimeBasePeriod(myEPWM3_BASE, compCount); // Initialize device clock and peripherals // Device_init(); // // Disable pin locks and enable internal pull ups. // Device_initGPIO(); CBSP_GIO_LED_Init(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // Initialize EPWM GPIOs // PinMuxEPWM1_init(); PinMuxEPWM2_init(); PinMuxEPWM3_init(); EPWM1_init(); EPWM2_init(); EPWM3_init(); // // Calling SFO() updates the HRMSTEP register with calibrated MEP_ScaleFactor. // HRMSTEP must be populated with a scale factor value prior to enabling // high resolution period control. // while(status == SFO_INCOMPLETE) { status = SFO(); if(status == SFO_ERROR) { error(); // SFO function returns 2 if an error occurs & # of MEP } // steps/coarse step exceeds maximum of 255. } // // Disable sync(Freeze clock to PWM as well) // SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC); initHRPWM(EPWM_TIMER_TBPRD); // // Enable sync and clock to PWM // SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; periodFine=MIN_HRPWM_PRD_PERCENT; changeHZ(periodFine,90); status = SFO(); // in background, MEP calibration module // continuously updates MEP_ScaleFactor if (status == SFO_ERROR) { error(); // SFO function returns 2 if an error occurs & # // of MEP steps/coarse step } for(;;) { // // Sweep DutyFine // //for(periodFine = MIN_HRPWM_PRD_PERCENT; periodFine < (MIN_HRPWM_PRD_PERCENT+0.805); periodFine += 0.1001) //for(periodFine = 1; periodFine < (180); periodFine++) LED_TOGGLE(); if(abit>0) { if(angle<(180-1)) { angle++; periodFine+=0.001; } else { abit=0; } } else { if(angle>1) { angle--; periodFine-=0.001; } else { abit=1; } } { DEVICE_DELAY_US(10); changeHZ(periodFine,angle); // // Call the scale factor optimizer lib function SFO() // periodically to track for any change due to temp/voltage. // This function generates MEP_ScaleFactor by running the // MEP calibration module in the HRPWM logic. This scale // factor can be used for all HRPWM channels. The SFO() // function also updates the HRMSTEP register with the // scale factor value. // status = SFO(); // in background, MEP calibration module // continuously updates MEP_ScaleFactor if (status == SFO_ERROR) { error(); // SFO function returns 2 if an error occurs & # // of MEP steps/coarse step } // exceeds maximum of 255. } } } void initHRPWM(uint32_t period) { EPWM_setEmulationMode(myEPWM1_BASE, EPWM_EMULATION_FREE_RUN); EPWM_setEmulationMode(myEPWM2_BASE, EPWM_EMULATION_FREE_RUN); EPWM_setEmulationMode(myEPWM3_BASE, EPWM_EMULATION_FREE_RUN); // // Set-up TBCLK // EPWM_setTimeBasePeriod(myEPWM1_BASE, period-1); EPWM_setPhaseShift(myEPWM1_BASE, 0U); EPWM_setTimeBaseCounter(myEPWM1_BASE, 0U); EPWM_setTimeBasePeriod(myEPWM2_BASE, period-1); EPWM_setTimeBaseCounter(myEPWM2_BASE, 0U); EPWM_setTimeBasePeriod(myEPWM3_BASE, period-1); EPWM_setTimeBaseCounter(myEPWM3_BASE, 0U); // // set duty 50% initially // HRPWM_setCounterCompareValue(myEPWM1_BASE, HRPWM_COUNTER_COMPARE_A, (period/2 << 8)); HRPWM_setCounterCompareValue(myEPWM1_BASE, HRPWM_COUNTER_COMPARE_B, (period/2 << 8)); HRPWM_setCounterCompareValue(myEPWM2_BASE, HRPWM_COUNTER_COMPARE_A, (period/2 << 8)); HRPWM_setCounterCompareValue(myEPWM2_BASE, HRPWM_COUNTER_COMPARE_B, (period/2 << 8)); HRPWM_setCounterCompareValue(myEPWM3_BASE, HRPWM_COUNTER_COMPARE_A, (period/2 << 8)); HRPWM_setCounterCompareValue(myEPWM3_BASE, HRPWM_COUNTER_COMPARE_B, (period/2 << 8)); // // Set up counter mode // EPWM_setTimeBaseCounterMode(myEPWM1_BASE, EPWM_COUNTER_MODE_UP); EPWM_disablePhaseShiftLoad(myEPWM1_BASE); EPWM_setClockPrescaler(myEPWM1_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); EPWM_setSyncOutPulseMode(myEPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_COUNTER_ZERO); EPWM_setTimeBaseCounterMode(myEPWM2_BASE, EPWM_COUNTER_MODE_UP); EPWM_enablePhaseShiftLoad(myEPWM2_BASE); EPWM_setTimeBaseCounterMode(myEPWM3_BASE, EPWM_COUNTER_MODE_UP); EPWM_enablePhaseShiftLoad(myEPWM3_BASE); uint32_t iPeriod=period/3; iPeriod=period*0.03; EPWM_setPhaseShift(myEPWM3_BASE, iPeriod); EPWM_setClockPrescaler(myEPWM3_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); EPWM_setSyncOutPulseMode(myEPWM3_BASE, EPWM_SYNC_OUT_PULSE_DISABLED); EPWM_setPhaseShift(myEPWM2_BASE, iPeriod); EPWM_setClockPrescaler(myEPWM2_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); EPWM_setSyncOutPulseMode(myEPWM2_BASE, EPWM_SYNC_OUT_PULSE_DISABLED); // // Set up shadowing // EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareShadowLoadMode(myEPWM3_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareShadowLoadMode(myEPWM3_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); // // Set actions // EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); HRPWM_setMEPEdgeSelect(myEPWM1_BASE, HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_RISING_EDGE); HRPWM_setMEPControlMode(myEPWM1_BASE, HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setCounterCompareShadowLoadEvent(myEPWM1_BASE, HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setMEPEdgeSelect(myEPWM3_BASE, HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_RISING_EDGE); HRPWM_setMEPControlMode(myEPWM3_BASE, HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setCounterCompareShadowLoadEvent(myEPWM3_BASE, HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setMEPEdgeSelect(myEPWM2_BASE, HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_RISING_EDGE); HRPWM_setMEPControlMode(myEPWM2_BASE, HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setCounterCompareShadowLoadEvent(myEPWM2_BASE, HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setMEPEdgeSelect(myEPWM1_BASE, HRPWM_CHANNEL_B, HRPWM_MEP_CTRL_RISING_EDGE); HRPWM_setMEPControlMode(myEPWM1_BASE, HRPWM_CHANNEL_B, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setCounterCompareShadowLoadEvent(myEPWM1_BASE, HRPWM_CHANNEL_B, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setMEPEdgeSelect(myEPWM3_BASE, HRPWM_CHANNEL_B, HRPWM_MEP_CTRL_RISING_EDGE); HRPWM_setMEPControlMode(myEPWM3_BASE, HRPWM_CHANNEL_B, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setCounterCompareShadowLoadEvent(myEPWM3_BASE, HRPWM_CHANNEL_B, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setMEPEdgeSelect(myEPWM2_BASE, HRPWM_CHANNEL_B, HRPWM_MEP_CTRL_RISING_EDGE); HRPWM_setMEPControlMode(myEPWM2_BASE, HRPWM_CHANNEL_B, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setCounterCompareShadowLoadEvent(myEPWM2_BASE, HRPWM_CHANNEL_B, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_enableAutoConversion(myEPWM1_BASE); HRPWM_enableAutoConversion(myEPWM3_BASE); HRPWM_enableAutoConversion(myEPWM2_BASE); // // Turn on high-resolution period control. // HRPWM_enablePeriodControl(myEPWM1_BASE); HRPWM_enablePhaseShiftLoad(myEPWM1_BASE); HRPWM_enablePeriodControl(myEPWM3_BASE); HRPWM_enablePhaseShiftLoad(myEPWM3_BASE); HRPWM_enablePeriodControl(myEPWM2_BASE); HRPWM_enablePhaseShiftLoad(myEPWM2_BASE); EPWM_forceSyncPulse(myEPWM1_BASE); EPWM_forceSyncPulse(myEPWM3_BASE); EPWM_forceSyncPulse(myEPWM2_BASE); } void EPWM3_init(){ EPWM_setClockPrescaler(myEPWM3_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_2); EPWM_setTimeBasePeriod(myEPWM3_BASE, 0); EPWM_setTimeBaseCounter(myEPWM3_BASE, 0); EPWM_setTimeBaseCounterMode(myEPWM3_BASE, EPWM_COUNTER_MODE_STOP_FREEZE); EPWM_enablePhaseShiftLoad(myEPWM3_BASE); EPWM_setPhaseShift(myEPWM3_BASE, 100); EPWM_setCounterCompareValue(myEPWM3_BASE, EPWM_COUNTER_COMPARE_A, 0); EPWM_setCounterCompareShadowLoadMode(myEPWM3_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareValue(myEPWM3_BASE, EPWM_COUNTER_COMPARE_B, 0); EPWM_setCounterCompareShadowLoadMode(myEPWM3_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setSyncOutPulseMode(myEPWM3_BASE, EPWM_SYNC_OUT_PULSE_ON_EPWMxSYNCIN); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM3_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setRisingEdgeDeadBandDelayInput(myEPWM3_BASE,EPWM_DB_INPUT_EPWMA); EPWM_setFallingEdgeDeadBandDelayInput(myEPWM3_BASE,EPWM_DB_INPUT_EPWMA); //配置死区输入模式 EPWM_setDeadBandDelayPolarity(myEPWM3_BASE,EPWM_DB_RED,EPWM_DB_POLARITY_ACTIVE_HIGH); EPWM_setDeadBandDelayPolarity(myEPWM3_BASE,EPWM_DB_FED,EPWM_DB_POLARITY_ACTIVE_LOW);//配置极性 EPWM_setDeadBandDelayMode(myEPWM3_BASE,EPWM_DB_RED,true); EPWM_setDeadBandDelayMode(myEPWM3_BASE,EPWM_DB_FED,true); //配置输出模式 EPWM_setDeadBandOutputSwapMode(myEPWM3_BASE,EPWM_DB_OUTPUT_A,false); EPWM_setDeadBandOutputSwapMode(myEPWM3_BASE,EPWM_DB_OUTPUT_B,false); //输出不交换 EPWM_setRisingEdgeDelayCount(myEPWM3_BASE,28); //上升沿延时0nS EPWM_setFallingEdgeDelayCount(myEPWM3_BASE,28); //下降沿延时0nS } void EPWM2_init(){ EPWM_setClockPrescaler(myEPWM2_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_2); EPWM_setTimeBasePeriod(myEPWM2_BASE, 0); EPWM_setTimeBaseCounter(myEPWM2_BASE, 0); EPWM_setTimeBaseCounterMode(myEPWM2_BASE, EPWM_COUNTER_MODE_STOP_FREEZE); EPWM_enablePhaseShiftLoad(myEPWM2_BASE); EPWM_setPhaseShift(myEPWM2_BASE, 100); EPWM_setCounterCompareValue(myEPWM2_BASE, EPWM_COUNTER_COMPARE_A, 0); EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareValue(myEPWM2_BASE, EPWM_COUNTER_COMPARE_B, 0); EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setSyncOutPulseMode(myEPWM2_BASE, EPWM_SYNC_OUT_PULSE_ON_EPWMxSYNCIN); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM2_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setRisingEdgeDeadBandDelayInput(myEPWM2_BASE,EPWM_DB_INPUT_EPWMA); EPWM_setFallingEdgeDeadBandDelayInput(myEPWM2_BASE,EPWM_DB_INPUT_EPWMA); //配置死区输入模式 EPWM_setDeadBandDelayPolarity(myEPWM2_BASE,EPWM_DB_RED,EPWM_DB_POLARITY_ACTIVE_HIGH); EPWM_setDeadBandDelayPolarity(myEPWM2_BASE,EPWM_DB_FED,EPWM_DB_POLARITY_ACTIVE_LOW);//配置极性 EPWM_setDeadBandDelayMode(myEPWM2_BASE,EPWM_DB_RED,true); EPWM_setDeadBandDelayMode(myEPWM2_BASE,EPWM_DB_FED,true); //配置输出模式 EPWM_setDeadBandOutputSwapMode(myEPWM2_BASE,EPWM_DB_OUTPUT_A,false); EPWM_setDeadBandOutputSwapMode(myEPWM2_BASE,EPWM_DB_OUTPUT_B,false); //输出不交换 EPWM_setRisingEdgeDelayCount(myEPWM2_BASE,28); //上升沿延时0nS EPWM_setFallingEdgeDelayCount(myEPWM2_BASE,28); //下降沿延时0nS } void EPWM1_init(){ EPWM_setClockPrescaler(myEPWM1_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_2);//ePWM 时钟为100MHZ EPWM_setTimeBasePeriod(myEPWM1_BASE, 0);//设置周期值 = 0 EPWM_setTimeBaseCounter(myEPWM1_BASE, 0);//设置初始值 EPWM_setTimeBaseCounterMode(myEPWM1_BASE, EPWM_COUNTER_MODE_STOP_FREEZE);//设置为 Stop 计数模式 EPWM_disablePhaseShiftLoad(myEPWM1_BASE);//不偏移 EPWM_setPhaseShift(myEPWM1_BASE, 0);//设置偏移值为0 EPWM_setCounterCompareValue(myEPWM1_BASE, EPWM_COUNTER_COMPARE_A, 0);//设置CMPA的值 EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO);//设置A比较值加载模式 EPWM_setCounterCompareValue(myEPWM1_BASE, EPWM_COUNTER_COMPARE_B, 0);//设置CMPB的值 EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO);//设置B比较值加载模式 EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); //ePWMA的 EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(myEPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setRisingEdgeDeadBandDelayInput(myEPWM1_BASE,EPWM_DB_INPUT_EPWMA); EPWM_setFallingEdgeDeadBandDelayInput(myEPWM1_BASE,EPWM_DB_INPUT_EPWMA); //配置死区输入模式 EPWM_setDeadBandDelayPolarity(myEPWM1_BASE,EPWM_DB_RED,EPWM_DB_POLARITY_ACTIVE_HIGH); EPWM_setDeadBandDelayPolarity(myEPWM1_BASE,EPWM_DB_FED,EPWM_DB_POLARITY_ACTIVE_LOW);//配置极性 EPWM_setDeadBandDelayMode(myEPWM1_BASE,EPWM_DB_RED,true); EPWM_setDeadBandDelayMode(myEPWM1_BASE,EPWM_DB_FED,true); //配置输出模式 EPWM_setDeadBandOutputSwapMode(myEPWM1_BASE,EPWM_DB_OUTPUT_A,false); EPWM_setDeadBandOutputSwapMode(myEPWM1_BASE,EPWM_DB_OUTPUT_B,false); //输出不交换 EPWM_setRisingEdgeDelayCount(myEPWM1_BASE,28); //上升沿延时0nS EPWM_setFallingEdgeDelayCount(myEPWM1_BASE,28); //下降沿延时0nS } void PinMuxEPWM3_init() { // // EPWM1 -> myEPWM1 Pinmux // GPIO_setPinConfig(GPIO_4_EPWM3A); GPIO_setPinConfig(GPIO_5_EPWM3B); } void PinMuxEPWM2_init() { // // EPWM1 -> myEPWM1 Pinmux // GPIO_setPinConfig(GPIO_2_EPWM2A); GPIO_setPinConfig(GPIO_3_EPWM2B); } void PinMuxEPWM1_init() { // // EPWM1 -> myEPWM1 Pinmux // GPIO_setPinConfig(GPIO_0_EPWM1A); GPIO_setPinConfig(GPIO_1_EPWM1B); }
一、在本论坛找到了一个帖子,照着改了下,发现pwm2和pwm3无法同时移相,具体如下:
1,PWM1正常开启,当开启pwm2和pwm3的时候,并同时设置pwm2和pwm3的相位角,发现只有pwm2的相位正常改变,pwn3的相位不动,;
2,PWM1正常开启,当把pwm2关闭,开启pwm3的时候,并同时设置pwm3的相位角,发现pwn3的相位正常改变,;
3,请问这是什么原因?
二、我需要实现的功能是:
1、PWM1A和PWM1B,PWM2A和PWM2B,PWM3A和PWM3B带死区互补输出;
2、通实时改变PWM1,2,3三组六路的频率,精度是0.1HZ;
3,PWM2A/B和PWM3A/B 相对于PWM1移相输出;
Hi,
我们的技术支持基于TI的例程。
EPWM2、3要相对于EPWM1移相,您需要设置EPWM1的同步输出信号,比如在CTR=0或CTR=PRD时输出;还需要设置EPWM2的同步输入信号为EPWM1的同步输出信号,并将这个信号直通给EPWM3。这样便实现了同步,然后EPWM2、3便会根据您配置的移相值,在同步信号到来时装载移相值进行移相。
(EPWM同步信号链)
死区互补输出是通过配置DB来实现的:
详细的配置请您阅读sprui33f_TMS320F28004x Real-Time Microcontrollers Technical Reference Manual (Rev. F) Chapter 18 Enhanced Pulse Width Modulator (ePWM)
我们只能给您提供一个大概的思路,或者为您解释困扰您的某个点。具体的代码实现您需要靠自己。TI提供的例程全部都在SDK中了。
--
谢谢