This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求解:自制F28069板子,使用controlSTICK的BlinkingLED例程,Flash中不能单机运行

1.选用F28069M的芯片,硬件电路跟TI提供的原理图基本相同;

2.使用controlSTICK的BlinkingLED例程可以在线进行RAM和FLASH仿真调试,但要是在FLASH中单机运行,上电/复位程序不能自行运行,硬件引导模式确认没有问题

3.测得复位电平正常

疑问:1.controlSTICK的BlinkingLED例程能否在单机模式下单独运行,要想上电或复位能正常启动,我该如何操作?

2. 我按硬件BOOTROM调整GPIO34、GPIO37和/TRST来选择模式,也不能正常启动,这是什么原因?

麻烦ti的技术人员能给我分析一下原因,该如何操作才能正常运行,谢谢!