我使用的F28335的controlSUITE里面提供F2833x Real FFT ,在开发板上跑了一遍,
输入波形如下:


经过FFT后的输出波形如下,感觉有点问题,不知道错在哪里,求助各位专家?????
源码如下:
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#include "math.h"
#include "float.h"
#include "FPU.h"
#define RFFT_STAGES 8
#define RFFT_SIZE (1 << RFFT_STAGES)
#pragma DATA_SECTION(RFFTin1Buff,"RFFTdata1"); //Buffer alignment for the input array,
float32 RFFTin1Buff[RFFT_SIZE]; //RFFT_f32u(optional), RFFT_f32(required)
//Output of FFT overwrites input if
//RFFT_STAGES is ODD
#pragma DATA_SECTION(RFFToutBuff,"RFFTdata2");
float32 RFFToutBuff[RFFT_SIZE]; //Output of FFT here if RFFT_STAGES is EVEN
#pragma DATA_SECTION(RFFTmagBuff,"RFFTdata3");
float32 RFFTmagBuff[RFFT_SIZE/2+1]; //Additional Buffer used in Magnitude calc
#pragma DATA_SECTION(RFFTF32Coef,"RFFTdata4");
float32 RFFTF32Coef[RFFT_SIZE]; //Twiddle buffer
float RadStep = 0.1963495408494f; // Step to generate test bench waveform
float Rad = 0.0f;
RFFT_F32_STRUCT rfft;
void main(void)
{
Uint16 i;
InitSysCtrl();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
// Clear input buffers:
for(i=0; i < RFFT_SIZE; i++)
{
RFFTin1Buff[i] = 0.0f;
}
// Generate sample waveforms:
Rad = 0.0f;
for(i=0; i < RFFT_SIZE; i++)
{
RFFTin1Buff[i] = sin(Rad) + cos(Rad*2.3567); //Real input signal
//FFTImag_in[i] = cos(Rad*8.345) + sin(Rad*5.789);
Rad = Rad + RadStep;
}
rfft.FFTSize = RFFT_SIZE;
rfft.FFTStages = RFFT_STAGES;
rfft.InBuf = &RFFTin1Buff[0]; //Input buffer
rfft.OutBuf = &RFFToutBuff[0]; //Output buffer
rfft.CosSinBuf = &RFFTF32Coef[0]; //Twiddle factor buffer
rfft.MagBuf = &RFFTmagBuff[0]; //Magnitude buffer
RFFT_f32_sincostable(&rfft); //Calculate twiddle factor
for (i=0; i < RFFT_SIZE; i++)
{
RFFToutBuff[i] = 0; //Clean up output buffer
}
for (i=0; i < RFFT_SIZE/2; i++)
{
RFFTmagBuff[i] = 0; //Clean up magnitude buffer
}
RFFT_f32(&rfft); //Calculate real FFT
// OutBuf[0] = real[0]
// OutBuf[1] = real[1]
// OutBuf[2] = real[2]
// 厖?
// OutBuf[N/2] = real[N/2]
// OutBuf[N/2+1] = imag[N/2-1]
// 厖?
// OutBuf[N-3] = imag[3]
// OutBuf[N-2] = imag[2]
// OutBuf[N-1] = imag[1]
//
RFFT_f32_mag(&rfft); //Calculate magnitude
// MagBuf[0] = magnitude[0]
// MagBuf[1] = magnitude[1]
// MagBuf[2] = magnitude[2]
// 厖?
// MagBuf[N/2] = magnitude[N/2]
// MagBuf[N/2+1] = magnitude[N/2+1]
// rfft.PhaseBuf = &RFFTmagBuff[0]; //Use magnitude buffer
// RFFT_f32_phase(&rfft); //Calculate phase
// Just sit and loop forever (optional):
for(;;);
} //End of main
.cmd文件如下:
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002 /* Boot to M0 will go here */
RAMM0 : origin = 0x000050, length = 0x0003B0
RAML0 : origin = 0x008000, length = 0x001000
RAML1 : origin = 0x009000, length = 0x001000
RAML2 : origin = 0x00A000, length = 0x001000
RAML3 : origin = 0x00B000, length = 0x001000
ZONE7A : origin = 0x200000, length = 0x00FC00 /* XINTF zone 7 - program space */
CSM_RSVD : origin = 0x33FF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
ADC_CAL : origin = 0x380080, length = 0x000009
RESET : origin = 0x3FFFC0, length = 0x000002
IQTABLES : origin = 0x3FE000, length = 0x000b50
IQTABLES2 : origin = 0x3FEB50, length = 0x00008c
FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0
BOOTROM : origin = 0x3FF27C, length = 0x000D44
PAGE 1 :
/* BOOT_RSVD is used by the boot ROM for stack. */
/* This section is only reserved to keep the BOOT ROM from */
/* corrupting this area during the debug process */
BOOT_RSVD : origin = 0x000002, length = 0x00004E /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML4 : origin = 0x00C000, length = 0x001000
RAML5 : origin = 0x00D000, length = 0x001000
RAML6 : origin = 0x00E000, length = 0x001000
RAML7 : origin = 0x00F000, length = 0x001000
ZONE7B : origin = 0x20FC00, length = 0x000400 /* XINTF zone 7 - data space */
}
SECTIONS
{
/* Setup for "boot to SARAM" mode:
The codestart section (found in DSP28_CodeStartBranch.asm)
re-directs execution to the start of user code. */
codestart : > BEGIN, PAGE = 0
ramfuncs : > RAML0, PAGE = 0
.text : > RAML1, PAGE = 0
.cinit : > RAML0, PAGE = 0
.pinit : > RAML0, PAGE = 0
.switch : > RAML0, PAGE = 0
.stack : > RAMM1, PAGE = 1
.ebss : > RAML4, PAGE = 1
.econst : > RAML5, PAGE = 1
.esysmem : > RAMM1, PAGE = 1
IQmath : > RAML1, PAGE = 0
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
DMARAML4 : > RAML4, PAGE = 1
DMARAML5 : > RAML5, PAGE = 1
DMARAML6 : > RAML6, PAGE = 1
DMARAML7 : > RAML7, PAGE = 1
ZONE7DATA : > ZONE7B, PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used */
csm_rsvd : > CSM_RSVD PAGE = 0, TYPE = DSECT /* not used for SARAM examples */
csmpasswds : > CSM_PWL PAGE = 0, TYPE = DSECT /* not used for SARAM examples */
/* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
.adc_cal : load = ADC_CAL, PAGE = 0, TYPE = NOLOAD
RFFTdata1 : > RAML7, PAGE = 1 //add for RFFT,2014-03-27
RFFTdata2 : > RAML7, PAGE = 1
RFFTdata3 : > RAML7, PAGE = 1
RFFTdata4 : > RAML7, PAGE = 1
FFTBUF ALIGN( 512 ) : { } > RAML6 PAGE 1
}