This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用得F28027,CCS3.3
输入的input[N]图形如下,inputFFT为FFT Magnitude下的图形:
下图为magTest[ ]的64点与128点时图形,个人感觉不对,应该要同inputFFT一样才对啊,是不是哪里用错了?
代码如下:
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File #include <fft.h> #include"math.h" // Prototype statements for functions found within this file. interrupt void adc_isr(void); void Adc_Config(void); // Global variables used in this example: Uint16 LoopCount; #if 0 Uint16 ConversionCount; Uint16 Voltage1[10]; Uint16 Voltage2[10]; #endif #define PI 3.1415926 #define N 128 long ipcb[N+2]; long mag[N/2+1]; long magTest[N/2+1]; #pragma DATA_SECTION(ipcb, "FFTipcb"); #pragma DATA_SECTION(mag, "FFTmag"); RFFT32 fft=RFFT32_128P_DEFAULTS; RFFT32_ACQ acq=FFTRACQ_DEFAULTS; #if 1 unsigned int input[N]= { 0x000,0x00b,0x02c,0x062,0x0ac,0x109,0x176,0x1f1,0x307,0x39b, 0x432,0x4c7,0x558,0x5e2,0x661,0x6d4,0x736,0x787,0x7c4,0x7ec, 0x7fe,0x7ec,0x7c4,0x787,0x736,0x6d4,0x661,0x5e2,0x558,0x4c7, 0x432,0x39b,0x307,0x1f1,0x176,0x109,0x0ac,0x062,0x02c,0x00b, 0x000,0x00b,0x02c,0x062,0x0ac,0x109,0x176,0x1f1,0x307,0x39b, 0x432,0x4c7,0x558,0x5e2,0x661,0x6d4,0x736,0x787,0x7c4,0x7ec, 0x7fe,0x7ec,0x7c4,0x787,0x736,0x6d4,0x661,0x5e2,0x558,0x4c7, 0x432,0x39b,0x307,0x1f1,0x176,0x109,0x0ac,0x062,0x02c,0x00b, 0x000,0x00b,0x02c,0x062,0x0ac,0x109,0x176,0x1f1,0x307,0x39b, 0x432,0x4c7,0x558,0x5e2,0x661,0x6d4,0x736,0x787,0x7c4,0x7ec, 0x7fe,0x7ec,0x7c4,0x787,0x736,0x6d4,0x661,0x5e2,0x558,0x4c7, 0x432,0x39b,0x307,0x1f1,0x176,0x109,0x0ac,0x062,0x02c,0x00b, 0x000,0x00b,0x02c,0x062,0x0ac,0x109,0x176,0x1f1 }; #endif #if 0 void MakeWave(void) { int i; for ( i=0;i<N;i++ ) { //INPUT[i]=sin(PI*2*i/SAMPLENUMBER*3)*1024; input[i]=sin(PI*2*i/N*3)*1024+1024; } } #endif main() { int i; unsigned int *pInput; pInput=input; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2803x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initialize GPIO: // This example function is found in the DSP2802x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2802x_PieCtrl.c file. InitPieCtrl(); /* Initialize acquisition module */ acq.buffptr=ipcb; acq.tempptr=ipcb; acq.size=N; acq.count=N; acq.acqflag=1; /* Initialize FFT module */ fft.ipcbptr=ipcb; fft.magptr=mag; // fft.winptr=(long *)win; fft.init(&fft); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2802x_DefaultIsr.c. // This function is found in DSP2802x_PieVect.c. InitPieVectTable(); for(;;) { LoopCount++; for(i=0;i<N;i++) { acq.input=((unsigned long)pInput[i])<<16; acq.update(&acq); } if (acq.acqflag==0) // If the samples are acquired { fft.calc(&fft); fft.split(&fft); fft.mag(&fft); acq.acqflag=1; // Enable the next acquisition for(i=0;i<N/2+1;i++) { magTest[i]=sqrt(mag[i]); } } } }