Part Number: TMS320F28377S
Dear TI' experts:
I have some issues when I use CCS and UIA about SYS/biose analysis tools.
- Goles: Analyzing the Execution Sequence with RTOS Analyzer
1.1 The versions of the APP:
|
CCS |
CCS v11.1.0.00011 |
|
Compiler |
C2000 Compiler v21.12.0.STS |
|
XDCtools |
XDCtools v3.62.1.16.core |
|
SYS/BIOS |
SYS/BIOS v6.83.0.18 |
|
UIA |
uia_2_30_01_02 |
|
Target |
ti.targets.C28_float |
1.2 The configuration of the UIA "Logging Setup"


2.0 The abnormal phenomenon
2.1

Received exception from ROV:server Target memory read failed at address :0x04, length :26,This read is an
INVALID address according to the application's section map .The application is likely either unintialized or corrupt.
I can not get messaage from the "RTOS Object View " "Records". See the up picture.
2.2
But when the debug is running for 3 senonds ,then hold the debug , it will get some messangs . See the bellow picture.