This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: 同步Buck电路的负载调整率问题

Part Number: TMS320F28379D


各位好,

我现在在做一个Buck电路,输入为30~100V,输出为7V,负载为3-7A。开关频率50kHz,滤波器C=300uF,L=100uF

采用28379D launchpad控制,单电压环,补偿器为PI。

目前的负载调整率不尽如人意:轻载(0.5A)时,输出正常7V。加载以后,如1.2A~6.72V,2.4A~6.62V。

我还没有做进一步的测试,想请问这个情况可能的原因是什么呢?通过调整PI补偿器参数能够解决么?

感谢您的关注!期待您的回答!