This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的28335,调用controlsuilt的定点FFT库例程计算512点FFT,代码如下,输出的是幅值的平方,而且是Q30格式,
fft.mag(&fft); /* Q31 format (abs(ipcbsrc)/2^16).^2 */ , 请问怎么将输出的幅值还原成真实值?
//###################################################################################### // $TI Release: C28x Fixed Point Library v1.01 $ // $Release Date: January 11,2011 $ //###################################################################################### #include "DSP28x_Project.h" #include <fft.h> #include "math.h" #include "float.h" /* Create an Instance of FFT module */ #define N 512 // FFT size #pragma DATA_SECTION(ipcb, "FFTipcb"); // Input/output memory allocation #pragma DATA_SECTION(ipcbsrc, "FFTipcbsrc"); long ipcbsrc[2*N]; long ipcb[2*N]; RFFT32 fft=RFFT32_512P_DEFAULTS; // Header structure definition /* Define window Co-efficient Array and place the .constant section in ROM memory */ const long win[N/2]=HAMMING32; // Select window, not used in this example int xn,yn; float RadStep = 0.1963495408494f; // Simulated signal generation parameter float Rad = 0.0f; // Initial value of Radstep void main() { unsigned long i; InitSysCtrl(); DINT; InitPieCtrl(); IER = 0x0000; IFR = 0x0000; InitPieVectTable(); EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // Generate sample waveforms: Rad = 0.0f; //Clean up input/output buffer for(i=0; i < (N*2); i=i+2) { ipcb[i] =0; ipcb[i+1] = 0; } //Simulated input signal for(i=0; i < N; i++) { ipcbsrc[i] =(long)(2147483648*(sin(Rad) + cos(Rad*2.3567))/2); //Q31 Rad = Rad + RadStep; } /*--------------------------------------------------------------------------- FFT Calculation ----------------------------------------------------------------------------*/ RFFT32_brev(ipcbsrc, ipcb, N); /* real FFT bit reversing */ fft.ipcbptr=ipcb; /* FFT computation buffer */ fft.magptr=ipcbsrc; /* Magnitude output buffer */ fft.winptr=(long *)win; /* Window coefficient array */ fft.init(&fft); /* Twiddle factor pointer initialization */ fft.calc(&fft); /* Compute the FFT */ fft.mag(&fft); /* Q31 format (abs(ipcbsrc)/2^16).^2 */ //asm(" ESTOP0"); for(;;); } /* End: main() */