| F28335的板子在CCS V4环境下连XDS100 V2的仿真器,在点击connect的时候一直报错如下: Error connecting to the target: Error 0x80000200/-1041 Fatal Error during: OCS, Device driver: Problem with the Emulation Controller. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. |
报错好久了,一直不能解决,求大神指导!