Part Number: TMS320F28335
使用28335上的XINTF端口与FPGA进行通信时,在dsp将一个指针指定到0x4002地址上,在主程序中对该指针进行幅值操作,理论上dsp应该会自动拉低xzcs0选区线,并在XA[19:0]上送相应地址,但我测的时候发现 XA0一直为高电平,且XZCS0选区线也为高电平。(在进行此操作前已经对xintf外部接口进行初始化,使用的数据宽度为16位)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
使用28335上的XINTF端口与FPGA进行通信时,在dsp将一个指针指定到0x4002地址上,在主程序中对该指针进行幅值操作,理论上dsp应该会自动拉低xzcs0选区线,并在XA[19:0]上送相应地址,但我测的时候发现 XA0一直为高电平,且XZCS0选区线也为高电平。(在进行此操作前已经对xintf外部接口进行初始化,使用的数据宽度为16位)
您好,我之前是使用万用表测的该引脚,对比其他地址位的引脚它一直是3.3V,但是今天写了一个使用偶数地址发指令给FPGA,发现FPGA也是可以响应的。
代码如下
#include "DSP2833x.Device.h"
#include "DSP2833x_Examples.h"
unsigned int * openlight=(unsigned int *) 0x4002;
int main(void)
{
InitSysCtrl();
EALLOW;
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 0; // GPIO5 = GPIO5
GpioCtrlRegs.GPADIR.bit.GPIO18 = 1;
EDIS;
DINT;
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
InitPieVectTable();
InitXintf();
while(1)
{
* openled=0x400a;
}
return 0;
}
FPGA的程序如下
inital
begin
led_1=1'b0;
end
always@(posedge CLK_IN)
begin
if(XADD==16'h0x4002&&XZCS0==1'b0)
begin led_1<=1'b1;end
end