This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2812将程序下载到RAM进行仿真调试和将程序烧写至FLASH内进行硬件调试时,GPIOF引脚状态是不是一样的?

疑问一:F2812将程序下载到RAM进行仿真调试和将程序烧写至FLASH内进行硬件调试时,GPIOF引脚状态是不是一样的?对于一个已经设计好的DSP系统,引脚状态在硬件上已经固定好了,是不是此时只能局限于一种引导模式了?因为仿真调试时,用户程序入口地址一般在SARAMH0处,烧写至FLASH内进行允许时,用户程序入口地址在FLASH处,那怎么既可以下载到RAM,也可以将程序烧写至FLASH

疑问二:CMD文件中   .reset           : > RESET,       PAGE = 0, TYPE = DSECT /* not used, */

.reset         复位中断向量表   不用代表什么意思。。。位于Ox3FFFC0的复位向量指向InitBoot,不用的话,怎么启动引导操作

等待大神解答