This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有F28M35x ADC结果使用DMA传输的例程吗

您好:请问有F28M35x ADC结果使用DMA传输的例程吗?
我之前浏览了F28M35x的数据表、技术参考手册和最新的Controlsuite3.2.9都没有找到F28M35x ADC结果使用DMA传输的例程。

 

  • 反正我是没有找到,自己写吧,把例程中的dma_ram_to_ram的参数稍微改一下,搬到workshop的lab4-1,稍微修改就差不多了。碰巧我前两天也在做这一块。

  • ''搬到workshop的lab4-1'',没明白什么意思。

    除例程中的dma_ram_to_ram外,最值得参考的应该是Example_2833xAdcToDMA.c了。可惜F28M35x中的ADC模块优化改进了,Example_2833xAdcToDMA.c中的代码不能直接使用。

    您的F28M35x ADC结果使用DMA传输的程序写出来了吗?可否共享交流一下?

  • workshop是TI给的一些实验以及例程,lab4-1是关于ADC配置的。我这边有,但是里面交杂的有其他模块的程序就是。

  • //###########################################################################
    //real sampling and real firlting;
    //###########################################################################
    //

    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File
    #include <string.h>
    #include "FPU.h"
    #include "math.h"
    #include "float.h"
    #include "config.h"


    #define C28_FREQ 150 //C28 CPU frequency in MHz

    extern Uint16 RamfuncsLoadStart;
    extern Uint16 RamfuncsLoadSize;
    extern Uint16 RamfuncsRunStart;

    extern float Value_num;
    void config_ADC1(void);

    void main(void)
    {
    InitSysCtrl(); // Init C28 core
    EALLOW;
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = ePWM1A
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO0 = ePWM1B
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO0 = ePWM2A
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO0 = ePWM2B
    EDIS;

    // Copy time critical code and Flash setup code to RAM
    // This includes the following functions: InitFlash();
    // The RamfuncsLoadStart, RamfuncsLoadSize and RamfuncsRunStart
    // symbols are created by the linker. Refer to the device .cmd file.
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);

    // Call Flash Initialization to setup flash waitstates
    // This function must reside in RAM
    InitFlash();

    Init_firFP();
    Value_num=CC_TBPRD/4095.0; // CMPA/B=(fir_A0/2^12)*CC_TBPRD=fir_A0*Value_num

    InitAdc1();
    config_ADC1();

    config_PWM();

    DINT;
    InitPieCtrl();
    IER=0x0000;
    IFR=0x0000;
    InitPieVectTable();
    EALLOW; // This is needed to write to EALLOW protected registers
    PieVectTable.ADCINT1 = &ADCINT1_ISR;
    EDIS;


    InitCpuTimers();
    ConfigCpuTimer(&CpuTimer0, C28_FREQ, 100); //AD采样间隔 100us
    //Enable INT
    PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
    IER |= M_INT1;
    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM

    CpuTimer0Regs.TCR.bit.TSS = 0; // start T0

    while(1) ;
    }

    void config_ADC1(void)
    {

    InitAdc1();
    EALLOW;
    Adc1Regs.ADCCTL2.bit.ADCNONOVERLAP = 1; // Enable non-overlap mode i.e. Overlap of sample is not allowed

    Adc1Regs.ADCCTL1.bit.INTPULSEPOS = 1; // ADCINT1 trips after AdcResults latch
    Adc1Regs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
    Adc1Regs.INTSEL1N2.bit.INT1CONT = 1; // Disable ADCINT1 Continuous mode
    Adc1Regs.INTSEL1N2.bit.INT1SEL = 3; // setup EOC0 to trigger ADCINT1 to fire

    AnalogSysctrlRegs.TRIG1SEL.all = 1; // Assigning TINT0 to ADC-TRIGGER 1
    AnalogSysctrlRegs.CCLKCTL.all =ACLKDIV4; //ASYSCLK=PLLCLK/ACLKDIV

    Adc1Regs.ADCSOC0CTL.bit.CHSEL = 0; // set SOC0 channel select to ADC1in_A0
    Adc1Regs.ADCSOC0CTL.bit.TRIGSEL = 5; // Set SOC0 start trigger1
    Adc1Regs.ADCSOC0CTL.bit.ACQPS = 6; // set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC1CTL.bit.CHSEL = 8; // set SOC1 channel select to ADC1in_A0
    Adc1Regs.ADCSOC1CTL.bit.TRIGSEL = 5; // Set SOC1 start trigger1
    Adc1Regs.ADCSOC1CTL.bit.ACQPS = 6; // set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC2CTL.bit.CHSEL = 2; // set SOC2 channel select to ADC1in_A0
    Adc1Regs.ADCSOC2CTL.bit.TRIGSEL = 5; // Set SOC2 start trigger1
    Adc1Regs.ADCSOC2CTL.bit.ACQPS = 6; // set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC3CTL.bit.CHSEL = 3; // set SOC3 channel select to ADC1in_A0
    Adc1Regs.ADCSOC3CTL.bit.TRIGSEL = 5; // Set SOC3 start trigger1
    Adc1Regs.ADCSOC3CTL.bit.ACQPS = 6; // set SOC3 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    EDIS;
    }

  • 上面程序是ADC4通道的采样结果,放在RAM L2的adc_buffer里,其中config_PWM();这个函数忘记注释掉了,这个你不需要用。

  • Init_firFP();
    Value_num=CC_TBPRD/4095.0; // CMPA/B=(fir_A0/2^12)*CC_TBPRD=fir_A0*Value_num

    这两行也要去了,不需要用。

  • qiuhong yao 说:

    //###########################################################################
    //real sampling and real firlting;
    //###########################################################################
    //

    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File
    #include <string.h>
    #include "FPU.h"
    #include "math.h"
    #include "float.h"
    #include "config.h"


    #define C28_FREQ 150 //C28 CPU frequency in MHz

    extern Uint16 RamfuncsLoadStart;
    extern Uint16 RamfuncsLoadSize;
    extern Uint16 RamfuncsRunStart;

    extern float Value_num;
    void config_ADC1(void);

    void main(void)
    {
    InitSysCtrl(); // Init C28 core
    EALLOW;
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = ePWM1A
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO0 = ePWM1B
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO0 = ePWM2A
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO0 = ePWM2B
    EDIS;

    // Copy time critical code and Flash setup code to RAM
    // This includes the following functions: InitFlash();
    // The RamfuncsLoadStart, RamfuncsLoadSize and RamfuncsRunStart
    // symbols are created by the linker. Refer to the device .cmd file.
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);

    // Call Flash Initialization to setup flash waitstates
    // This function must reside in RAM
    InitFlash();

    Init_firFP();
    Value_num=CC_TBPRD/4095.0; // CMPA/B=(fir_A0/2^12)*CC_TBPRD=fir_A0*Value_num

    InitAdc1();
    config_ADC1();

    config_PWM();

    DINT;
    InitPieCtrl();
    IER=0x0000;
    IFR=0x0000;
    InitPieVectTable();
    EALLOW; // This is needed to write to EALLOW protected registers
    PieVectTable.ADCINT1 = &ADCINT1_ISR;
    EDIS;


    InitCpuTimers();
    ConfigCpuTimer(&CpuTimer0, C28_FREQ, 100); //AD采样间隔 100us
    //Enable INT
    PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
    IER |= M_INT1;
    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM

    CpuTimer0Regs.TCR.bit.TSS = 0; // start T0

    while(1) ;
    }

    void config_ADC1(void)
    {

    InitAdc1();
    EALLOW;
    Adc1Regs.ADCCTL2.bit.ADCNONOVERLAP = 1; // Enable non-overlap mode i.e. Overlap of sample is not allowed

    Adc1Regs.ADCCTL1.bit.INTPULSEPOS = 1; // ADCINT1 trips after AdcResults latch
    Adc1Regs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
    Adc1Regs.INTSEL1N2.bit.INT1CONT = 1; // Disable ADCINT1 Continuous mode
    Adc1Regs.INTSEL1N2.bit.INT1SEL = 3; // setup EOC0 to trigger ADCINT1 to fire

    AnalogSysctrlRegs.TRIG1SEL.all = 1; // Assigning TINT0 to ADC-TRIGGER 1
    AnalogSysctrlRegs.CCLKCTL.all =ACLKDIV4; //ASYSCLK=PLLCLK/ACLKDIV

    Adc1Regs.ADCSOC0CTL.bit.CHSEL = 0; // set SOC0 channel select to ADC1in_A0
    Adc1Regs.ADCSOC0CTL.bit.TRIGSEL = 5; // Set SOC0 start trigger1
    Adc1Regs.ADCSOC0CTL.bit.ACQPS = 6; // set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC1CTL.bit.CHSEL = 8; // set SOC1 channel select to ADC1in_A0
    Adc1Regs.ADCSOC1CTL.bit.TRIGSEL = 5; // Set SOC1 start trigger1
    Adc1Regs.ADCSOC1CTL.bit.ACQPS = 6; // set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC2CTL.bit.CHSEL = 2; // set SOC2 channel select to ADC1in_A0
    Adc1Regs.ADCSOC2CTL.bit.TRIGSEL = 5; // Set SOC2 start trigger1
    Adc1Regs.ADCSOC2CTL.bit.ACQPS = 6; // set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC3CTL.bit.CHSEL = 3; // set SOC3 channel select to ADC1in_A0
    Adc1Regs.ADCSOC3CTL.bit.TRIGSEL = 5; // Set SOC3 start trigger1
    Adc1Regs.ADCSOC3CTL.bit.ACQPS = 6; // set SOC3 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    EDIS;
    }

    首先感谢您的积极解答和分享。但我注意到以上代码里没有DMA传输的设置。您的F28M35x ADC结果“使用DMA传输”的程序写出来了吗?可否分享交流一下?

  • 哎呀,失误失误,我当时打开的文件太多了,把一个类似文件的内容拷贝过来了。

    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File
    #include <string.h>
    #include "FPU.h"
    #include "math.h"
    #include "float.h"
    #include "config.h"


    #define C28_FREQ 150 //C28 CPU frequency in MHz

    extern Uint16 RamfuncsLoadStart;
    extern Uint16 RamfuncsLoadSize;
    extern Uint16 RamfuncsRunStart;

    extern float Value_num;
    Uint16 Gpio70_count;

    #pragma DATA_SECTION(adc_buffer, "DMARAML2")

    volatile Uint16 adc_buffer[40];
    volatile Uint16 *DMADest;
    volatile Uint16 *DMASource;
    interrupt void local_DINTCH1_ISR(void);

    void config_ADC1(void);

    void main(void)
    {
    InitSysCtrl(); // Init C28 core
    EALLOW;

    GpioCtrlRegs.GPCMUX1.bit.GPIO70=0;
    GpioCtrlRegs.GPCDIR.bit.GPIO70=1;

    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = ePWM1A
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO0 = ePWM1B
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO0 = ePWM2A
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO0 = ePWM2B
    EDIS;

    // Copy time critical code and Flash setup code to RAM
    // This includes the following functions: InitFlash();
    // The RamfuncsLoadStart, RamfuncsLoadSize and RamfuncsRunStart
    // symbols are created by the linker. Refer to the device .cmd file.
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);

    // Call Flash Initialization to setup flash waitstates
    // This function must reside in RAM
    InitFlash();

    // Init_firFP();
    // Value_num=CC_TBPRD/4095.0; // CMPA/B=(fir_A0/2^12)*CC_TBPRD=fir_A0*Value_num


    config_ADC1();

    // config_PWM();

    DINT;
    InitPieCtrl();
    IER=0x0000;
    IFR=0x0000;
    InitPieVectTable();
    EALLOW; // This is needed to write to EALLOW protected registers
    // PieVectTable.ADCINT1 = &ADCINT1_ISR;
    PieVectTable.DINTCH1 = &local_DINTCH1_ISR;
    EDIS;

    DMADest=adc_buffer;
    DMASource=&Adc1Result.ADCRESULT0;
    DMAInitialize();
    DMACH1AddrConfig(DMADest,DMASource);
    DMACH1BurstConfig(3,1,10);
    DMACH1TransferConfig(9,0xfffd,0xffe3);
    DMACH1WrapConfig(0xffff,0,0xffff,0);

    DMACH1ModeConfig(DMA_ADCINT1,PERINT_ENABLE,ONESHOT_DISABLE,CONT_DISABLE,
    SYNC_DISABLE,SYNC_SRC,OVRFLOW_DISABLE,SIXTEEN_BIT,
    CHINT_END,
    CHINT_ENABLE);

    InitCpuTimers();
    ConfigCpuTimer(&CpuTimer0, C28_FREQ, 100); //AD采样间隔 100us
    //Enable INT
    // PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
    IER |= M_INT7;
    EnableInterrupts();
    // EINT; // Enable Global interrupt INTM
    // ERTM; // Enable Global realtime interrupt DBGM
    GpioDataRegs.GPCDAT.bit.GPIO70=0;


    CpuTimer0Regs.TCR.bit.TSS = 0; // start T0

    StartDMACH1();

    while(1) ;
    }

    __interrupt void local_DINTCH1_ISR(void)
    {

    // if(Gpio70_count++==1000)
    // {
    GpioDataRegs.GPCDAT.bit.GPIO70^=1;
    // Gpio70_count=0;
    // }

    PieCtrlRegs.PIEACK.all = PIEACK_GROUP7;
    StartDMACH1();
    }

    void config_ADC1(void)
    {

    InitAdc1();
    EALLOW;
    Adc1Regs.ADCCTL2.bit.ADCNONOVERLAP = 1; // Enable non-overlap mode i.e. Overlap of sample is not allowed

    Adc1Regs.ADCCTL1.bit.INTPULSEPOS = 1; // ADCINT1 trips after AdcResults latch
    Adc1Regs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
    Adc1Regs.INTSEL1N2.bit.INT1CONT = 1; // Disable ADCINT1 Continuous mode
    Adc1Regs.INTSEL1N2.bit.INT1SEL = 3; // setup EOC0 to trigger ADCINT1 to fire

    AnalogSysctrlRegs.TRIG1SEL.all = 1; // Assigning TINT0 to ADC-TRIGGER 1
    AnalogSysctrlRegs.CCLKCTL.all =ACLKDIV4; //ASYSCLK=PLLCLK/ACLKDIV

    Adc1Regs.ADCSOC0CTL.bit.CHSEL = 0; // set SOC0 channel select to ADC1in_A0
    Adc1Regs.ADCSOC0CTL.bit.TRIGSEL = 5; // Set SOC0 start trigger1
    Adc1Regs.ADCSOC0CTL.bit.ACQPS = 6; // set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC1CTL.bit.CHSEL = 8; // set SOC1 channel select to ADC1in_A0
    Adc1Regs.ADCSOC1CTL.bit.TRIGSEL = 5; // Set SOC1 start trigger1
    Adc1Regs.ADCSOC1CTL.bit.ACQPS = 6; // set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC2CTL.bit.CHSEL = 2; // set SOC2 channel select to ADC1in_A0
    Adc1Regs.ADCSOC2CTL.bit.TRIGSEL = 5; // Set SOC2 start trigger1
    Adc1Regs.ADCSOC2CTL.bit.ACQPS = 6; // set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    Adc1Regs.ADCSOC3CTL.bit.CHSEL = 3; // set SOC3 channel select to ADC1in_A0
    Adc1Regs.ADCSOC3CTL.bit.TRIGSEL = 5; // Set SOC3 start trigger1
    Adc1Regs.ADCSOC3CTL.bit.ACQPS = 6; // set SOC3 S/H Window to 7 ADC Clock Cycles, (6 ACQPS + 1)

    EDIS;
    }