This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C28X FPU的问题 , benchmark 的 cycle count对应时间是什么?



是不是SYSCLKOUT? 即CPU 时钟数? 我的一个FFT程序如下

    rfft_adc.Tail = &rfft.OutBuf;        // Link the RFFT_ADC_F32_STRUCT to
                                                   // RFFT_F32_STRUCT. Tail pointer of
                                                   // RFFT_ADC_F32_STRUCT is passed to
                                                   //  the OutBuf pointer of RFFT_F32_STRUCT
    rfft.FFTSize   = nRFFT_SIZE;
    rfft.FFTStages = nRFFT_STAGES;
    rfft_adc.InBuf = Signal_In;                     // Input buffer
    //rfft.InBuf     = Signal_In;                // Input buffer
    rfft.OutBuf    = &RFFT_Out_Buf[0];           // Output buffer
    rfft.CosSinBuf = &RFFT_Coef_Buf[0];          // Twiddle factor buffer
    rfft.MagBuf    = Signal_Mag;                 // Magnitude buffer
    rfft.PhaseBuf =  Signal_Phase;

    RFFT_f32_sincostable(&rfft);        // Calculate twiddle factor
    RFFT_adc_f32(&rfft_adc);            // Calculate real FFT with 12-bit ADC input

这段程序的执行时间 TI 给出的benchmark是 29466 cycle count, 我的系统是28335, 运行时钟是150M, RAM 使用片外RAM,测量下来所需时间是2508380*6.67ns = 16.7ms, 为什么会相差这么大? 我想了想,除了使用 片外RAM外,差别在哪里? 怎么会这样慢? 我在程序中使用了c28x   fast 库的。