This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: GPIO口通过Input X-BAR连接到epwm去触发DC模块,TRIP6不起作用

Part Number: TMS320F280049


GPIO口通过Input X-BAR连接到epwm去触发DC模块执行OST封波功能,通过配置如下:

InputXbarRegs.INPUT6SELECT = 0x1C;GPIO12

EPwm1Regs.DCTRIPSEL.bit.DCBLCOMPSEL = DC_TRIPIN6;

一直是封波状态.

当GPIO12配置成TRIP10

InputXbarRegs.INPUT10SELECT = 0x1C;GPIO12;

EPwmXbarRegs.TRIP10MUX16TO31CFG.bit.MUX23 = 1; //INPUT10

EPwmXbarRegs.TRIP10MUXENABLE.bit.MUX23 = 1;

EPwm1Regs.DCTRIPSEL.bit.DCBLCOMPSEL = DC_TRIPIN10;

可以实现GPIO电平实现epwm OST功能.

如图:TRIP6是不是还需要什么其他的配置.