This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: 关于多个EPWM模块时钟同步问题

Part Number: TMS320F28335

目的:要求同步EPWM1,EPWM2。

在使用EPWM模块同步功能时,配置时基时钟等于系统时钟,使EPWM1产生同步信号,使能EPWM2同步信号和使能TBCTL[PHSEN],令相位寄存器的值TBPHS的值为0,发现EPWM2和EPWM1相差两个系统时钟。这个可以在28335数据手册和相关参考书中可以找到依据,相关参考例程也是如此配置的。

但在实验中发现,保持其他条件不变,EPWM1产生同步信号,并传递给EPWM2,清除EPWM2的TBCTL[PHSEN]=0,发现此时EPWM1和EPWM2则保持完全同步,没有相差。但这种配置在数据手册中并无参考,不知道这种方式是否可靠?