This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急急急,CCS6 报"specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2800" specified in a previous file or on the command line"



3个问题:

1.  我目前的工程project链接了自己编写的lib1,而库1又包含lib2.请问最后的project是不是要把两个库都链接上?或者只要链接lib1就可以?

2.  目前我的库2里的函数是用IQmpy等库函数运算的,而库1和proect里的函数的计算是直接计算的,没有IQmpy等函数,请问最后在build option里怎么设置RTS lib?设置为哪个目前都会报类似下面的错误。

"specifies ISA revision "C28FPU32", which is not compatible with ISA revision  "C2800" specified in a previous file or on the command line"

3. 上述错误里还会出现C2800" 和C2700"不兼容的问题,请问ISA revision  C2800和C2700指什么?如何能修改?