3个问题:
1. 我目前的工程project链接了自己编写的lib1,而库1又包含lib2.请问最后的project是不是要把两个库都链接上?或者只要链接lib1就可以?
2. 目前我的库2里的函数是用IQmpy等库函数运算的,而库1和proect里的函数的计算是直接计算的,没有IQmpy等函数,请问最后在build option里怎么设置RTS lib?设置为哪个目前都会报类似下面的错误。
"specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2800" specified in a previous file or on the command line"
3. 上述错误里还会出现C2800" 和C2700"不兼容的问题,请问ISA revision C2800和C2700指什么?如何能修改?