您好,
我在用28379D Launch Pad的ADC读取DAC输出时结果对不上,如下图DAC输出3000.ADC读取为2924

请问这个该如何校准?
下面是我的代码
//
// Included Files
//
#include "F28x_Project.h"
typedef unsigned char Uint8;
//
// Function Prototypes
//
void ConfigureADC(void);
void SetupADCContinuous();
void configureDAC();
void gpio_init();
//
// Globals
//
Uint16 AdcaResult;
Uint16 dacval = 3000;
void main(void)
{
InitSysCtrl();
InitGpio(); // Skipped for this example
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
configureDAC();
//
// Configure the ADC and power it up
//
ConfigureADC();
//
// Setup the ADC for continuous conversions on channel 0
//
SetupADCContinuous();
//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// take conversions indefinitely in loop
//
do
{
DacaRegs.DACVALS.all = dacval;//选DAC?
DELAY_US(2);
//
//enable ADCINT flags
//
EALLOW;
AdcaRegs.ADCINTSEL1N2.bit.INT2E = 1;
AdcaRegs.ADCINTFLGCLR.all = 0x0002;
EDIS;
//
//software force start SOC0
//
AdcaRegs.ADCSOCFRC1.all = 0x0001;
AdcaResult = AdcaResultRegs.ADCRESULT0;
//
//disable all ADCINT flags to stop sampling
//
EALLOW;
AdcaRegs.ADCINTSEL1N2.bit.INT2E = 0;
EDIS;
}while(1);
}
//
// ConfigureADC - Write ADC configurations and power up the ADC for both
// ADC A and ADC B
//
void ConfigureADC(void)
{
EALLOW;
//
//write configurations
//
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
//
//Set pulse positions to late
//
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//
//power up the ADC
//
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//
//delay for 1ms to allow ADC time to power up
//
DELAY_US(1000);
EDIS;
}
//
// SetupADCContinuous - setup the ADC to continuously convert on one channel
//
void SetupADCContinuous()
{
Uint16 acqps;
//
// Determine minimum acquisition window (in SYSCLKS) based on resolution
//
if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
{
acqps = 14; //75ns
}
else //resolution is 16-bit
{
acqps = 63; //320ns
}
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 2; //SOC will convert on channel A2
AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCINTSEL1N2.bit.INT2E = 0; //disable INT2 flag
AdcaRegs.ADCINTSEL1N2.bit.INT2CONT = 0;
AdcaRegs.ADCINTSEL1N2.bit.INT2SEL = 14; //end of SOC14 will set INT2 flag
//
//ADCINT2 will trigger first 8 SOCs
//
AdcaRegs.ADCINTSOCSEL1.bit.SOC0 = 2;
EDIS;
}
void configureDAC()
{
EALLOW;
DacaRegs.DACCTL.bit.DACREFSEL = 1;//参考电压选择 0:VDAC/VSSA 1:VREFHI/VREFLO
DacaRegs.DACOUTEN.bit.DACOUTEN = 1;//DAC输出使能
DacaRegs.DACVALS.all = 0;//影子寄存器
DELAY_US(10); // Delay for buffered DAC to power up
EDIS;
}