28035的CLA程序空间0x9000~0xA000被配置给CLA后CPU无访问权限,我现在遇到的问题时CLA不需要那么多程序空间,启用CLA后占用了太多的RAM资源,所以我想确认下是不是真的没有方法减小CLA对程序空间的占用?例如我想CLA只用0x9000~0x9400做程序空间,把0x9400~0xA000留给CPU用。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
28035的CLA程序空间0x9000~0xA000被配置给CLA后CPU无访问权限,我现在遇到的问题时CLA不需要那么多程序空间,启用CLA后占用了太多的RAM资源,所以我想确认下是不是真的没有方法减小CLA对程序空间的占用?例如我想CLA只用0x9000~0x9400做程序空间,把0x9400~0xA000留给CPU用。
通过CCS下的Memory Allocation看一下相关区域的内存占用情况。
我不问内存的占用情况,我的问题是:我想CLA只用0x9000~0x9400做CLA的程序空间,把0x9400~0xA000留给CPU用可以实现吗?
我实测是不行的,你有试过CPU和CLA共用CLA的程序空间0x9000~0xA000这种操作吗?
我刚才仔细看了一下,之前回复你的不太准确。
0x9000~0xA000是CLA专用的RAM,CLA程序在这里运行。这一块区域不能用作它用。