移植的时候报错:
file "../source/C28x_SGEN_Lib_fixed.lib<sgt1c.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C28FPU32" specified in a previous file or on the command line Sin C/C++ Problem
"file:/C:/ti/ccs1230/ccs/tools/compiler/dmed/HTML/16008.html">#16008-D</a> file "../source/C28x_SGEN_Lib_fixed.lib<SINTB360.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line Sin C/C++ Problem
这个怎么解决啊,这是他库里面提供的lib文件