Other Parts Discussed in Thread: TIDA-01606
您好,在进行TIDA-01606项目的学习中遇到了一些问题希望能得到解答。
问题1:关于在功率板上的继电器问题,在该项目中4个继电器上都并联了一个电阻,我想知道并联这个电阻的作用,因为我发现当并联上此电阻后继电器相当于不发生作用了,因为即使没有给他命令使其吸合,逆变侧和网侧通过此电阻依然是连接在了一起。
问题2:在参考设计文档中实验的部分,以及在功率板板上的丝印我都注意到了J33连接15V辅助电源,但在PCB文档中可以看到这个地方连接的是24V电源,并且这一部分连接到了驱动板上,在驱动板上24V电源经过UCC14240DWNQ1 DC/DC变换芯片得到15V和-4V电压,如果J33连接15V的话,显然是不在UCC14240DWNQ1输入电压范围内的,这样不就出现了不能工作的问题吗。
希望能得到解答。
LC