Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE
void PWMDRV_PSFB_PCMC_CNF(int16 n, int16 period, int16 SR_Enable, int16 Comp2_Prot)
{
// n = the ePWM module number, i.e. selects the target module for init.
// ePWM(n) init. Note EPWM(n) is the Master
//Time Base SubModule Register
(*ePWM[n]).TBCTL.bit.PRDLD = TB_IMMEDIATE; // Set Immediate load
(*ePWM[n]).TBPRD = period;
(*ePWM[n]).TBPHS.half.TBPHS = 0;
(*ePWM[n]).TBCTR = 0;
(*ePWM[n]).TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
(*ePWM[n]).TBCTL.bit.PHSEN = TB_DISABLE;
(*ePWM[n]).TBCTL.bit.SYNCOSEL = TB_CTR_CMPB; // Used to sync EPWM(n+1) "down-stream"
(*ePWM[n]).TBCTL.bit.HSPCLKDIV = TB_DIV1;
(*ePWM[n]).TBCTL.bit.CLKDIV = TB_DIV1;
// Counter compare submodule registers
(*ePWM[n]).CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE;
(*ePWM[n]).CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;
(*ePWM[n]).CMPA.half.CMPA = period-68;
(*ePWM[n]).CMPB = period;
// Action Qualifier SubModule Registers
(*ePWM[n]).AQCTLA.bit.ZRO = AQ_SET;
(*ePWM[n]).AQCTLA.bit.PRD = AQ_CLEAR;
// DeadBand Control Register
(*ePWM[n]).DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
(*ePWM[n]).DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi Complimentary
(*ePWM[n]).DBRED = 20; // Initial value
(*ePWM[n]).DBFED = 20; // Initial value
// ePWM(n+1) init. EPWM(n+1) is a slave
//Time Base SubModule Register
(*ePWM[n+1]).TBCTL.bit.PRDLD = TB_SHADOW;
(*ePWM[n+1]).TBPRD = period-1;
(*ePWM[n+1]).TBPHS.half.TBPHS = 0;
(*ePWM[n+1]).TBCTR = 0;
(*ePWM[n+1]).TBCTL.bit.CTRMODE = TB_COUNT_UP;
(*ePWM[n+1]).TBCTL.bit.PHSEN = TB_ENABLE;
(*ePWM[n+1]).TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Sync "flow through" mode
(*ePWM[n+1]).TBCTL.bit.HSPCLKDIV = TB_DIV1;
(*ePWM[n+1]).TBCTL.bit.CLKDIV = TB_DIV1;
// Counter compare submodule registers
(*ePWM[n+1]).CMPA.half.CMPA = period + 10; // Initial value
(*ePWM[n+1]).CMPB = 20; // Initial value
(*ePWM[n+1]).CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
(*ePWM[n+1]).CMPCTL.bit.SHDWAMODE = CC_SHADOW;
(*ePWM[n+1]).CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
(*ePWM[n+1]).CMPCTL.bit.SHDWBMODE = CC_SHADOW;
// Action Qualifier SubModule Registers
(*ePWM[n+1]).AQCTLA.bit.CAU = AQ_SET;
(*ePWM[n+1]).AQCTLA.bit.CBU = AQ_CLEAR;
(*ePWM[n+1]).AQCTLA.bit.ZRO = AQ_CLEAR;
(*ePWM[n+1]).AQCTLA.bit.PRD = AQ_CLEAR;
(*ePWM[n+1]).AQCTLB.bit.CBU = AQ_SET;
(*ePWM[n+1]).AQCTLB.bit.CAU = AQ_CLEAR;
(*ePWM[n+1]).AQCTLB.bit.ZRO = AQ_CLEAR;
(*ePWM[n+1]).AQCTLB.bit.PRD = AQ_CLEAR;
// Cycle-by-cycle shutdown mechanism configuration
EALLOW;
//===========================================================================
// Define an event (DCAEVT1) based on Comparator 1 Output
(*ePWM[n+1]).DCTRIPSEL.bit.DCAHCOMPSEL = DC_COMP1OUT; // DCAH = Comparator 1 output
(*ePWM[n+1]).TZDCSEL.bit.DCAEVT1 = TZ_DCAH_HI; // DCAEVT1 = DCAH high(will become active
// as Comparator output goes high)
(*ePWM[n+1]).DCACTL.bit.EVT1SRCSEL = DC_EVT_FLT; // DCAEVT1 = DC_EVT_FLT (filtered)
(*ePWM[n+1]).DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC; // Take async path
// Enable DCAEVT1 as a one-shot source
(*ePWM[n+1]).TZSEL.bit.DCAEVT1 = 1; // Enable One-Shot Trip
// Following code for the sync mechanism based on the same trigger event - COMPxOUT
(*ePWM[n+1]).DCACTL.bit.EVT1SYNCE = 1; // Sync enabled
// What do we want the DCAEVT1 event to do? - Initial Configuration
(*ePWM[n+1]).TZCTL.bit.TZA = TZ_NO_CHANGE; // EPWMxA - no change
(*ePWM[n+1]).TZCTL.bit.TZB = TZ_FORCE_LO; // EPWMxB - go low
//===========================================================================
// Event Filtering Configuration
(*ePWM[n+1]).DCFCTL.bit.SRCSEL = DC_SRC_DCAEVT1;
(*ePWM[n+1]).DCFCTL.bit.BLANKE = DC_BLANK_ENABLE;
(*ePWM[n+1]).DCFCTL.bit.PULSESEL = DC_PULSESEL_ZERO;
(*ePWM[n+1]).DCFOFFSET = 2; // Blanking Window Offset = CMPA(n+1)
(*ePWM[n+1]).DCFWINDOW = 4; // Blanking window length - initial value
//===========================================================================
EDIS;
在上述的配置epwm1模块以及epwm2模块的代码中,有一些我不太理解的地方:
1.首先是epwm1模块将计数到CMPB时记为一次同步信号输出,同步信号输出到epwm2中,而epwm2模块的DCAEVT1事件的配置中,同样使能了DCAEVT1的同步信号,那epwm2模块会响应两个同步信号吗,如果是响应两个同步信号,峰值电流控制的波形就不太对了。
2.其次是在设置epwm2时,将PRD设置为period-1,而CMPA设置为period+10,那下方AQ配置中的CAU事件又是怎么触发的。
3.整段函数读下来我无法和峰值电流控制的波形所对应,由于我还没有完整地分析过此例程,此例程还配合其他部分来产生峰值电流控制的epwm了吗?