This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320F28377SPZPQ 我们现在老项目出现的问题是上电一段时间后出现了MCU反复复位的现象,将所有旁路电路进行了更换维修,都无法解决,只有更换TMS320F28377 主芯片才能回复正常。现场比例装了108台,陆续已经返回26台此问题.请帮忙看看原理图是否正确?
C58的作用?
pin17 - VSSA/VREFLOA,没有接模拟地;
pin18&38 - VDDA,每个VDDA要分别接一个最小2.2uF的去耦电容;
pin64 - VREGENZ,必须连接至VDDIO,而不是VDD。
1.从主板上电开始算起,多长时间会出现问题?
主板上电后运行2min会出现断电重启现象
2.在复位开始出现之前,电路板是否正常工作?
复位出现之前,电路板正常工作
3.重置的持续时间和频率是多少?请附上示波器图像。
主板上电后运行2min断电,持续20S,重新上电。继续运行2min,再次断电
4.如果你能够重新编程固件,问题就会消失吗?软件部分可以发来看一下么?
1台烧录过新程序,依然会出现断电重启现象,剩余2台烧录程序时软件报错,无法烧录。
5.代码中是否启用了看门狗?
代码中启用了看门狗功能
6.这些电路板在现场工作了多久才开始出现这个问题?
该批探测器在现场已经使用了1年以上,1年后陆续出现复位问题,1年中都是正常使用的
还是之前那颗料,看看这些是否有问题.
主板上电后运行2min会出现断电重启现象
1. 是指器件自己reset吗?
主板上电后运行2min断电,持续20S,重新上电。继续运行2min,再次断电
3. 这个过程中,哪些是人为的操作,哪些是器件本身自己的动作,请指明;
1台烧录过新程序,依然会出现断电重启现象,剩余2台烧录程序时软件报错,无法烧录。
4. 新程序?