通过仿真器下载BootLoader和APP程序之后,APP程序能正常运行(两路PWM输出,设置相同的占空比,两路PWM输出占空比相同),此时程序没有经过BootLoader,但是重启之后,程序由BootLoader跳转到APP之后,在测试APP程序,发现pwm输出不正确(发现两路PWM输出占空比不同),多次测试出现现象相同
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过仿真器下载BootLoader和APP程序之后,APP程序能正常运行(两路PWM输出,设置相同的占空比,两路PWM输出占空比相同),此时程序没有经过BootLoader,但是重启之后,程序由BootLoader跳转到APP之后,在测试APP程序,发现pwm输出不正确(发现两路PWM输出占空比不同),多次测试出现现象相同
BootLoader的CMD配置
MEMORY { PAGE 0: /* Program Memory */ RAML00 : origin = 0x008000, length = 0x000100 /* on-chip RAM block L2 */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */ BOOT_CODE : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block L2 */ } SECTIONS { /* Allocate program areas: */ .cinit : > BOOT_CODE PAGE = 0 /* 初始化的全局变量和static变量表*/ .pinit : > BOOT_CODE, PAGE = 0 /* 全局对象的构造函数表 C++范畴*/ .text : > BOOT_CODE PAGE = 0 /* 可执行代码和常数段 */ codestart : > BEGIN PAGE = 0 /* 代码启动段 */ // Flash28_API: // { // -l Flash2803x_API_V100.lib(.econst) // -l Flash2803x_API_V100.lib(.text) // } LOAD = BOOT_CODE, // RUN = RAML0, // LOAD_START(_Flash28_API_LoadStart), // LOAD_END(_Flash28_API_LoadEnd), // RUN_START(_Flash28_API_RunStart), // PAGE = 0 ramfuncs : LOAD = BOOT_CODE, /* 将定义到段ramfuncs上的代码,载入到BOOT_CODE */ RUN = RAML00, /* 定义到ramfuncs上的代码,复制到RAML0上运行 */ LOAD_START(_RamfuncsLoadStart), /* 所要加载程序在Flash里的初始地址 */ LOAD_END(_RamfuncsLoadEnd), /* 所要加载程序在Flash里的结束地址 */ RUN_START(_RamfuncsRunStart), /* 程序运行的起始地址 */ PAGE = 0 csmpasswds : > CSM_PWL_P0 PAGE = 0 /* 密码段 */ csm_rsvd : > CSM_RSVD PAGE = 0 /* 使用代码安全模块时,需要预留的段 */ /* Allocate uninitalized data sections: 未初始化数据段 */ .stack : > RAMM0 PAGE = 1 /* 栈空间*/ .ebss : > RAMM1 PAGE = 1 /* 长调用的全局或static变量,初始化和未初始化变量*/ .esysmem : > RAMM0 PAGE = 1 /* Initalized sections go in Flash 已初始化的段*/ .econst : > BOOT_CODE PAGE = 0 /* 字符串常量和far const定义的全局和静态变量(static const)*/ .switch : > BOOT_CODE PAGE = 0 /* 存放switch语句产生的常数表格*/ /* Allocate IQ math areas: 分配 IQ 数学表区域 */ IQmath : > BOOT_CODE PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT }
APP的CMD配置
_Cla1Prog_Start = _Cla1funcsRunStart; -heap 0x200 -stack 0x400 CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { PAGE 0: /* Program Memory */ RAML00 : origin = 0x008000, length = 0x000100 /* on-chip RAM block L0 */ RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */ RAML3 : origin = 0x009000, length = 0x000400 /* on-chip RAM block L3 */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */ APP_INFO_ADDR :origin = 0x3EE000, length = 0x000006 APP_BEGIN : origin = 0x3EE006, length = 0x000002 APP_CODE : origin = 0x3EE200, length = 0x005E00 IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x000050, length = 0x0007B0 /* on-chip RAM block M0 */ RAML01 : origin = 0x008100, length = 0x000700 /* on-chip RAM block L0 */ CLA_DATA : origin = 0x3EE008, length = 0x0001F8 CLARAM0 : origin = 0x008800, length = 0x000400 CLARAM1 : origin = 0x009800, length = 0x000400 CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } SECTIONS { /* Allocate program areas: */ .cinit : > APP_CODE PAGE = 0 .pinit : > APP_CODE, PAGE = 0 .text : > APP_CODE PAGE = 0 codestart : > APP_BEGIN PAGE = 0 ramfuncs : LOAD = APP_CODE, RUN = RAML2, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), RUN_START(_RamfuncsRunStart), PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > RAMM0 PAGE = 1 .ebss : > RAML01 PAGE = 1 .esysmem : > RAMM0 PAGE = 1 /* Initalized sections go in Flash */ .econst : > APP_CODE PAGE = 0 .switch : > APP_CODE PAGE = 0 InfoData : > APP_INFO_ADDR PAGE = 0 /* Allocate IQ math areas: */ IQmath : > APP_CODE PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD .bss_cla : > CLARAM0, PAGE = 1 .scratchpad : > CLARAM0, PAGE = 1 Cla1Prog : LOAD = APP_CODE, RUN = RAML3, LOAD_START(_Cla1funcsLoadStart), LOAD_END(_Cla1funcsLoadEnd), RUN_START(_Cla1funcsRunStart), LOAD_SIZE(_Cla1funcsLoadSize), PAGE = 0 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 Cla1DataRam0 : > CLARAM0, PAGE = 1 Cla1DataRam1 : > CLARAM1, PAGE = 1 GROUP : LOAD = CLA_DATA, RUN = CLARAM1, LOAD_START(_Cla1mathTablesLoadStart), LOAD_END(_Cla1mathTablesLoadEnd), RUN_START(_Cla1mathTablesRunStart), LOAD_SIZE(_Cla1mathTablesLoadSize), PAGE = 1 { CLA1mathTables .const_cla } CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > CLARAM0, PAGE = 1 /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT }
发现pwm输出不正确(发现两路PWM输出占空比不同)
能不能上传一下PWM的波形?占空比不同会相差多少?相差的值固定吗?
这个是正确的波形,直接从BootLoader程序跳转到app
你之前说的是不经过bootloader时波形是正常的,而从bootloader跳到APP的时候波形是不正常的。这里再确认一下;
这是错误的波形,右边是启动时的EPWM1、EPWM2、EPWM3、EPWM4寄存器的变化情况
示波器上的波形对应的分别是哪两路信号?