This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题1:目前F28035芯片的CLA有C语言版本的实例吗,有的话哪里能找到?
问题2:在CCS3.3下,要使用CLA功能,想用C语言进行编程,编译器版本应该是多少?如下图行吗?
controlSUITE中有F28035芯片的CLA例程,路径是:C:\ti\controlSUITE\device_support\f2803x\v128\DSP2803x_examples_cla_ccsv5,需要使用CCS V5以上的版本才能直接打开
Joey Mao,
前面我在参加TI 2014 C2000系列研讨会的时候,说是可以再CCS3.3用C语言编程CLA,只要编译器版本在多少就行了,我想直接用CCS3.3不知道有没有办法?
另外,从CCS3.3直接切刀CCS V5以上不知道区别有多大,会不会影响开发进度?
编译器版本6.1.0以上,CCS 3.3是可以但是目前没有相关例程
CCS V5比3.3更强大,更稳定,界面和菜单有所变化,刚开始用可能有点不太习惯,但是熟悉了CCS V5比3.3更好用,你可以安装一个试试