This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何使用IO口模拟I2C?



需要要配置什么是不是定义如下(扩展MPU6050)

#define SCL GpioCtrlRegs.GPBDIR.bit.GPIO0
#define SDA GpioCtrlRegs.GPBDIR.bit.GPIO1

EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 0;
GpioCtrlRegs.GPAQSEL1.bit.GPIO0=0;

GpioCtrlRegs.GPAQSEL1.bit.GPIO1=0;

GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1;

GpioCtrlRegs.GPAPUD.bit.GPIO1 = 1;


EDIS;