现在正使用F28377D的2837xD_RAM_lnk_cpu1.cmd 和2837xD_RAM_lnk_cpu2.cmd 发现cpu1里的cmd文件是有共享内存的,cpu2的cmd文件中,没有,这是问什么,那cpu2的一些变量怎么能放在共享内存里共享呢?
如上两图所示的cmd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在正使用F28377D的2837xD_RAM_lnk_cpu1.cmd 和2837xD_RAM_lnk_cpu2.cmd 发现cpu1里的cmd文件是有共享内存的,cpu2的cmd文件中,没有,这是问什么,那cpu2的一些变量怎么能放在共享内存里共享呢?
如上两图所示的cmd
您好,我看了一下数据手册上的说明,有一个GSxMSEL寄存器,由这个寄存器选择GSx归属哪。个cpu,现在有两个问题,
1.初始化时用这个寄存器分配GSx,是不是提前也要把两个cpu的cmd文件改好,比如将GS1、2、3、4、5、6分配给CPU1,GS7-15分配给cpu2,就要把两个核的cmd文件改写,将下面这些写到cpu2的cmd里
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
2.手册上说,这些GSX分配给一个CPU之后,另一个cpu就只能读了,不能写,那请问有没有一个区域,定义的变量两个cpu都能读写呢,谢谢