Other Parts Discussed in Thread: TMS320F280039,
项目编译没有问题,CCXML文件 Test Connection也没有问题
但是在尝试Debug时,出现如下提示:
C28xx_CPU1: GEL Output: RAM initialization done C28xx_CPU1: GEL Output: Memory Map Initialization Complete C28xx_CPU1: GEL Output: ... DCSM Initialization Start ... C28xx_CPU1: GEL Output: ... DCSM Initialization Done ... C28xx_CPU1: GEL: Error while executing OnReset(0): identifier not found: SYSCTL_O_DC21 at (0x0005D000+SYSCTL_O_DC21) [f280033.gel:815] at Device_Config() [f280033.gel:193] at OnReset(0) C28xx_CPU1: GEL Output: ... DCSM Initialization Start ... C28xx_CPU1: GEL Output: ... DCSM Initialization Done ... C28xx_CPU1: GEL: Error while executing OnReset(0): identifier not found: SYSCTL_O_DC21 at (0x0005D000+SYSCTL_O_DC21) [f280033.gel:815] at Device_Config() [f280033.gel:193] at OnReset(0) C28xx_CPU1: Flash Programmer: Missing Flash Programming Settings. C28xx_CPU1: File Loader: Memory write failed: Unknown error C28xx_CPU1: GEL: File: D:\GitWorkSpace\Standard\AST-Boot-F280033\Project\Debug\ast-boot_f280033.out: Load failed.

根据提示,检查f280033.gel文件,其中确实没有定义SYSCTL_O_DC21
根据上下文,手动补录了SYSCTL_O_DC21的定义:
#define SYSCTL_O_DC20 0x38 // Device Capability: GSx SRAM Customization #define SYSCTL_O_DC21 0x3A // Device Capability: #define SYSCTL_O_DC22 0x3C // Device Capability: FSI
再次尝试下载,出现如下错误提示:

检查工程设置,确实没有发现Flash 扇区设置的页面(Flash Setting)

删除了ccxml,重新建立该文件,还是一样的结果
正常的项目Debug设置如下:

之前某个工程遇见过同样的问题,当时不知道怎么就好了。
请问有没有相关的提示?