This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: 无法在cpu1的epwm中断里面,嵌套cpu1的ipc中断(CMTOCPUx IPCINTR0)

Part Number: TMS320F28388D


参照例程1、interrupt\interrupt_ex3_sw_prioritization.c

2、ipc_ex1_basic_c28x1.c

3、ipc_ex1_basic_cm.c

无法在epwm中断里面,嵌套来自M4触发的ipc中断

  • EPWM的中断嵌套设置:

    __interrupt void epwm1ISR(void)
    {
        //
        // Save IER register on stack
        //
        volatile uint16_t tempPIEIER = HWREGH(PIECTRL_BASE + PIE_O_IER3);
        
        //
        // Set the global and group priority to allow CPU interrupts
        // with higher priority
    
        IER |= M_INT3;
        IER &= MINT3;
        HWREGH(PIECTRL_BASE + PIE_O_IER3) &= MG3_1;
        
        //
        // Clear INT flag for this timer
        //
        EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE);
        
        //
        // Enable Interrupts
        //
        Interrupt_clearACKGroup(0xFFFFU);
        __asm("  NOP");
        EINT;
        
        // Insert ISR Code here.......
        epwm_ISR();
        
        //
        // Disable interrupts and restore registers saved:
        //
        DINT;
        HWREGH(PIECTRL_BASE + PIE_O_IER3) = tempPIEIER;
    
        //Add ISR to Trace
        traceISR[traceISRIndex % TRACE_SIZE] = 0x0017;
        traceISRIndex++;
        
    }

  • 中断嵌套的宏定义:

    全局:

    #define INT1PL      0       // Global Priority for Group1 Interrupts
    #define INT2PL      0        // Global Priority for Group2 Interrupts
    #define INT3PL      16        // Global Priority for Group3
    #define INT4PL      0        // Global Priority for Group4 Interrupts
    #define INT5PL      0        // Global Priority for Group5 Interrupts
    #define INT6PL      0        // Global Priority for Group6
    #define INT7PL      0        // Global Priority for Group7 Interrupts
    #define INT8PL      0        // Global Priority for Group8 Interrupts
    #define INT9PL      0        // Global Priority for Group9
    #define INT10PL     0        // Global Priority for Group10 Interrupts
    #define INT11PL     1        // Global Priority for Group11 Interrupts
    #define INT12PL     0        // Global Priority for Grou
    #define INT13PL     0        // Global Priority for INT13 (TINT1)
    #define INT14PL     0        // Global Priority for INT14 (TINT2)
    #define INT15PL     0        // Global Priority for DATALOG
    #define INT16PL     0        // Global Priority for RTOSINT

    组:

    #define G3_1PL      1       // EPWM1_INT
    #define G3_2PL      0       // EPWM2_INT
    #define G3_3PL      0       // EPWM3_INT
    #define G3_4PL      0       // EPWM4_INT
    #define G3_5PL      0       // EPWM5_INT
    #define G3_6PL      0       // EPWM6_INT
    #define G3_7PL      0       // EPWM7_INT
    #define G3_8PL      0       // EPWM8_INT
    #define G3_9PL      0       // EPWM9_INT
    #define G3_10PL     0       // EPWM10_INT
    #define G3_11PL     0       // EPWM11_INT
    #define G3_12PL     0       // EPWM12_INT
    #define G3_13PL     0       // EPWM13_INT
    #define G3_14PL     0       // EPWM14_INT
    #define G3_15PL     0       // EPWM15_INT
    #define G3_16PL     0       // EPWM16_INT
    
    
    #define G11_1PL     0       // CLA1_1_INT
    #define G11_2PL     0       // CLA1_2_INT
    #define G11_3PL     0       // CLA1_3_INT
    #define G11_4PL     0       // CLA1_4_INT
    #define G11_5PL     0       // CLA1_5_INT
    #define G11_6PL     0       // CLA1_6_INT
    #define G11_7PL     0       // CLA1_7_INT
    #define G11_8PL     0       // CLA1_8_INT
    #define G11_9PL     1       // CMTOCPUXIPC0_INT
    #define G11_10PL    0       // CMTOCPUXIPC1_INT
    #define G11_11PL    0       // CMTOCPUXIPC2_INT
    #define G11_12PL    0       // CMTOCPUXIPC3_INT
    #define G11_13PL    0       // CMTOCPUXIPC4_INT
    #define G11_14PL    0       // CMTOCPUXIPC5_INT
    #define G11_15PL    0       // CMTOCPUXIPC6_INT
    #define G11_16PL    0       // CMTOCPUXIPC7_INT

  • 好的,感谢您的帮助!