Part Number: TMS320F28335
28335,CSM,已烧录设置的密码程序,程序正常运行,
然后在Debug Confugurations中输入错误密码,
接着再用xds100v3烧录,此时会锁死芯片吗
如果不是csm的原因,芯片锁死的的原因可能是什么呢?
提示信息为:
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.