Part Number: TMS320F280049C
IODFTCTRL寄存器用于模拟各种错误和测试条件,其中第28位用于创建ISF错误,启用IODFT模式后(IODFTENA=1010),在LIN模式下,同步字段中的位宽会发生变化,发送数据未设置ISF错误,但是仅在CERRENA/PBERRENA/BERRENA使能后相应的错误标准位都置位了,这个功能是如何使用的呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049C
IODFTCTRL寄存器用于模拟各种错误和测试条件,其中第28位用于创建ISF错误,启用IODFT模式后(IODFTENA=1010),在LIN模式下,同步字段中的位宽会发生变化,发送数据未设置ISF错误,但是仅在CERRENA/PBERRENA/BERRENA使能后相应的错误标准位都置位了,这个功能是如何使用的呢
问题在于使能ISFERRENA以后,开启模拟回环通过发送引脚后,相应的标志位没有被设置,我使用逻辑分析仪捕捉了信号,发现同步字段与正常的一样,
(波特率20K)
以下是我的代码
__interrupt void level0ISR(void);
__interrupt void level1ISR(void);
void lin_enable_int(LIN_InterruptLine INTERRUPT_LINEx,uint32_t intFlags);
void main()
{
uint16_t txID;
txID = 0x10 ;
txID = LIN_generateParityID(txID);
Device_init();
Device_initGPIO();
GPIO_setPinConfig(GPIO_37_LINA_TX);
GPIO_setPadConfig(37, GPIO_PIN_TYPE_STD | GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(37, GPIO_QUAL_ASYNC);
GPIO_setDirectionMode(37U, GPIO_DIR_MODE_OUT);
GPIO_setPinConfig(GPIO_35_LINA_RX);
GPIO_setPadConfig(35, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(35, GPIO_QUAL_ASYNC);
GPIO_setDirectionMode(35U, GPIO_DIR_MODE_IN);
Interrupt_initModule();
Interrupt_initVectorTable();
EINT;
ERTM;
Interrupt_register(INT_LINA_0, &level0ISR);
Interrupt_register(INT_LINA_1, &level1ISR);
Interrupt_enable(INT_LINA_0);
Interrupt_enable(INT_LINA_1);
LIN_initModule(LINA_BASE);
//波特率20K
LIN_setBaudRatePrescaler(LINA_BASE, 312U, 0U);
//设置ISF中断
lin_enable_int(LIN_INTERRUPT_LINE0,LIN_INT_ISFE);
LIN_disableIntLoopback(LINA_BASE);
//创建isf错误
// Clear the IO DFT Enable Key
HWREGH(myLIN_BASE + LIN_O_IODFTCTRL) &= ~(LIN_IODFTCTRL_IODFTENA_M);
// Enable write access
HWREGH(myLIN_BASE + LIN_O_IODFTCTRL) |= (LIN_IO_DFT_KEY <<LIN_IODFTCTRL_IODFTENA_S);
//HWREG_BP(myLIN_BASE + LIN_O_IODFTCTRL) |= LIN_ISF_ERROR;
HWREG_BP(myLIN_BASE + LIN_O_IODFTCTRL) |= LIN_ISF_ERROR|0x2;//模拟回环通过发送引脚
while(!LIN_isTxReady(LINA_BASE));
//发送数据
LIN_sendData(LINA_BASE, txData);
LIN_setIDByte(LINA_BASE, txID);
while(1);
}
void lin_enable_int(LIN_InterruptLine INTERRUPT_LINEx,uint32_t intFlags)
{
LIN_enableInterrupt(LINA_BASE, intFlags);
//INT0
if(INTERRUPT_LINEx==LIN_INTERRUPT_LINE0)
{
//仅在LIN模式下,将各个中断源映射到 INT0 线
LIN_setInterruptLevel0(LINA_BASE, intFlags);
//使能全局中断0
LIN_enableGlobalInterrupt(LINA_BASE, LIN_INTERRUPT_LINE0);
//失能全局中断1
LIN_disableGlobalInterrupt(LINA_BASE, LIN_INTERRUPT_LINE1);
//清除全局中断标志位
LIN_clearGlobalInterruptStatus(LINA_BASE, LIN_INTERRUPT_LINE0);
}
//INT1
else
{
//仅在LIN模式下,将各个中断源映射到 INT1 线
LIN_setInterruptLevel1(LINA_BASE, intFlags);
LIN_enableGlobalInterrupt(LINA_BASE, LIN_INTERRUPT_LINE1);
//失能全局中断0
LIN_disableGlobalInterrupt(LINA_BASE, LIN_INTERRUPT_LINE0);
LIN_clearGlobalInterruptStatus(LINA_BASE, LIN_INTERRUPT_LINE1);
}
}
__interrupt void level0ISR(void)
{
level0Count++;
if(LIN_getInterruptStatus(LINA_BASE)& LIN_FLAG_ISFE)
{
vectorOffset = LIN_getInterruptLine0Offset(LINA_BASE);
LIN_clearInterruptStatus(LINA_BASE, LIN_INT_ISFE);
}
if(LIN_getInterruptStatus(LINA_BASE)& LIN_FLAG_CE)
{
vectorOffset = LIN_getInterruptLine0Offset(LINA_BASE);
LIN_clearInterruptStatus(LINA_BASE, LIN_INT_ISFE);
}
vectorOffset = LIN_getInterruptLine0Offset(LINA_BASE);
LIN_clearGlobalInterruptStatus(LINA_BASE, LIN_INTERRUPT_LINE0);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP8);
}
__interrupt void level1ISR(void)
{
}